Solid Edge FrameworkSupport Type Library
BreakLine Property
Description
Specifies whether or not a breakline is added between the leader line and the referenced dimensioning object.
Property type
Read-write property
Syntax
Visual Basic
Public Property BreakLine As Boolean
Remarks
The BreakLine property can only be True if the Leader property is also True. For all dimensioning objects, the break lines are horizontal (traverses the X axis) and connect to either the left or right side of the object. All break lines attach such that they would pass through the object's center if they were not trimmed by the object's outline.
See Also

WeldSymbol Object  | WeldSymbol Members