Solid Edge FrameworkSupport Type Library
AddWeldSymbol Method
Description
Creates a WeldSymbol. For creating PMI WeldSymbol a plane must be set (XY plane is the default). The collection object from which it is derived (sheet/profile2d/PMI) dictate the creation of WeldSymbol.
Syntax
Visual Basic
Public Function AddWeldSymbol( _
   ByVal AnnotInitData As AnnotInitData _
) As WeldSymbol
Parameters
AnnotInitData
See Also

WeldSymbols Collection  | WeldSymbols Members  | Solid Edge ST5 - What's New