Solid Edge FrameworkSupport Type Library
GetFraction Method
Description
Returns the fraction data if it is there at insert index
Syntax
Visual Basic
Public Sub GetFraction( _
   ByRef Flag As Boolean, _
   ByRef UpperText As String, _
   ByRef LowerText As String, _
   ByRef typeOption As TextFractionTypeConstants, _
   ByRef alignOption As TextFractionAlignConstants, _
   ByRef fractionSize As TextFractionSizeConstants _
) 
Parameters
Flag
UpperText
LowerText
typeOption
ValueDescription
igLinearFractionText Fraction Linear Type
igSkewedText Fraction Skewed Type
igStackedText Fraction Stacked Type
igToleranceText Fraction Tolerance Type
alignOption
ValueDescription
igLowerText Fraction Align Lower Type
igMiddleText Fraction Align Middle Type
igUpperText Fraction Align Upper Type
fractionSize
ValueDescription
ig10Text Fraction Size 10
ig100Text Fraction Size 100
ig20Text Fraction Size 20
ig30Text Fraction Size 30
ig40Text Fraction Size 40
ig50Text Fraction Size 50
ig60Text Fraction Size 60
ig70Text Fraction Size 70
ig80Text Fraction Size 80
ig90Text Fraction Size 90
See Also

TextEdit Object  | TextEdit Members  | Solid Edge ST5 - What's New