Solid Edge FrameworkSupport Type Library
SurfaceFinishSymbol Object
Members 
Description
Defines surface roughness, waviness, and any necessary machining lay markings.
Object Model
SurfaceFinishSymbol ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionDisplayData ObjectDimStyle Object
Remarks
These symbols specify the mean surface roughness as measured in micro-units. Individual characteristics (such as the maximum roughness information) are specified and modified through properties of the SurfaceFinishSymbol object.
See Also

SurfaceFinishSymbol Members