Solid Edge FrameworkSupport Type Library : SizeModeConstants Enumeration |
Member | Value | Description |
---|---|---|
igFrameChangesSize | 2 | The frame size changes to match the extents of the object. |
igFrameCrops | 1 | The frame keeps its size and the object gets cropped or fits within the frame. |
igObjectScaled | 3 | The object is scaled so that the entire object can be viewed within the frame. |