Solid Edge FrameworkSupport Type Library
FeatureControlFrameDataSets Collection
Members 
Description
A collection of FeatureControlFrameDataSet objects.
Remarks
Each of these collections of settings is a data set. By adding a data set to the FeatureControlFrameDataSets collection object, those settings are available to the FeatureControlFrames collection object as a DataSet property selection. This property specifies the set of feature control symbol characteristics on which to base a new FeatureControlFrame object.
See Also

FeatureControlFrameDataSets Members