Solid Edge FrameworkSupport Type Library
FeatureControlFrameDataSet Object Members
Overview 
Public Properties
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property BoxAlignmentSets and returns the status of the alignment of a feature control frame. Note: This is a multi-level feature control option. if it's set true value, all first and second box would align and text move to the center of box.
Public Property CompositePrimaryAndSecondaryTextSets and returns the composite status of primary and secondary text.
Public Property CompositeSecondaryAndTertiaryTextSets and returns the composite status of secondary and tertiary text.
Public Property CompositeTertiaryAndQuaternaryTextSets and returns the composite status of tertiary and quaternary text.
Public Property FCFAllAroundSpecifies whether or not an all around symbol is to be applied to the Leader of the referenced object.
Public Property FCFAllOverSpecifies whether or not an all over symbol is to be applied to the Leader of the referenced object.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property NameReturns the name of the referenced object.
Public Property PrimaryFrameSets and returns the primary frame text.
Public Property QuaternaryFrameSets and returns the quaternary frame text.
Public Property SecondaryFrameSets and returns the secondary frame text for the referenced FeatureControlFrame object.
Public Property TertiaryFrameSets and returns the tertiary frame text.
See Also

FeatureControlFrameDataSet Object