Solid Edge FrameworkSupport Type Library
DimSurfTextureSymTypeConstants Enumeration
Description
Surface Finish Texture Symbol Types
Members
MemberValueDescription
igDimSurfaceFinishBasic1Basic
igDimSurfaceFinishBasicHz4Basic With Horizontal
igDimSurfaceFinishMachined2Machined
igDimSurfaceFinishMachined211Machined (2)
igDimSurfaceFinishMachined312Machined (3)
igDimSurfaceFinishMachined413Machined (4)
igDimSurfaceFinishMachinedHz5Machined With Horizontal
igDimSurfaceFinishMachinedHz214Machined With Horizontal (2)
igDimSurfaceFinishMachinedHz315Machined With Horizontal (3)
igDimSurfaceFinishMachinedHz416Machined With Horizontal (4)
igDimSurfaceFinishNoMaterialRemoval3No Material Removal
igDimSurfaceFinishNoMaterialRemovalHz6No Material Removal With Horizontal
igDimSurfaceFinishNoWorkingSurface17No Working Surface
igDimSurfaceFinishTriangle7Triangle
igDimSurfaceFinishTriangle28Triangle (2)
igDimSurfaceFinishTriangle39Triangle (3)
igDimSurfaceFinishTriangle410Triangle (4)