Solid Edge FrameworkSupport Type Library
UseTextSizeForCombinedTolValueDisplay Property
Description
If True, specifies that the dimension text size will be used for the tolerance when upper and lower tolerance have the same absolute value but opposite signs.
Property type
Read-write property
Syntax
Visual Basic
Public Property UseTextSizeForCombinedTolValueDisplay As Boolean
See Also

DimStyle Object  | DimStyle Members  | Solid Edge ST5 - What's New