Solid Edge FrameworkSupport Type Library
SetAxisMode Method
Description
Sets the axis mode. Not used when creating a Chamfer Dimension, use SetChamferAxisMode instead.
Syntax
Visual Basic
Public Sub SetAxisMode( _
   ByVal AxisMode As DimAxisModeConstants _
) 
Parameters
AxisMode
ValueDescription
igDimAxisModeCoordinateCorresponds to Use Coordinate System
igDimAxisModeDefaultCorresponds to Horizontal/Vertical
igDimAxisModeExplicitCorresponds to Use DimensionAxis
igDimAxisModeImpliedCorresponds to By Two Points
See Also

DimInitData Object  | DimInitData Members  | Solid Edge ST5 - What's New  | Solid Edge ST4 MP1 - What's New  | Solid Edge ST3 MP8 - What's New