Solid Edge FrameworkSupport Type Library
CenterMark Object
Members 
Description
Consists of two perpendicular linear elements that form a crosshair pattern at the center point of a curved element.
Object Model
CenterMark ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionDimStyle Object
Remarks
The characteristics of the centermark are determined by the active dimension style settings. That is, the current active width and line type determines the line width and style, respectively.
See Also

CenterMark Members