Solid Edge FrameworkSupport Type Library
BackDrop Object Members
Overview 
Public Properties
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property CustomSheetColorSets and returns the color of the sheet when the UseCustomSheetColor property is True.
Public Property DynamicGridSpacingSets and returns the spacing definition for a dynamic grid.
Public Property GridColorSets and returns the color of the grid for the referenced BackDrop object when the GridDisplay property is True.
Public Property GridDisplaySpecifies whether or not the grid of the referenced BackDrop object is to be displayed.
Public Property GridTypeSets and returns the type of the grid.
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property MarginColorSets and returns the color of the margin of the referenced BackDrop object when the MarginDisplay property is True.
Public Property MarginDisplaySpecifies whether or not the margin of the referenced BackDrop object is displayed in the window.
Public Property StaticGridSpacingSets and returns the spacing of a static grid for the referenced BackDrop object.
Public Property UseCustomSheetColorDetermines if a custom sheet color is to be used in the window as a backdrop color.
See Also

BackDrop Object