Solid Edge FrameworkSupport Type Library
AreaProperties Object Members
Overview 
Public Methods
Public Method AddBoundariesThis method creates a blend between edges, faces, or a combination of the two.
Public Method BringForward
Public Method BringToFront
Public Method Copy
Public Method Cut
Public Method DeleteDeletes the referenced object.
Public Method Duplicate
Public Method GetAreaProperties
Public Method MirrorCopies the referenced object about an axis.
Public Method MoveMoves the referenced object.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method RotateRotates the referenced object.
Public Method ScaleScales the referenced object by a specified factor.
Public Method SendBackwardThis method changes the display order of visible objects by moving the referenced object so that it is in back of the first object behind it.
Public Method SendToBackThis method changes the display order of visible objects by moving the referenced object behind all overlapping objects.
Public Method SetAxesLabels
Public Method SetAxesLength
Public Method ShowAxes
Public Properties
Public Property Application
Public Property AreaFillStyleReturns the Shells collection object for the referenced Body object.
Public Property AxesLabelStyle
Public Property AxesStyle
Public Property DocumentReturns the document to which the referenced object belongs.
Public Property IndexReturns the numeric index for the active object.
Public Property Key
Public Property LayerSets and returns the named layer on which the referenced object resides.
Public Property NameReturns the name of the referenced object.
Public Property Parent
Public Property TypeSpecifies the type of the object being referenced.
See Also

AreaProperties Object  | Solid Edge V20 - What's New