Solid Edge Draft Type Library
DisplayAnnotation Property
Description
Specifies whether or not the annotation geometry is to be displayed. The annotation is typically either the DetailEnvelope object or the ViewPlane object.
Property type
Read-write property
Syntax
Visual Basic
Public Property DisplayAnnotation As Boolean
See Also

DrawingView Object  | DrawingView Members