Solid Edge Draft Type Library
DrawingView Object
Members 
Description
A 2-D representation of a 3-D part or assembly model.
Object Model
DrawingView ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionBrokenOutSectionProfiles CollectionCoordinateSystems2d CollectionDraftProfile ObjectApplication ObjectArcs2d CollectionBSplineCurves2d CollectionCircles2d CollectionDimensions CollectionEllipses2d CollectionEllipticalArcs2d CollectionLines2d CollectionRelations2d CollectionCuttingPlanes CollectionDetailEnvelopes CollectionDVArcs2d CollectionDVBSplineCurves2d CollectionDVCircles2d CollectionDVEllipses2d CollectionDVEllipticalArcs2d CollectionDVLines2d CollectionDVLineStrings2d CollectionDVPoints2d CollectionModelMembers CollectionReference ObjectGraphicMembers CollectionHighlightDrawingViewMembers ObjectModelMembers CollectionDrawingView ObjectApplication ObjectBrokenOutSectionProfiles CollectionCoordinateSystems2d CollectionDraftProfile ObjectCuttingPlanes CollectionDetailEnvelopes CollectionDVArcs2d CollectionDVBSplineCurves2d CollectionDVCircles2d CollectionDVEllipses2d CollectionDVEllipticalArcs2d CollectionDVLines2d CollectionDVLineStrings2d CollectionDVPoints2d CollectionModelMembers CollectionReference ObjectGraphicMembers CollectionHighlightDrawingViewMembers ObjectModelMembers CollectionDrawingView Object
Remarks
A drawing view is used to display design space geometry in document space. A view of design space is enclosed by the drawing view border (a handle that allows manipulation of the drawing view). Only one part or assembly document can be used as the basis for drawing views in a draft document.
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDraftDocument As SolidEdgeDraft.DraftDocument
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objDrawingViews As SolidEdgeDraft.DrawingViews = Nothing
        Dim objDrawingView As SolidEdgeDraft.DrawingView = Nothing

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objDraftDocument = objApplication.ActiveDocument
            objSheet = objDraftDocument.ActiveSheet
            objDrawingViews = objSheet.DrawingViews
            objDrawingView = objDrawingViews.Item(1)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

DrawingView Members