Solid Edge Draft Type Library
ViewSide Property
Description
Sets or returns the side of the free end of the fold segment that determines the direction of the view. This will use the existing enumerated type SectionViewProfileSide, with only igLeftProfileSide and igRightProfileSide being valid. If the view has not been created it will have a default value of igLeftProfileSide.
Property type
Read-write property
Syntax
Visual Basic
Public Property ViewSide As SectionViewProfileSide
See Also

CuttingPlane Object  | CuttingPlane Members