Solid Edge Draft Type Library
CuttingPlane Object
Members 
Description
Object Model
CuttingPlane ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionDrawingView ObjectApplication ObjectBrokenOutSectionProfiles CollectionCoordinateSystems2d CollectionDraftProfile ObjectCuttingPlanes CollectionDetailEnvelopes CollectionDVArcs2d CollectionDVBSplineCurves2d CollectionDVCircles2d CollectionDVEllipses2d CollectionDVEllipticalArcs2d CollectionDVLines2d CollectionDVLineStrings2d CollectionDVPoints2d CollectionModelMembers CollectionReference ObjectGraphicMembers CollectionHighlightDrawingViewMembers ObjectModelMembers CollectionDrawingView ObjectDraftProfile ObjectApplication ObjectArcs2d CollectionBSplineCurves2d CollectionCircles2d CollectionDimensions CollectionEllipses2d CollectionEllipticalArcs2d CollectionLines2d CollectionRelations2d CollectionDrawingView ObjectApplication ObjectBrokenOutSectionProfiles CollectionCoordinateSystems2d CollectionDraftProfile ObjectCuttingPlanes CollectionDetailEnvelopes CollectionDVArcs2d CollectionDVBSplineCurves2d CollectionDVCircles2d CollectionDVEllipses2d CollectionDVEllipticalArcs2d CollectionDVLines2d CollectionDVLineStrings2d CollectionDVPoints2d CollectionModelMembers CollectionReference ObjectGraphicMembers CollectionHighlightDrawingViewMembers ObjectModelMembers CollectionDrawingView ObjectDrawingView ObjectApplication ObjectBrokenOutSectionProfiles CollectionCoordinateSystems2d CollectionDraftProfile ObjectCuttingPlanes CollectionDetailEnvelopes CollectionDVArcs2d CollectionDVBSplineCurves2d CollectionDVCircles2d CollectionDVEllipses2d CollectionDVEllipticalArcs2d CollectionDVLines2d CollectionDVLineStrings2d CollectionDVPoints2d CollectionModelMembers CollectionReference ObjectGraphicMembers CollectionHighlightDrawingViewMembers ObjectModelMembers CollectionDrawingView Object
Example
Imports System.IO
Imports System.Runtime.InteropServices

Public Class Form1

    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objFolder As DirectoryInfo
        Dim objFileInfo As FileInfo
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing

        Dim objDraftDoc As SolidEdgeDraft.DraftDocument = Nothing
        Dim objSheet As SolidEdgeDraft.Sheet = Nothing
        Dim objDrawingViews As SolidEdgeDraft.DrawingViews = Nothing
        Dim objDrawingView As SolidEdgeDraft.DrawingView = Nothing

        Dim CPLs As SolidEdgeDraft.CuttingPlanes
        Dim CPL As SolidEdgeDraft.CuttingPlane
        Dim sectionView As SolidEdgeDraft.DrawingView
        Dim draftProfile As SolidEdgeDraft.DraftProfile
        Dim xmin, ymin, xmax, ymax As Double
        Dim xhalf As Double
        Try


            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            If objApplication Is Nothing Then
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
                objApplication.Visible = True

            End If
            objFolder = GetTrainingFolder()
            objFileInfo = New FileInfo(Path.Combine(objFolder.FullName, "sbddaan.dft"))
            objDocuments = objApplication.Documents
            objDraftDoc = objDocuments.Open(objFileInfo.FullName)

            'objDraftDoc = objApplication.ActiveDocument
            objSheet = objDraftDoc.ActiveSheet
            objDrawingViews = objSheet.DrawingViews
            objDrawingView = objDrawingViews.Item(1)


            CPLs = objDrawingView.CuttingPlanes
            CPL = CPLs.Add()
            CPL = CPLs.Item(1)
            'User can get position of multisegment section line by using profile
            draftProfile = CPL.Profile

            draftProfile.BeginEdit()

            objDrawingView.Range(xmin, ymin, xmax, ymax)

            xhalf = xmin + (xmax - xmin) / 2
            ymax += 0.01
            ymin -= 0.01

            draftProfile.Lines2d.AddBy2Points(xhalf, ymax, xhalf, ymin)

            If (Not SolidEdgeDraft.ProfileValidationStatus.igProfileStatusValid =
                draftProfile.Validate()) Then

            End If

            draftProfile.EndEdit()

            CPL.ViewSide = SolidEdgeFramework.SectionViewProfileSide.igRightProfileSide
            'User can set the active segment by using FoldSegment API
            CPL.FoldSegment = draftProfile.Lines2d.Count


            sectionView = CPL.CreateView()
            sectionView.Update()
        Catch ex As Exception
            MessageBox.Show(ex.ToString)
        End Try

    End Sub
    Function GetTrainingFolder() As DirectoryInfo
        Dim objInstallData As SEInstallDataLib.SEInstallData = Nothing
        Dim objInstallFolder As DirectoryInfo = Nothing
        Dim objTrainingFolder As DirectoryInfo = Nothing

        Try
            objInstallData = New SEInstallDataLib.SEInstallData
            objInstallFolder = New DirectoryInfo(objInstallData.GetInstalledPath())
            objTrainingFolder = New DirectoryInfo(Path.Combine(objInstallFolder.Parent.FullName, "Training"))
        Catch
        Finally
            If Not (objInstallData Is Nothing) Then
                Marshal.FinalReleaseComObject(objInstallData)
                objInstallData = Nothing
            End If
        End Try

        Return objTrainingFolder
    End Function


End Class
See Also

CuttingPlane Members  | Solid Edge V19 - What's New  | Solid Edge V18 SP7 - What's New