Solid Edge Draft Type Library
TerminatorRatio Property
Description
Sets and returns the terminator ratio for the active ViewPlane object.
Property type
Read-write property
Syntax
Visual Basic
Public Property TerminatorRatio As Double
Remarks
The default ratio is two times the length of the drawing view terminator.
See Also

CuttingPlane Object  | CuttingPlane Members  | Solid Edge V19 - What's New  | Solid Edge V18 SP7 - What's New