Solid Edge Draft Type Library
Depth Property
Description
Returns or sets the depth of the section from the front of the view.
Property type
Read-write property
Syntax
Visual Basic
Public Property Depth As Double
Remarks
This property sets or returns the depth of the broken out section. There will be a default value to allow the broken out section to be applied, but it will not be of much use.
See Also

BrokenOutSectionProfile Object  | BrokenOutSectionProfile Members