Solid Edge Draft Type Library : BrokenOutSectionProfile Object |
Application | Returns the active application object. |
Depth | Returns or sets the depth of the section from the front of the view. |
DepthPlaneOffset | Returns or sets the offset of the depth plane of the section relative to the model origin along the drawing view vector. |
Layer | Sets and returns the named layer on which the referenced object resides. |
Parent | Returns the parent object for the referenced object. |
Profile | Returns the profile associated with the parent object. |
TargetView | Returns or sets the target view associated with the broken out section profile. |