Solid Edge Assembly Type Library
PublishPath Property
Description
Specify or retrieve the path to the directory in which to create the document file when the Virtual Component is published.
Property type
Read-write property
Syntax
Visual Basic
Public Property PublishPath As String
See Also

VirtualComponent Object  | VirtualComponent Members  | Solid Edge V17 - What's New