Solid Edge Assembly Type Library
ReturnOccurrenceForGivenSectionID Method
Description
Syntax
Visual Basic
Public Sub ReturnOccurrenceForGivenSectionID( _
   ByVal SectionId As Long, _
   Optional ByRef OccurrenceId As Variant, _
   Optional ByRef OccurrenceAsObject As Variant _
) 
Parameters
SectionId
OccurrenceId
OccurrenceAsObject
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objAssemblyDocument As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objStructuralFrames As SolidEdgeAssembly.StructuralFrames = Nothing
        Dim objStructuralFrame As SolidEdgeAssembly.StructuralFrame = Nothing
        Dim objOccurrences As SolidEdgeAssembly.Occurrences = Nothing
        Dim objOccurrence As SolidEdgeAssembly.Occurrence = Nothing
        Dim aSections As Array = Array.CreateInstance(GetType(Int32), 1)
        Dim numSections As Integer
        Dim occurrenceId As Integer
        Dim i As Integer

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objAssemblyDocument = objApplication.ActiveDocument
            objStructuralFrames = objAssemblyDocument.StructuralFrames
            objoccurrences = objAssemblyDocument.Occurrences
            objOccurrence = objoccurrences.Item(1)

            ' Loop through all of the structural frames.
            For Each objStructuralFrame In objStructuralFrames
                numSections = 0
                aSections = Array.CreateInstance(GetType(Int32), 1)
                objStructuralFrame.GetSections(numSections, aSections)

                For i = 0 To numSections - 1
                    occurrenceId = 0
                    ' Get the occurrence for this section
                    objStructuralFrame.ReturnOccurrenceForGivenSectionID(aSections(i), occurrenceId, objOccurrence)
                Next
            Next

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

StructuralFrame Object  | StructuralFrame Members  | Solid Edge V20 - What's New  | Solid Edge V19 SP3 - What's New  | Solid Edge V18 SP10 - What's New