Solid Edge Assembly Type Library : Splice Object |
AddConductors | |
CreatePhysicalConductor | |
Delete | |
DeletePhysicalConductor | |
Edit | |
GetConductors | |
GetOuterConductors | |
GetSplicePosition | |
GetTopMostConductors | |
Remove |
Application | Returns the active application object. |
AssemblyProperty | |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
Color | |
Description | |
Gage | |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
Material | |
MaterialType | |
Name | |
OuterDiameter | |
Parent | Returns the parent object for the referenced object. |
PartNumber | |
Type | |
Visible | Specifies whether or not the referenced object is displayed to the screen. |