Solid Edge Assembly Type Library
FileMissing Method
Description
This method will check if the particular file is missing or not.
Syntax
Visual Basic
Public Function FileMissing() As Boolean
Example
Imports System.Runtime.InteropServices
Imports System.IO
Public Class Form1

    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
        Dim objSEApplication As SolidEdgeFramework.Application = Nothing
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing
        Dim objAssemblyDoc As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objPart As SolidEdgeAssembly.Occurrence = Nothing
        Dim objSubOcc As SolidEdgeAssembly.SubOccurrence = Nothing
        Dim bFileMissingArray() As Boolean
        Dim objFolder As DirectoryInfo
        Dim objFileInfo As FileInfo
        Dim index As Integer
        Dim i As Integer

        Try
            objFolder = GetTrainingFolder()
            objFileInfo = New FileInfo(Path.Combine(objFolder.FullName, "Coffee Pot.asm"))

            objSEApplication = Marshal.GetActiveObject("SolidEdge.Application")
            If objSEApplication Is Nothing Then
                objSEApplication = Activator.CreateInstance(Type.GetTypeFromProgID("SolidEdge.Application"))
                objSEApplication.Visible = True
            End If

            objDocuments = objSEApplication.Documents
            ' opening an existing assembly file.
            objAssemblyDoc = objDocuments.Open(objFileInfo.FullName)

            ReDim bFileMissingArray(objAssemblyDoc.Occurrences.Count + 1)
            ' getting a part in the assembly
            For index = 1 To objAssemblyDoc.Occurrences.Count
                objPart = objAssemblyDoc.Occurrences.Item(index)
                bFileMissingArray(index - 1) = objPart.FileMissing
                If (objPart.Type = SolidEdgeFramework.ObjectType.igSubAssembly) Then
                    For i = 1 To objPart.SubOccurrences.Count
                        objSubOcc = objPart.SubOccurrences.Item(i)
                        bFileMissingArray(index + i - 1) = objSubOcc.FileMissing
                    Next i
                End If
            Next index

        Catch ex As Exception
            MessageBox.Show(ex.ToString)
        End Try
    End Sub
    Function GetTrainingFolder() As DirectoryInfo
        Dim objInstallData As SEInstallDataLib.SEInstallData = Nothing
        Dim objInstallFolder As DirectoryInfo = Nothing
        Dim objTrainingFolder As DirectoryInfo = Nothing

        Try
            objInstallData = New SEInstallDataLib.SEInstallData
            objInstallFolder = New DirectoryInfo(objInstallData.GetInstalledPath())
            objTrainingFolder = New DirectoryInfo(Path.Combine(objInstallFolder.Parent.FullName, "Training"))
        Catch
        Finally
            If Not (objInstallData Is Nothing) Then
                Marshal.FinalReleaseComObject(objInstallData)
                objInstallData = Nothing
            End If
        End Try

        Return objTrainingFolder
    End Function

End Class
See Also

Occurrence Object  | Occurrence Members