Solid Edge Assembly Type Library
DeleteHoleLocation Method
Description
Deletes the construction surfaces from the frame.
Syntax
Visual Basic
Public Sub DeleteHoleLocation() 
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objAssemblyDocument As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objOccurrences As SolidEdgeAssembly.Occurrences = Nothing
        Dim objOccurrence As SolidEdgeAssembly.Occurrence = Nothing

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objAssemblyDocument = objApplication.ActiveDocument
            objOccurrences = objAssemblyDocument.Occurrences

            For Each objOccurrence In objOccurrences
                objOccurrence.RetrieveHoleLocation()
                objOccurrence.DeleteHoleLocation()
            Next

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Occurrence Object  | Occurrence Members  | Solid Edge ST3 - What's New