Solid Edge Assembly Type Library
SaveAsEcad Method
Description
Saves wire harness component and connection list files for input to an Ecad system
Syntax
Visual Basic
Public Sub SaveAsEcad( _
   ByRef HarnessSaveAsEcadStatus As HarnessSaveAsEcadStatusConstants, _
   ByVal CompanyName As String, _
   Optional ByVal ComponentFilePath As Variant, _
   Optional ByVal ConnectionFilePath As Variant _
) 
Parameters
HarnessSaveAsEcadStatus
ValueDescription
seHarnessSaveAsEcadStatus_FailedThe Save As ECAD operation has failed.
seHarnessSaveAsEcadStatus_FailedBadArgsThe Save As ECAD operation has failed. The SaveAsEcad api argument list is invalid.
seHarnessSaveAsEcadStatus_FailedBadConfigThe Save As ECAD operation has failed. The document format is invalid.
seHarnessSaveAsEcadStatus_FailedBothThe Save As ECAD operation has failed. The component and connection document will not be created.
seHarnessSaveAsEcadStatus_FailedCompsThe Save As ECAD operation has failed. A component document will not be created.
seHarnessSaveAsEcadStatus_FailedConnsThe Save As ECAD operation has failed. A connection document will not be created.
seHarnessSaveAsEcadStatus_FailedDupCompsThis harness contains duplicate components. The component and connection document will not be created.
seHarnessSaveAsEcadStatus_FailedDupConnsThis harness contains duplicate connections. A connection document will not be created.
seHarnessSaveAsEcadStatus_FailedNoCompsThis harness contains no components. A component document will not be created.
seHarnessSaveAsEcadStatus_FailedNoConnsThis harness contains no connections. A connection document will not be created.
seHarnessSaveAsEcadStatus_SuccessThe input documents for the ECAD system have been successfully generated.
CompanyName
ComponentFilePath
ConnectionFilePath
See Also

Harness Object  | Harness Members  | Solid Edge V18 - What's New