Solid Edge Assembly Type Library
EndOffset Property
Description
Sets and returns the length of material to remove from the end of the weld bead for the referenced AssemblyStitchWeld object.
Property type
Read-write property
Syntax
Visual Basic
Public Property EndOffset As Double
Remarks
This property modifies the computed length of the bead, but does not modify the weld symbol attributes.
See Also

AssemblyStitchWeld Object  | AssemblyStitchWeld Members  | Solid Edge V18 - What's New