Solid Edge Assembly Type Library
AssemblyFilletWeld Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method GoTo
Public Method RangeReturns the high and low range values for the referenced object.
Public Method RecomputeRecalculates the referenced object.
Public Properties
Public Property Application
Public Property BaseThickness
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. The result of the Edges property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object. The result of the Faces property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property NameReturns the name of the referenced object.
Public Property Parent
Public Property SetBackType
Public Property SuppressTemporarily suppresses the referenced object.
Public Property TargetThickness
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
See Also

AssemblyFilletWeld Object  | Solid Edge V18 - What's New