Solid Edge Assembly Type Library
AssemblyFeaturesSweptProtrusion Object Members
Overview 
Public Methods
Public Method DeleteDeletes the referenced object.
Public Method RangeReturns the high and low range values for the referenced object.
Public Method RollToFeatureThis method rolls the referenced object back to a specified feature.
Public Properties
Public Property Application
Public Property EdgesReturns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. The result of the Edges property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used.
Public Property FacesReturns a collection of faces of a specified type that belong to a model, a feature, or a topology object. The result of the Faces property is a topology collection. This topology collection is a temporary collection and is overwritten the next time the Edges, Faces, or FacesByRay property is used.
Public Property FacesByRayReturns a collection of faces that are intersected by a specified vector.
Public Property NameReturns the name of the referenced object.
Public Property Parent
Public Property SuppressTemporarily suppresses the referenced object.
See Also

AssemblyFeaturesSweptProtrusion Object  | Solid Edge V18 - What's New