Solid Edge Assembly Type Library
FacesByRayForScopePart Property
Description
Property type
Read-only property
Syntax
Visual Basic
Public Property FacesByRayForScopePart( _
   ByVal ScopePart As Unknown, _
   ByVal Xorigin As Double, _
   ByVal Yorigin As Double, _
   ByVal Zorigin As Double, _
   ByVal Xdir As Double, _
   ByVal Ydir As Double, _
   ByVal Zdir As Double _
) As Object
Parameters
ScopePart
Xorigin
Yorigin
Zorigin
Xdir
Ydir
Zdir
See Also

AssemblyFeaturesRevolvedCutout Object  | AssemblyFeaturesRevolvedCutout Members  | Solid Edge V20 - What's New