Private Sub Form_Load()
Dim objApp As solidedgeFramework.Application
Dim objDoc As solidedgeAssembly.AssemblyDocument
Const TESTFILE = "T:\vbtests\testcases\sample.asm"
Dim sPath As String
' Report errors
Const PI = 3.14159265358979
' Create/get the application with specific settings
On Error Resume Next
Set objApp = GetObject(, "SolidEdge.Application")
If Err Then
Err.Clear
Set objApp = CreateObject("SolidEdge.Application")
Set objDoc = objApp.Documents.Add("SolidEdge.AssemblyDocument")
objApp.Visible = True
Else
Set objDoc = objApp.ActiveDocument
End If
' Clsoe the Active document
Call objDoc.Close
' Opening the test case file
Set objDoc = objApp.Documents.Open(TESTFILE)
' Getting the Path property of the AssemblyDocument object.
sPath = objDoc.Path
' USER DISPLAY
' Release objects
Set objApp = Nothing
Set objDoc = Nothing
End Sub