Solid Edge Assembly Type Library
NewNavigatorWindow Method
Collapse All
Expand All
Solid Edge Assembly Type Library
>
AssemblyDocument Object
: NewNavigatorWindow Method
Description
creates a Pathfinder window for the referenced AssemblyDocument object.
Syntax
Visual Basic
Public Sub NewNavigatorWindow()
Remarks
This is a defunct API to create the old Pathfinder view. It will return an error when called and is of no use to the developer.
See Also
AssemblyDocument Object
|
AssemblyDocument Members