Solid Edge Assembly Type Library
InquireElement Method
Specify the first element to be inquired.
Returns surface area if applicable.
Returns volume if applicable.
Returns length if applicable.
Description
Gives information about elements.
Syntax
Visual Basic
Public Sub InquireElement( _
   ByVal Element As Object, _
   ByRef InPoint() As Double, _
   ByVal CoordinateSystem As Variant, _
   ByRef Point() As Double, _
   ByRef SurfaceArea As Double, _
   ByRef Volume As Double, _
   ByRef Length As Double _
) 
Parameters
Element
Specify the first element to be inquired.
InPoint
CoordinateSystem
Point
SurfaceArea
Returns surface area if applicable.
Volume
Returns volume if applicable.
Length
Returns length if applicable.
Example
Imports System.IO
Imports System.Runtime.InteropServices
Public Class Form1

    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
        Dim objApp As SolidEdgeFramework.Application = Nothing
        Dim objAssemblyDoc As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing
        Dim objFolder As DirectoryInfo
        Dim objFileInfo As FileInfo
        Dim objFace1 As SolidEdgeGeometry.Face
        Dim objFace2 As SolidEdgeGeometry.Face
        Dim dblPoint1(0) As Double
        Dim dblPoint2(0) As Double
        Dim dblPoint3(0) As Double
        Dim distance As Double
        Dim dx As Double
        Dim dy As Double
        Dim dz As Double
        Dim dgoem(2) As Double
        Dim featedges As SolidEdgeGeometry.Edges
        Dim featedge1 As SolidEdgeGeometry.Edge
        Dim featedge2 As SolidEdgeGeometry.Edge
        Dim featedge3 As SolidEdgeGeometry.Edge
        Dim strRetStatusMsg As String
        strRetStatusMsg = ""
        Dim angle1 As Double
        Dim angle2 As Double
        Dim angle3 As Double
        Dim angle4 As Double
        Dim SurfArea As Double
        Dim Volume As Double
        Dim Length As Double
        Dim coSyss As SolidEdgePart.CoordinateSystem
        Dim objRef1 As Object
        Dim objRef2 As Object
        Dim objRef3 As Object
        Dim objRef4 As Object

        dgoem(0) = 0
        dgoem(1) = 0
        dgoem(2) = 0

        Try

            objApp = Marshal.GetActiveObject("SolidEdge.Application")
            objFolder = GetTrainingFolder()
            objFileInfo = New FileInfo(Path.Combine(objFolder.FullName, "carrier.asm"))
            objDocuments = objApp.Documents
            objAssemblyDoc = objDocuments.Open(objFileInfo.FullName)


            objFace1 = objAssemblyDoc.Occurrences.Item(1).OccurrenceDocument.Models.Item(1).ExtrudedProtrusions.Item(1).Faces(SolidEdgeGeometry.FeatureTopologyQueryTypeConstants.igQueryAll).Item(3)
            objFace2 = objAssemblyDoc.Occurrences.Item(1).OccurrenceDocument.Models.Item(1).ExtrudedProtrusions.Item(1).Faces(SolidEdgeGeometry.FeatureTopologyQueryTypeConstants.igQueryAll).Item(4)

            objRef1 = objAssemblyDoc.CreateReference(objAssemblyDoc.Occurrences(0), objFace1)
            objRef2 = objAssemblyDoc.CreateReference(objAssemblyDoc.Occurrences(0), objFace2)

            Call objAssemblyDoc.MeasureDistance(objRef1, objRef2, SolidEdgePart.MeasureDistanceTypeConstants.MeasureDistanceTypeConstants_MaximumDistance, distance, dx, dy, dz, dblPoint1, dblPoint2)

            MsgBox("Distance between the elements is " + distance.ToString)

            featedges = objAssemblyDoc.Occurrences.Item(1).OccurrenceDocument.Models.Item(1).ExtrudedProtrusions.Item(1).Edges(SolidEdgeConstants.FeatureTopologyQueryTypeConstants.igQueryAll)
            featedge1 = featedges.Item(1)
            featedge2 = featedges.Item(2)
            featedge3 = featedges.Item(3)

            objRef3 = objAssemblyDoc.CreateReference(objAssemblyDoc.Occurrences(0), featedge1)
            objRef4 = objAssemblyDoc.CreateReference(objAssemblyDoc.Occurrences(0), featedge2)

            Call objAssemblyDoc.MeasureAngleEx(objRef3, objRef4, Nothing, angle1, angle2, angle3, angle4)

            MsgBox("Angle between the edges is " + Math.Round(RadiansToDegrees(angle1)).ToString + " degrees")

            Call objAssemblyDoc.InquireElement(objRef3, dgoem, Nothing, dblPoint1, SurfArea, Volume, Length)

            coSyss = objAssemblyDoc.CoordinateSystems.Item(1)

            Call objAssemblyDoc.InquireElement(objRef3, dblPoint2, coSyss, dblPoint3, SurfArea, Volume, Length)
            MsgBox("Length of Inquired Element is " + Length.ToString)

        Catch ex As Exception
            MessageBox.Show(ex.ToString)
            Clipboard.SetText(ex.ToString)
        End Try

    End Sub

    Private Function RadiansToDegrees(ByVal radians As Double) As Double
        Return radians * (180 / Math.PI)
    End Function

    Function GetTrainingFolder() As DirectoryInfo
        Dim objInstallData As SEInstallDataLib.SEInstallData = Nothing
        Dim objInstallFolder As DirectoryInfo = Nothing
        Dim objTrainingFolder As DirectoryInfo = Nothing

        Try
            objInstallData = New SEInstallDataLib.SEInstallData
            objInstallFolder = New DirectoryInfo(objInstallData.GetInstalledPath())
            objTrainingFolder = New DirectoryInfo(Path.Combine(objInstallFolder.Parent.FullName, "Training"))
        Catch
        Finally
            If Not (objInstallData Is Nothing) Then
                Marshal.FinalReleaseComObject(objInstallData)
                objInstallData = Nothing
            End If
        End Try

        Return objTrainingFolder
    End Function
End Class
See Also

AssemblyDocument Object  | AssemblyDocument Members