You will learn how to: |
|
|
Step |
Summary |
|
---|---|---|
1. |
Assign fatigue material properties. |
The material assigned to the part of the model where you perform the durability analysis must have the appropriate durability and fatigue material properties. If you do not assign fatigue material properties, you can override the referenced material when you create durability events. |
2. |
Create and solve the structural analysis solution. |
The type of structural analysis solution that you create determines the type of events you can create during the durability analysis. Because the results file needs to contain either stress or strain result sets for performing the durability analysis, you must specify either stress or strain results in the output requests. |
3. |
Create the Durability solution process. |
A Durability solution process can contain multiple static and transient events. |
4. |
Create durability objects. |
Durability objects define durability solver settings that this software uses when solving durability events. Because you can reuse durability objects in different durability events, you can define durability solver settings once, and use them in multiple events. |
5. |
Create events. |
Depending on the structural analysis solution, you can create static events or transient events. For each event, you specify the following:
In the case of a transient event, you also specify the part of your loading history on which you perform the durability analysis. You can select only a portion of your model to perform the durability analysis. You can override the material specified in the file for either of the following reasons:
|
6. |
Solve for durability analysis results. |
You can solve each event and the durability solution process separately, or you can solve the durability solution process and all events at the same time. The durability solution process results cumulate damage and life results from all the active static and transient events. Worst case safety factors are taken from all active events. |
7. |
Post process durability analysis results. |
You can view the results you requested for each event separately and cumulatively under the durability result node in the Post Processing Navigator. |
On your desktop or the appropriate network drive, create a folder named durability_muffler.
Click the link below:
Extract the part files to your durability_muffler folder.
Start Simcenter 3D.
File |
Open
Look in |
durability_muffler |
Files of type |
Simulation Files (*.sim) |
File name |
muffler_sim.sim |
OK |
|
The following nodes are created in the Simulation Navigator.
muffler_sim.sim |
muffler_fem.fem |
CSYS |
Selection Recipes |
Groups |
Fields |
Modeling Objects |
Regions |
Simulation Object Container |
Constraint Container |
Load Container |
Solver Sets |
Static Solution |
Transient Solution |
Temperatures |
Simulation Objects |
Constraints |
Subcase - Direct Transient 1 |
Loads |
Results |
Structural |
The options you select in dialog boxes are preserved for the next time you open the same dialog box within a given session. Restore the default settings to ensure that the dialog boxes are in the expected initial state for each step of the activity.
File |
Preferences→User Interface
Options |
Reset Dialog Memory
OK |
|
The durability solver can compute results only when the appropriate material properties are set.
Manage Materials (Home tab→Properties group)
Materials |
|
Aluminum_2014 |
Inspect
The Isotropic Material dialog box opens.
Strength |
Examine the Yield Strength and Ultimate Tensile Strength values.
These properties are used to evaluate the static strength safety factors and margins of safety. You can display the property values as functions of temperature. The yield strength of Aluminum_2014 at 20°C is 394 MPa.
Durability |
Examine the values in the Fatigue Strength, Fatigue Ductility, and Cyclic Parameters groups.
The Fatigue Strength Coefficient and Fatigue Strength Exponent values are used to evaluate high-cycle and low-cycle fatigue results.
The Fatigue Ductility Coefficient and Fatigue Ductility Exponent values are used to evaluate low-cycle fatigue results.
The Cyclic Yield Strength, Cyclic Strength Coefficient, and Cyclic Strain Hardening Exponent values are used in constitutive relationships to convert between stress cycles and strain cycles while computing fatigue damage and fatigue life results.
Close |
both dialog boxes |
In the Simulation Navigator, observe the following nodes:
Static Solution — This is the node for the Simcenter Nastran SOL 101 Linear Statics – Global Constraints solution that will be referenced by the static durability event.
Transient Solution — This is the node for the Simcenter Nastran SOL 109 Direct Transient Response solution that will be referenced by the transient durability event.
Static Solution |
Transient Solution |
Temperatures |
Simulation Objects |
Constraints |
Subcase - Direct Transient 1 |
Loads |
Results |
Structural |
Simulation Navigator
Static Solution
Results (under Static Solution)
Post Processing Navigator
Examine the stress results of the Static Solution.
Structural→Stress - Elemental
Von-Mises
Notice that the maximum stress of Static Solution (~528 MPa) is higher than the material yield strength. Therefore, the Smith–Watson–Topper fatigue life criterion will be used for the static durability event that references results from this solution. This criterion needs both stress and strain results and is typically used for low cycle fatigue analysis.
Load the Transient Solution results.
Structural (under Transient Solution)
Animate the stress results of the Transient Solution over all iterations.
Notice that when the stress results of Transient Solution are animated over all iterations the maximum value (~280 MPa) is lower than the material yield strength. Therefore, the stress life criterion will be used for the transient durability event that references results from this Response Dynamics solution process. This criterion is typically used for high cycle fatigue analysis.
Return to Home (Context group)
If necessary, right-click in the Ribbon bar and turn the Durability tab on.
Durability |
New Durability Simulation (Durability group)
OK |
Durability dialog box |
The Durability 1 node is created in the Simulation Navigator.
Durability 1 |
The Durability 1 solution process node will contain both a static event and a transient event that you will create.
The strength durability object defines requests for stress criterion, stress type, and strength output. Both the static and the transient event will use the same strength durability object.
Manage Durability Objects (Durability group)
Edit
Yield Stress (under Stress Criterion group)
Verify that Stress Type is set to Von Mises.
Margin of Safety
Because you want to maximize strength output, you request both the strength safety factor and margin of safety results.
Factor of Safety |
1.2 |
OK |
Strength dialog box |
Do not leave the Durability Object Manager dialog box.
The fatigue durability object defines fatigue life settings, fatigue life output requests, fatigue safety factor settings, and fatigue safety factor output requests. The static event will use the fatigue durability object called fatigue static and the transient event will use the object called fatigue transient.
Object Type |
Fatigue |
Edit
Name |
Fatigue static |
Number Of Occurrences |
1e5 |
Verify that Fatigue Life Criterion is set to Smith Watson Topper.
The Smith-Watson-Topper fatigue life criterion uses a strain life approach and solicits both the stress and strain results from the Static Solution solution.
Fatigue Life Output |
|
Event Damage
Fatigue Safety Factor |
|
Failure Index
OK |
Fatigue dialog box |
Clone
Edit
Name |
Fatigue transient |
Number of Occurrences |
1e9 |
Fatigue Life Criterion |
Stress Life |
The stress life criterion is selected because the Transient Solution stress results are in the linear elastic range and because a high number of occurrences (109) is specified.
OK |
Fatigue dialog box |
Do not leave the Durability Object Manager dialog box.
The axis search durability object defines how the durability solver determines:
The critical loading path of the structure.
The most likely direction along which cracks could form and propagate.
Because fatigue is a surface phenomenon, damage values are calculated only on the free faces of elements and the plane stress assumption is used.
The static event will use the axis search durability object called axis search static and the transient event will use the axis search durability object called axis search transient.
Object Type |
Axis Search |
Edit
Name |
Axis Search static |
Element Face Stress Axis |
Bi-Axial |
When you set the Element Face Stress Axis to Bi-Axial, the forces acting perpendicularly to the crack propagation direction contribute to the calculation of crack growth.
OK |
Axis Search dialog box |
Clone
Edit
Name |
Axis Search transient |
Maximum Damage (under Stress Axis Direction Search Method)
When you select the maximum damage method, the durability solver calculates damage in every direction on element free faces to determine the primary loading direction, its damage, and life values.
Search Resolution |
30 |
OK |
both dialog boxes |
Static Event (Durability group)
The existing static solution Static Solution is detected and selected in the Static Solution List.
Strength |
Strength 1 |
Fatigue |
Fatigue static |
Axis Search |
Axis Search static |
OK |
Static Durability Event dialog box |
As the solve options durability object was not defined, the Solve Options 1 durability object is used. The software creates one durability object of each type with default values when you first open the Durability Object Manager dialog box.
The Static Event 1 node is created in the Simulation Navigator.
Durability 1 |
Static Event 1 |
Simulation Navigator
Static Event 1
New Excitation
Pattern Name |
ForceExt+Z |
Subcase 1 |
Full Unit Cycle
OK |
Load Pattern dialog box |
The ForceExt+Z node is created in the Simulation Navigator under the Static Event 1 node.
Durability 1 |
Static Event 1 |
ForceExt+Z |
Transient Event (Durability group)
The existing transient solution Transient Solution–SOL 109 is detected and selected in the Transient Solution List.
The existing subcase Subcase – Direct Transient 1 is detected and selected in the Transient Solution Subcase List.
Strength |
Strength 1 |
Fatigue |
Fatigue transient |
Axis Search |
Axis Search transient |
Data Control |
Verify that the Decimation Order is set to 1.
The decimation order value controls the number of stress/strain data points that are used in the durability evaluation. The default decimation order of 1 means that every data point is used; a value of 2 means that every other point is used.
Solve Options |
Create Solve Options
Name |
Solve Options transient |
Select (under Use Elements)
Method (Top Border bar) |
Elements by Group |
any element that is on the face shown.
1721 elements are selected. These elements are in the Joint group.
OK |
both dialog boxes |
The Transient Event 1 node is created in the Simulation Navigator.
Durability 1 |
Static Event 1 |
ForceExt+Z |
Transient Event 1 |
Solve Durability Simulation (Durability group)
OK |
Durability Solver dialog box |
Wait for the job to finish. This could take a couple of minutes.
the Information window
The following three result nodes are created in the Simulation Navigator.
Durability 1 |
Static Event 1 |
ForceExt+Z |
Static Event 1 |
Transient Event 1 |
Transient Event 1 |
Durability 1 |
The Static Event 1 result node contains the set of results you specified in the Static Durability Event dialog box.
The Transient Event 1 result node contains the set of results you specified in the Transient Durability Event dialog box.
The Durability 1 result node contains the set of results that cumulates the results from the two event result sets.
In general, when a Durability solution process contains multiple active events, the durability results are calculated as described in the following table.
Cumulative durability results set |
Values calculated |
Strength Safety Factor |
Minimum value of all events |
Margin of Safety |
Minimum value of all events |
Fatigue Safety Factor |
Minimum value of all events |
Fatigue Failure Index |
Maximum value of all events |
Fatigue Damage |
Algebraic sum of damage due to each event |
Fatigue Life |
Reciprocal of Fatigue Damage value |
Simulation Navigator
Static Event 1
Post Processing Navigator
Static Event 1
The following result nodes are created in the Post Processing Navigator.
Durability 1 |
Durability 1 |
Static Event 1 |
Fatigue Life – Element-Nodal |
Fatigue Damage – Element-Nodal |
Fatigue Safety Factor – Element-Nodal |
Strength Safety Factor – Element-Nodal |
Margin of Safety (%) – Element-Nodal |
Fatigue Failure Index – Element-Nodal |
Transient Event 1 |
You can use the following table as a guide to evaluate the durability results.
Durability results set |
Failure when value is |
Strength Safety Factor |
< 1.0 |
Margin of Safety |
Negative |
Fatigue Safety Factor |
< 1.0 |
Fatigue Failure Index |
> 1.0 |
Fatigue Damage |
> 1.0 |
Fatigue Life |
< 1.0 |
Fatigue Life – Element-Nodal
You will invert the color bar scheme to get a more meaningful representation of fatigue life results.
Results |
Edit Post View (Post View group)
Legend |
Invert Spectrum (Color Control group)
OK |
Post View dialog box |
Post View 2
New Template
Transient Event 1 under Durability 1 node
The Transient Event 1 results are loaded in the Post Processing Navigator.
Transient Event 1
Fatigue Life – Element-Nodal
Post_View_2 under Templates node
The durability results of the Transient Event 1 result sets are only computed on the elements that are in the Joint group.
Durability 1
The Durability 1 results are loaded in the Post Processing Navigator.
Durability 1 |
Durability 1
Fatigue Life – Element-Nodal
Post_View_2 under Templates node
Notice that for each result set, some regions of the muffler have fatigue life results that are less than one. Therefore, further analysis and design changes are required.
Post Processing Navigator
Fatigue Failure Index – Element-Nodal under Transient Event 1 node
Fatigue failure index values should be less than one for the model to withstand the stress history from the transient solution. In this case, some elements have fatigue failure index values that are greater than one. Therefore, further analysis and design changes are required.
Examine other durability result sets.
Modify your model to withstand the provided stress histories.
Save and close your files when you are finished.
File |
Save→Save All
File |
Close→All Parts