In this tutorial, you will use basic geometry idealization and abstraction commands to simplify a model in preparation for meshing. You will use the Split Body command to partition the model and then remove features from the geometry, including edge blends and a slot that are not significant to the analysis.
Before starting the tutorial, you must download the part.
On your desktop or the appropriate network drive, create a folder named geometry_cleanup.
Click the link below:
Extract the files to your geometry_cleanup folder.
Start Simcenter 3D or NX.
Open disk_fem1.fem.
The options you select in dialog boxes are preserved for the next time you open the same dialog box within a given session. Restore the default settings to ensure that the dialog boxes are in the expected initial state for each step of the activity.
File |
Preferences→User Interface
Options |
Reset Dialog Memory
OK |
|
You can remove sliver surfaces, along with features such as fillets, in preparation for a finite element mesh. You perform this idealization on the idealized part, which is an assembly instance of your master part. You do not make these changes directly on the master part.
Simulation Navigator
disk_fem1_i.prt
Load
disk_fem1_i.prt
Make Displayed Part
OK |
Idealized Part Warning |
The warning alerts you to the fact that you must first promote or WAVE-link the body you are working with before you can perform any idealization command.
The idealized part is now displayed in the Simulation Navigator.
Because the disk is symmetrical, you can decrease the solve time by splitting the body and analyzing only half of it. For simplicity, we are splitting the body in half, but you could also split it into quarters for even greater efficiency.
Before you can split the body, you must promote it.
Promote (Home tab→Start group)
the part
OK |
|
Split Body (Geometry Preparation group)
the part
Because there is no partitioning geometry, you will create a datum plane.
Tool Option |
New Plane |
Specify Plane |
XC-ZC Plane |
OK |
|
Hide (Top border bar→Show/Hide Drop-down list)
the left half of the disk
OK |
|
The edge blends on your part are not significant to your analysis, so you will remove them.
Delete Face (Synchronous Modeling group)
OK |
|
The edges of the part are now sharp.
You will examine the geometry for tiny surfaces that may cause meshing problems.
Menu |
Analysis→Examine Geometry
Drag a box around the entire part.
Object Checks / Post Check Status |
|
Tiny
Check Criteria |
|
Distance |
3.0 |
For this analysis, you can assume a “tiny” surface to be about 1/100 of the radius of the disk. The overall radius of the disk is 270 mm, so 3 mm is a good value to use.
Angle |
0.5 |
Examine Geometry |
|
The entire part is highlighted and the Highlight Results check box appears under the Object Checks / Post Check Status group.
Highlight Results
Note the tiny slot that is highlighted on the bottom face of the part (zoom in on the slot if necessary).
Close |
|
Refresh (graphics window)
The disk is supported by the small slot around the outside edge. The slot is needed for a boundary condition, but it will interfere with meshing. You will remove the slot and replace it with an edge to which you can later assign the boundary condition.
Delete Face (Synchronous Modeling group)
Type |
Face |
Face Rule (Top Border bar) |
Slot Faces |
any face in the slot; zoom in if necessary
OK |
|
The slot is removed.
Simulation Navigator
Simulation File View |
|
disk_fem1
Make Displayed Part
the Information window
The FEM file is now displayed in the Simulation Navigator. It is also the work part.
In the FEM file, you can use abstraction tools to further prepare your part for meshing. You will suppress an edge that will distort elements created along the curved face.
Merge Face (Polygon Geometry group)
OK |
|
Mesh collectors let you organize your model by grouping your meshes logically. Each mesh collector references a physical property table. They are especially valuable when working with complex, non-homogenous models because you can use them to control the mesh display properties, such as element color, shrink percentage, and so on.
Mesh Collector (Properties group)
Element Family |
3D |
Name |
Polycarb |
Create Physical (Solid)
Choose material (Material)
Materials |
|
Polycarbonate |
OK |
all dialog boxes |
You are now ready to mesh the part.
3D Tetrahedral (Mesh group)
the part
Type |
CTETRA(10) |
Automatic Element Size (Element Size)
Clicking this button calculates the element length based on the geometry you selected.
Destination Collector |
|
Automatic Creation
Mesh Collector |
Polycarb |
This is the mesh collector you created in the previous step.
OK |
|
Save
At this point, you could add loads and constraints, solve the model, and display results.
File |
Close→All Parts