In this tutorial, you will define a material property using a table field.
Start Simcenter 3D or NX.
File |
New
Model |
Templates |
|
Units |
Inches |
Model |
Modeling |
Inches |
Make sure that you use inches as the units.
Name |
nl_material.prt |
Folder |
your part file folder name |
OK |
The options you select in dialog boxes are preserved for the next time you open the same dialog box within a given session. Restore the default settings to ensure that the dialog boxes are in the expected initial state for each step of the activity.
File |
Preferences→User Interface
Options |
Reset Dialog Memory
OK |
|
Create a five-inch-long block with a one-inch square cross section.
Block (Home tab→Feature group→More list)
Block is visible only when Role is set to Advanced.
Type |
Origin and Edge Lengths |
the origin of the work coordinate system (WCS)
Length (XC) |
1 |
Width (YC) |
5 |
Height (ZC) |
1 |
OK |
|
File |
All Applications→Pre/Post
Simulation Navigator
nl_material.prt
New FEM and Simulation
Solver |
Simcenter Nastran |
Analysis Type |
Structural |
OK |
New FEM and Simulation dialog box |
Name |
Material Nonlinear |
Solution Type |
SOL 106 Nonlinear Statics – Global Constraints |
Case Control |
Edit (Nonlinear Parameters)
Number of Increments |
20 |
OK |
all dialog boxes |
Save
Manage Materials (Properties group)
Materials |
|
Steel |
Copy
(Young’s Modulus (E))
Make Formula
fd(“Young’s Modulus (E)”)
You will replace the formula name with a constant value.
Young's Modulus (E) |
26.9E6 lbf/in² |
Make sure that you change the units to lbf/in².
(Poisson’s Ratio (NU))
Make Formula
fd(“Poisson’s Ratio(NU)”)
Poisson's Ratio (NU) |
0.3 |
Stress-Strain Related Properties |
|
(Stress-Strain (H))
New Field→Table
Independent |
Strain |
Data Points |
|
0,0 |
Type this value in the unlabeled box at the bottom of the group.
Accept Edit
Type the remaining values for the table, as listed below. Use commas or spaces to separate values in a row, and use semicolons to separate rows. Click Accept Edit to add values to the table.
OK |
Table Field dialog box |
Initial Yield Point (LIMIT1) |
34970 lbf/in² |
Make sure that the units are lbf/in².
OK |
Isotropic Material dialog box |
Materials |
|
Steel_1 |
Rename
Name |
Strain Hardening Steel |
Enter |
|
Close |
Manage Materials dialog box |
Save
At this point, you could mesh the part, add constraints, add a pressure load, use subcases to control load steps, and solve the model.
File |
Close→All Parts