In this tutorial, you will assign material and physical properties to a golf club assembly.
On your desktop or the appropriate network drive, create a folder named material_physical.
Click the link below:
Extract the part file to your material_physical folder.
Start Simcenter 3D or NX.
Open Golf_Club_Assem_fem2.fem.
The options you select in dialog boxes are preserved for the next time you open the same dialog box within a given session. Restore the default settings to ensure that the dialog boxes are in the expected initial state for each step of the activity.
File |
Preferences→User Interface
Options |
Reset Dialog Memory
OK |
|
Create a new material, Graphite, by copying and editing the Nylon material record.
Manage Materials (Properties group)
Materials |
|
Nylon |
Copy
The Isotropic Material dialog box opens.
Name - Description |
Graphite |
Properties |
|
Mass Density |
1.4e-006 kg/mm³ |
Mechanical |
Young's Modulus |
14500 MPa |
Make sure that you change the units to MPa.
Poisson's Ratio |
0.4 |
Strength |
Yield Strength |
110 MPa |
Make sure that you change the units to MPa.
Ultimate Tensile Strength |
165 MPa |
OK |
Isotropic Material dialog box |
Close |
|
Create a 2D mesh collector for the shaft of the club using Graphite as the material.
Mesh Collector (Properties group)
Element Family |
2D |
Collector Type |
ThinShell |
Name |
Shaft graphite |
Create Physical (Shell Property)
Name |
Shaft graphite |
Material 1 |
Graphite |
Default Thickness |
1.5 mm |
OK |
both dialog boxes |
The new collector appears in the Simulation Navigator.
2D Collectors |
Change the display color of the new mesh collector to medium faded red.
Simulation Navigator
2D Collectors
Shaft graphite
Edit Display
Color
Selected Color |
|
ID |
155 |
(Medium Faded Red) |
Enter |
|
OK |
both dialog boxes |
All meshes assigned to a collector inherit the properties of the collector. When you reassign a mesh from one collector to another, the properties of the mesh automatically change to that of the new collector.
Simulation Navigator
2D Collectors→Shaft steel
2d_mesh(1) and drag it from Shaft steel to the Shaft graphite node.
Apply Defaults |
Move Mesh Display Settings box |
ESC |
|
Pressing ESC clears the selection color.
Save
You can zoom in to see that the color of the shaft has changed from gray to red, which is the display color of the Shaft graphite collector.
You can also examine the Simulation Navigator to see that the shaft mesh is now assigned to the Shaft graphite collector.
2D Collectors |
By switching the Simulation Navigator to Material View, you can identify the material assigned to each collector, mesh, and polygon body.
Simulation Navigator
Name (the column title)
Material View
Materials→Polycarbonate→Ferrule
Similarly expand the nodes for Polypropylene, Graphite, Steel, and No Material. You can see that Graphite is now the material associated with the shaft mesh.
Materials |
By expanding the No Material node, you see that materials are not assigned to the polygon bodies. Because each collector has an assigned material and each mesh is assigned to a collector, it is not necessary to have materials assigned to the polygon bodies.
Switch the Simulation Navigator back to Standard View.
Simulation Navigator
Name (the column title)
Standard View
The meshing process is now complete.
Save
File |
Close →All Parts