In this tutorial, you will learn how to use a spatial field to define the thickness of elements.
On your desktop or the appropriate network drive, create a folder named strut3.
Click the link below:
Extract the file to your strut3 folder.
Start Simcenter 3D or NX.
Open strut_fem1.fem.
Load the idealized part file.
strut_fem1_i.prt
Load
The options you select in dialog boxes are preserved for the next time you open the same dialog box within a given session. Restore the default settings to ensure that the dialog boxes are in the expected initial state for each step of the activity.
File |
Preferences→User Interface
Options |
Reset Dialog Memory
OK |
|
In this activity, the provided FEM includes two meshes, 2d_mesh(1) and 2d_mesh(2), that have been copied and translated to create two additional meshes, 2d_mesh(1)_translated(1) and 2d_mesh(2)_translated(1). Because element thickness data is not passed along to copied and translated meshes, you must define the element thickness data for these meshes. To do so, you will:
Create a spatial table field for element thickness from the thickness data for the 2d_mesh(1) and 2d_mesh(2) meshes.
Create a linked field from the spatial table field.
Define the coordinate basis of the linked field to be rotated +30 degrees about the X-axis of the absolute coordinate system.
Assign the linked field as the thickness source for the copied and translated meshes.
In this step, you create the spatial table field for element thickness from the thickness data for the 2d_mesh(1) and 2d_mesh(2) meshes.
Simulation Navigator
2D Collectors→ThinShell(1)
2d_mesh(1)
Thickness Information
Create Thickness Field |
|
Create Field
The status bar lets you know that a field has been successfully created.
Cancel |
|
Simulation Navigator
Fields
Thickness 2d_mesh(1) field
Rename
ribs |
Repeat the preceding steps to create a spatial table field for thickness from 2d_mesh(2). Rename the field strutcase.
In this step, you create linked fields for the spatial table fields and assign them to the copied and translated meshes.
Simulation Navigator
Fields
New Field→Linked
Source Field |
|
ribs |
Spatial Map |
|
Type |
Cartesian |
CSYS Dialog (Specify CSYS)
Type |
Offset CSYS |
Reference |
Absolute - Displayed Part |
Rotation |
|
Angle X |
30 |
OK |
all dialog boxes |
Simulation Navigator
Fields
Link Field
Rename
ribs30 |
Enter |
|
Simulation Navigator
2D Collectors→ThinShell(1)
2d_mesh(1)_translated(1)
Edit Mesh Associated Data
Thickness Source |
Field/Expression |
Select Existing Field (Thickness)
Fields |
|
ribs30 |
OK |
all dialog boxes |
Repeat the preceding steps to create a linked field for strutcase. Rename the new field strutcase30 and assign it to 2d_mesh(2)_translated(1).
Simulation Navigator
2D Collectors→ThinShell(1)
2d_mesh(2)_translated(1)
Edit Display
Element Thickness and Offset
OK |
|
The element thickness defined with a field appears the same as the element thickness defined with the midsurface.
2d_mesh(2)_translated(1)
Edit Display
Element Thickness and Offset
OK |
|
Save
File |
Close→All Parts