In this tutorial, you will create spider elements and then apply loads to them.
On your desktop or the appropriate network drive, create a folder named spider.
Click the link below:
Extract the part file to your spider folder.
Start Simcenter 3D or NX.
Open spider_sim1.sim.
The options you select in dialog boxes are preserved for the next time you open the same dialog box within a given session. Restore the default settings to ensure that the dialog boxes are in the expected initial state for each step of the activity.
File |
Preferences→User Interface
Options |
Reset Dialog Memory
OK |
|
Make the FEM file both the displayed part and work part.
Simulation Navigator
Simulation File View |
|
spider_fem1
Make Displayed Part
Create a 2D seed mesh that will force the 3D mesh to follow a paver mesh around the holes in the part.
2D Mesh (Home tab→Mesh group)
Type |
CQUAD4 |
Meshing Method |
Paver |
Element Size |
6 mm |
Mesh Settings |
|
Export Mesh to Solver
OK |
|
3D Tetrahedral (Mesh group)
the part
Type |
CTETRA(10) |
Element Size |
6 mm |
Destination Collector |
|
New Collector (Mesh Collector)
Create Physical (Solid Property)
Choose material (Material)
Materials |
|
Aluminum_2014 |
OK |
Material List, PSOLID, and Mesh Collector dialog boxes |
Automatic Creation
Mesh Collector |
Solid(1) |
OK |
3D Tetrahedral Mesh dialog box |
You will create a spider element in each of the holes in the model to provide a place to apply loads. For the first three holes, you will use the point-to-edge technique.
1D Connection (Connections group)
Type |
Point to Edge |
Source and Target Selection |
|
Source |
|
(Select Point)
Select the arc center as the source.
Target |
|
(Select Edge)
Type |
RBE2 |
Mid-Node Option |
|
Connect Mid-Nodes
Apply |
1D Connection dialog box |
Repeat these steps for the next two holes, moving clockwise from the upper-left hole. For the subsequent holes, however, select the Connect Mid-Nodes check box.
The upper left hole has fewer legs in its spider element because it was created without the mid-nodes option, which generates connections at the mid-node of each element.
Cancel |
1D Connection dialog box |
You will create the last spider element using a different technique, which can be helpful when creating a spider element in an irregularly shaped hole.
Nodes and Elements |
Node Create (Nodes group)
Location |
|
Specify Point |
Arc/Ellipse/Sphere Center |
OK |
|
Home |
1D Connection (Connections group)
Type |
Node to Node |
Select the node that you created in the previous step.
Source |
|
Node (Select Node)
Target |
|
Node (Select Node)
Method (Top Border bar) |
Related Nodes |
Type Filter (Top Border bar) |
Polygon Edge |
Select the edge of the hole.
All nodes along that edge are selected automatically.
Type |
RBE2 |
OK |
|
In the next step, you will modify this element.
When you use the node-to-node technique to create a spider element, you cannot specify whether or not to include legs to the mid-nodes; they are created automatically. However, you can add or remove legs for any 1D connection as needed.
Nodes and Elements |
Connectivity (Elements group)
Elements to Modify |
|
|
Single Element |
Type |
Modify Leg Nodes |
Press Shift and select some of the mid-nodes.
To add a leg to a node, select the node without pressing the Shift key.
OK |
|
Make the Simulation file the displayed and work part so you can apply boundary conditions.
Simulation Navigator
Simulation File View |
|
spider_sim1
Make Displayed Part
Constrain the groove on the underside of the part.
Fixed Translation Constraint (Home tab→Loads and Conditions group→ Constraint Type list)
Type Filter (Top Border bar) |
Polygon Face |
OK |
|
You will use a group to quickly apply the loads.
Simulation Navigator
Groups
New Group
Type Filter (Top Border bar) |
Node |
Select the center node of each spider element.
Name |
Spider Nodes |
OK |
Use the new group to apply loads to the spider elements.
Force (Loads and Conditions group→ Load Type list)
Model Objects |
|
Group Reference
Name |
|
Spider Nodes |
Magnitude |
|
Force |
100 N |
Direction |
|
Specify Vector |
–XC Axis |
Distribution |
|
Method |
Total per Object |
OK |
|
At this point you can check the model, solve it, and display the results.
Save
File |
Close→All Parts