In this tutorial, you will learn how to use the Automatic Coupling command.
On your desktop or the appropriate network drive, create a folder named impeller2.
Click the link below:
Extract the file to your impeller2 folder.
Start Simcenter 3D or NX.
Open impeller_sim1.sim.
The options you select in dialog boxes are preserved for the next time you open the same dialog box within a given session. Restore the default settings to ensure that the dialog boxes are in the expected initial state for each step of the activity.
File |
Preferences→User Interface
Options |
Reset Dialog Memory
OK |
|
In this cyclic symmetric analysis, the solid body of the impeller has been trimmed to a single blade. In the supplied FEM, a 2D mesh dependency on the symmetry faces was used to seed the 3D solid mesh. It also includes a global cyclic coordinate system, a cylindrical coordinate system whose Z-axis defines the default axis of rotation for the FEM.
You will assign the global cyclic coordinate system that was defined for the FEM as the nodal displacement coordinate system.
Menu |
Edit→Node→Assign Nodal Coordinate System
Type Filter (Top Border bar) |
Polygon Body |
CSYS |
Global Cyclic Analysis |
Boundary Options |
|
Interior and Boundary Nodes
OK |
|
Fixed Translation Constraint (Home tab→Loads and Conditions group→ Constraint Type list)
Rotate the model to view the underside.
Type Filter (Top Border bar) |
Polygon Face |
OK |
|
Couple the degrees of freedom (DOF) for each pair of equivalently positioned nodes lying on the repeated faces.
Automatic Coupling (Loads and Conditions group→ Constraint Type list)
Independent Seed Object |
|
Independent (Select Object)
Use QuickPick to select the polygon vertex.
Dependent Seed Object |
|
(the polygon vertex)
Reference Coordinate System |
|
Type |
Global Cyclic Analysis |
Degrees of Freedom |
|
DOF1 |
On |
DOF2 |
On |
DOF3 |
On |
OK |
|
The constraint symbols have a large default size and may clutter your display. Reduce the size of the symbols.
Simulation Navigator
Constraint Container
NoTrans(1)
Ctrl |
+ Automatic Coupling(1) |
Edit Display
Scale
Drag toward Tiny.
OK |
|
Coupling the DOF of node pairs created a constraint that conflicts with the fixed translation constraint. The conflict occurs along the four edges of the model shared by the dependent face of the coupling constraint and the faces that have the fixed translation constraint. In the illustration, these edges are shown in orange.
If you attempt to solve this model, the conflicting constraints would cause the solve to terminate.
You can resolve the conflicting constraints by excluding the edges where the conflicting constraint occurs from the fixed translation constraint. The nodes on the excluded edges will still be fixed because they are coupled to fixed nodes on the independent face.
The independent and dependent faces were determined when the 2D dependent mesh was created.
is the independent face
is the dependent face
Edit the fixed translation constraint to exclude the edges with the conflicting constraint condition.
Simulation Navigator
Constraint Container
NoTrans(1)
Edit
Excluded |
|
Excluded (Select Object)
Type Filter (Top Border bar) |
Polygon Edge |
OK |
|
The fixed translation constraint no longer exists on the edges that are excluded. By selecting the fixed translation constraint in the Simulation Navigator, you can zoom in and see that the constraint symbols are no longer applied along the excluded edges.
Rotation (Loads and Conditions group→ Load Type list)
Type |
Whole Model |
Direction |
|
If necessary:
Axis of Rotation |
Global Cyclic Analysis |
Properties |
|
Angular Velocity |
10000 rev/min2 |
Make sure that you use the correct units.
OK |
|
Save
Simulation Navigator
Solution 1
Model Setup Check
In the Information window, note the recommendation to use the iterative solver.
the Information window
Solution 1
Edit
General |
Element Iterative Solver
OK |
|
Solution 1
Solve
OK |
|
Wait until the solve is complete.
No |
Review Results dialog box |
the Information window
Cancel |
Analysis Job Monitor dialog box |
Simulation Navigator
Solution 1→Results
Structural
Post Processing Navigator
Solution 1→Structural→Displacement – Nodal
Magnitude
Save
After viewing the displacement magnitude results, try displaying the Von Mises results under Stress - Element-Nodal.
File |
Close→All Parts