ITK Function Reference
(12.1) |
Macros | |
#define | POM_array_length 19905 |
#define | POM_array_length_gt 19904 |
#define | POM_array_length_lt 19903 |
#define | POM_enquiry_cpid_of 19901 |
#define | POM_enquiry_uid_of 19900 |
#define | POM_MAX_action_token 0 |
#define | POM_MIN_action_token 1 |
#define | POM_sponsor_group "Sponsor" |
#define | POM_SPONSORABLE 1 |
#define | POM_SPONSORABLE_OFF 0 |
Type tokens for attributes | |
#define | POM_MIN_type_token 2001 |
#define | POM_char 2001 |
#define | POM_date 2002 |
#define | POM_double 2003 |
#define | POM_float 2004 |
#define | POM_int 2005 |
#define | POM_logical 2006 |
#define | POM_short 2007 |
#define | POM_string 2008 |
#define | POM_typed_reference 2009 |
#define | POM_untyped_reference 2010 |
#define | POM_external_reference 2011 |
#define | POM_note 2012 |
#define | POM_long_string 2013 |
#define | POM_MAX_type_token 2013 |
Attribute tokens for attribute properties | |
These may be added; note there is no MIN or MAX, but SUM = all-bits-set. | |
#define | POM_has_initial_value ( 1 << 0 ) |
#define | POM_has_lowerbound ( 1 << 1 ) |
#define | POM_has_upperbound ( 1 << 2 ) |
#define | POM_is_classvariable ( 1 << 3 ) |
#define | POM_is_unique ( 1 << 5 ) |
#define | POM_null_is_valid ( 1 << 6 ) |
#define | POM_cannot_be_frozen ( 1 << 7 ) |
#define | POM_public_read ( 1 << 8 ) |
#define | POM_public_write ( 1 << 9 ) |
#define | POM_transient ( 1 << 10 ) |
#define | POM_attr_is_candidate_key ( 1 << 11 ) |
#define | POM_attr_follow_on_export ( 1 << 12 ) |
#define | POM_attr_export_as_string ( 1 << 13 ) |
#define | POM_attr_ignore_export_errors ( 1 << 14 ) |
#define | POM_attr_may_not_be_stubbed ( 1 << 15 ) |
#define | POM_attr_no_pom_backpointer ( 1 << 16 ) |
#define | POM_public ( POM_public_read | POM_public_write ) |
#define | POM_SUM_attr_tokens |
Bit flags for the bit mask attribute on POM object | |
These may be added; note there is no MIN or MAX, but SUM = all-bits-set. | |
#define | POM_object_mask_frozen ( 1 << 0 ) |
#define | POM_object_mask_has_ixr ( 1 << 1 ) |
#define | POM_object_mask_is_locked ( 1 << 2 ) |
#define | POM_object_mask_not_changed ( 1 << 3 ) |
#define | POM_object_mask_is_bulkcheckedout ( 1 << 4 ) |
#define | POM_object_mask_has_ds ( 1 << 5 ) |
#define | POM_SUM_object_tokens |
Date conversion tokens | |
#define | POM_MIN_date_conversion_token 6001 |
#define | POM_gmt_to_local 6001 |
#define | POM_local_to_gmt 6002 |
#define | POM_MAX_date_conversion_token 6002 |
Instance state tokens | |
#define | POM_MIN_instance_state_token 7001 |
#define | POM_inst_is_not_loaded 7001 |
#define | POM_inst_is_loaded 7002 |
#define | POM_inst_is_loaded_for_modify 7003 |
#define | POM_inst_is_new 7004 |
#define | POM_inst_is_modified 7005 |
#define | POM_inst_is_selected 7006 |
#define | POM_inst_is_selected_modified 7007 |
#define | POM_inst_is_being_deleted 7008 |
#define | POM_MAX_instance_state_token 7008 |
Order tokens | |
#define | POM_MIN_order_token 8001 |
#define | POM_order_ascending 8001 |
#define | POM_order_descending 8002 |
#define | POM_order_ascending_asnumber 8003 |
#define | POM_order_descending_asnumber 8004 |
#define | POM_MAX_order_token 8004 |
Class tokens for class properties | |
#define | POM_uninstantiable_class 0x10000000 |
#define | POM_uninheritable_class 0x20000000 |
#define | POM_class_requires_sa 0x40000000 |
#define | POM_class_is_exportable 0x80000000 |
#define | POM_class_is_versionable 0x00200000 |
#define | POM_can_have_versionable_subclasses 0x00800000 |
#define | POM_class_prop_has_flat_tables 0x00010000 |
#define | POM_class_is_revisable 0x00200000 |
#define | POM_can_have_revisable_subclasses 0x00800000 |
#define | POM_SUM_class_tokens 0xf0a10000 |
Where_to_search tokens for referencers_of_instance | |
#define | POM_MIN_search_token 9001 |
#define | POM_in_ds_only 9001 |
#define | POM_in_db_only 9002 |
#define | POM_in_ds_and_db 9003 |
#define | POM_MAX_search_token 9003 |
Attribute array type tokens for generating sql | |
#define | POM_MIN_array_type_token 0x01000000 |
#define | POM_large_array 0x01000000 |
#define | POM_small_array 0x02000000 |
#define | POM_variable_length_array 0x04000000 |
#define | POM_non_array 0x08000000 |
#define | POM_any_array (POM_large_array | POM_small_array | POM_variable_length_array) |
#define | POM_SUM_array_type_token (POM_any_array | POM_non_array) |
#define | POM_MAX_array_type_token 0x08000000 |
Lock type tokens | |
#define | POM_MIN_lock_type_token 0 |
#define | POM_no_lock 0 |
#define | POM_modify_lock 1 |
#define | POM_read_lock 2 |
#define | POM_delete_lock 3 |
#define | POM_MAX_lock_type_token 3 |
Space type tokens | |
#define | POM_MIN_space_type_token 0 |
#define | POM_space_markup 0 |
#define | POM_space_change 1 |
#define | POM_space_staging 2 |
#define | POM_MAX_space_type_token 2 |
#define | POM_space_non_exclusive 0 |
#define | POM_space_exclusive 1 |
#define | POM_space_private 2 |
tokens for reasons for losing locks | |
#define | POM_MIN_lost_lock_token 0 |
#define | POM_lost_lock_session_gone 0 |
#define | POM_lost_lock_session_killed 1 |
#define | POM_lost_lock_stolen 2 |
#define | POM_lost_lock_dont_know 3 |
#define | POM_MAX_lost_lock_token 3 |
Auditable action tokens | |
#define | POM_AUDIT_purge_audit "POM_AUDIT_purge_audit" |
#define | POM_AUDIT_bad_password_login "POM_AUDIT_bad_password_login" |
#define | POM_AUDIT_bad_password_check "POM_AUDIT_bad_password_check" |
#define | POM_AUDIT_change_password "POM_AUDIT_change_password" |
Machine type tokens | |
#define | POM_MIN_machine_token 10001 |
#define | POM_UNKNOWN 10001 |
#define | POM_APOLLO 10002 |
#define | POM_VAX 10003 |
#define | POM_HP_68K 10004 |
#define | POM_HP_RISC 10005 |
#define | POM_SUN_68K 10006 |
#define | POM_SUN_SPARC 10007 |
#define | POM_DEC_5000 10008 |
#define | POM_DEC_ALPHA_OSF 10009 |
#define | POM_DEC_ALPHA_VMS 10010 |
#define | POM_SGI 10011 |
#define | POM_IBM_MVS 10012 |
#define | POM_IBM_RS6000 10013 |
#define | POM_DEC_ALPHA_NT 10014 |
#define | POM_INTEL_NT 10015 |
#define | POM_MAX_machine_token 10015 |
Schema conversion tokens | |
#define | POM_MIN_conv_class_token 11001 |
#define | POM_conv_class_changed 11001 |
#define | POM_conv_class_removed 11002 |
#define | POM_MAX_conv_class_token 11002 |
#define | POM_MIN_conv_attr_token 12001 |
#define | POM_conv_attr_new 12001 |
#define | POM_conv_attr_removed 12002 |
#define | POM_MAX_conv_attr_token 12002 |
Import ownership tokens | |
#define | POM_MIN_import_token 13001 |
#define | POM_import_raise_error 13001 |
#define | POM_import_always_map 13002 |
#define | POM_import_default_to_map 13003 |
#define | POM_import_default_to_current 13004 |
#define | POM_import_default_as_apt 13005 |
#define | POM_MAX_import_token 13005 |
POM_site_config_file tokens | |
#define | POM_site_config_file_preferences 1 |
#define | POM_site_config_file_overlay 2 |
#define | POM_site_config_file_definition 3 |
#define | POM_site_config_definition_runtime 4 |
Operator tokens for building new enquiries | |
#define | POM_enquiry_asc_order 0 |
#define | POM_enquiry_desc_order 1 |
#define | POM_enquiry_const_value 0 |
#define | POM_enquiry_bind_value 1 |
Logical operators | |
#define | POM_enquiry_not 14000 |
#define | POM_enquiry_and 14001 |
#define | POM_enquiry_and_filter 14002 |
#define | POM_enquiry_or 14003 |
Comparative operators | |
#define | POM_enquiry_equal 15000 |
#define | POM_enquiry_greater_than 15001 |
#define | POM_enquiry_greater_than_or_eq 15002 |
#define | POM_enquiry_less_than 15003 |
#define | POM_enquiry_less_than_or_eq 15004 |
#define | POM_enquiry_not_equal 15005 |
#define | POM_enquiry_not_between 15006 |
#define | POM_enquiry_between 15007 |
#define | POM_enquiry_join 15008 |
#define | POM_enquiry_left_outer_join 15009 |
#define | POM_enquiry_right_outer_join 15010 |
#define | POM_enquiry_full_outer_join 15011 |
#define | POM_enquiry_nvl 15012 |
Unary operators | |
#define | POM_enquiry_is_null 15500 |
#define | POM_enquiry_is_not_null 15502 |
wild_card_operator | |
#define | POM_enquiry_like 16001 |
#define | POM_enquiry_not_like 16002 |
list_operators | |
#define | POM_enquiry_in 16501 |
#define | POM_enquiry_not_in 16502 |
existantial_operator | |
#define | POM_enquiry_exists 17001 |
#define | POM_enquiry_not_exists 17002 |
vla_operators | |
#define | POM_enquiry_contains 17501 |
#define | POM_enquiry_contains_lt 17502 |
#define | POM_enquiry_contains_gt 17503 |
#define | POM_enquiry_contains_between 17504 |
#define | POM_enquiry_contains_like 17505 |
#define | POM_enquiry_contains_other_than 17506 |
#define | POM_enquiry_contains_not_like 17507 |
#define | POM_enquiry_contains_not_gt 17508 |
#define | POM_enquiry_contains_not_lt 17509 |
#define | POM_enquiry_contains_not_between 17510 |
set_operators | |
#define | POM_enquiry_union 18001 |
#define | POM_enquiry_unionall 18002 |
#define | POM_enquiry_difference 18003 |
#define | POM_enquiry_intersection 18004 |
string_function | |
#define | POM_enquiry_substr 18500 |
#define | POM_enquiry_ltrim 18501 |
#define | POM_enquiry_rtrim 18502 |
#define | POM_enquiry_concat 18503 |
#define | POM_enquiry_ascii 18504 |
#define | POM_enquiry_lower 18505 |
#define | POM_enquiry_upper 18506 |
#define | POM_enquiry_length 18507 |
Aggregate function | |
#define | POM_enquiry_max 19000 |
#define | POM_enquiry_min 19001 |
#define | POM_enquiry_sum 19002 |
#define | POM_enquiry_avg 19004 |
#define | POM_enquiry_count 19300 |
#define | POM_enquiry_countall 19301 |
#define | POM_enquiry_countdist 19302 |
Conversion function | |
#define | POM_enquiry_tonumber 19500 |
#define | POM_enquiry_tc_to_number 19501 |
#define | POM_enquiry_todate 19502 |
Arithmetic operators | |
#define | POM_enquiry_plus 19800 |
#define | POM_enquiry_minus 19801 |
#define | POM_enquiry_multiply 19802 |
#define | POM_enquiry_divide 19803 |
#define | POM_enquiry_mod 19804 |
Procedure argument tokens | |
#define | POM_MIN_procedure_arg_token 20001 |
#define | POM_proc_mode_in 20001 |
#define | POM_proc_mode_out 20002 |
#define | POM_proc_mode_inout 20003 |
#define | POM_MAX_procedure_arg_token 20003 |
Custom function | |
#define | POM_enquiry_configure_eblck 20101 |
#define | POM_enquiry_configure_cnf 20102 |
Functional index tokens. | |
#define | POM_index_func_upper "UPPER" |
#define | POM_index_func_substr "SUBSTR" |
#define | POM_index_func_coalesce "COALESCE" |
Site flag tokens. | |
#define | POM_site_ODS ( 1 << 1 ) |
#define | POM_site_Hub ( 1 << 2 ) |
#define | POM_site_Http ( 1 << 3 ) |
#define | POM_site_TCXML ( 1 << 4 ) |
#define | POM_site_Offline ( 1 << 5 ) |
#define | POM_site_master_delete_allowed ( 1 << 6 ) |
#define | POM_site_unmanaged ( 1 << 7 ) |
#define | POM_site_external_application ( 15 << 8 ) |
#define | POM_site_unknown ( 1 << 12 ) |
#define | POM_site_test_env ( 1 << 13 ) |
#define | POM_site_archive ( 1 << 14 ) |
#define | POM_briefcase_browser ( 1 << 15 ) |
#define | POM_briefcase_browser_with_plugin ( 1 << 16 ) |
This section contains a complete list of the tokens that can be handed to, or returned by, a POM function.
Conjunction Tokens (for combining enquiries):
POM_and
POM_nand
POM_nor
POM_or
Type Tokens (for attributes):
POM_char
POM_date
POM_double
POM_float
POM_int
POM_logical
POM_short
POM_string
POM_typed_reference
POM_untyped_reference
POM_external_reference
POM_note POM_long_string
Switch Tokens (for setting environment)
POM_ds_checking_switch
POM_rollback_switch
POM_arg_checking_switch
POM_journaling_switch
POM_error_traceback_switch
POM_log_sql_switch
POM_timeout_strategy
POM_timeout_interval
POM_enable_set_attr_callbacks
POM_timeout_strategy_flat
POM_timeout_strategy_linear
POM_timeout_strategy_exp POM_check_space_uniqueness_switch
Attribute Tokens (for attribute properties) These can be added to combine properties.
POM_has_initial_value
POM_has_lowerbound
POM_has_upperbound
POM_is_classvariable
POM_is_unique
POM_is_unique
POM_null_is_valid
POM_cannot_be_frozen
POM_public_read
POM_public_write
POM_public
Operator Tokens (for building enquiries)
POM_is_equal_to
POM_is_greater_than
POM_is_less_than
POM_is_null
POM_is_like
POM_is_referenced_by
POM_has_reference_to
POM_not
POM_case_insensitive
Order Tokens (for specifying the order of the result of an enquiry)
POM_order_ascending
POM_order_descending
Class Tokens (for class properties). These can be added to combine properties.
POM_uninstantiable_class
POM_uninheritable_class
Where-to-Search Tokens (for referencers_of_instance)
POM_in_ds_only
POM_in_db_only
POM_in_ds_and_db
Attribute Array Type Tokens
POM_large_array
POM_small_array
POM_variable_length_array
POM_non_array
POM_any_array
Data Conversion Tokens
POM_gmt_to_local
POM_local_to_gmt
#define POM_and ( 1 << 1 ) |
Definition at line 261 of file pom_tokens.h.
#define POM_any_array (POM_large_array | POM_small_array | POM_variable_length_array) |
Definition at line 409 of file pom_tokens.h.
#define POM_APOLLO 10002 |
Definition at line 479 of file pom_tokens.h.
#define POM_arg_checking_switch 3003 |
Definition at line 167 of file pom_tokens.h.
#define POM_array_length 19905 |
Definition at line 685 of file pom_tokens.h.
#define POM_array_length_equals ( 1 << 19 ) |
Definition at line 276 of file pom_tokens.h.
#define POM_array_length_gt 19904 |
Definition at line 684 of file pom_tokens.h.
#define POM_array_length_lt 19903 |
Definition at line 683 of file pom_tokens.h.
#define POM_array_length_not_equals ( POM_not | POM_array_length_equals ) |
Definition at line 297 of file pom_tokens.h.
#define POM_attr_export_as_string ( 1 << 13 ) |
Definition at line 220 of file pom_tokens.h.
#define POM_attr_follow_on_export ( 1 << 12 ) |
Definition at line 219 of file pom_tokens.h.
#define POM_attr_ignore_export_errors ( 1 << 14 ) |
Definition at line 221 of file pom_tokens.h.
#define POM_attr_is_candidate_key ( 1 << 11 ) |
Definition at line 218 of file pom_tokens.h.
#define POM_attr_may_not_be_stubbed ( 1 << 15 ) |
Definition at line 222 of file pom_tokens.h.
#define POM_attr_no_pom_backpointer ( 1 << 16 ) |
Definition at line 223 of file pom_tokens.h.
#define POM_AUDIT_bad_password_check "POM_AUDIT_bad_password_check" |
Definition at line 469 of file pom_tokens.h.
#define POM_AUDIT_bad_password_login "POM_AUDIT_bad_password_login" |
Definition at line 468 of file pom_tokens.h.
#define POM_AUDIT_change_password "POM_AUDIT_change_password" |
Definition at line 470 of file pom_tokens.h.
#define POM_AUDIT_purge_audit "POM_AUDIT_purge_audit" |
Definition at line 467 of file pom_tokens.h.
#define POM_briefcase_browser ( 1 << 15 ) |
Token to represent unmanaged briefcase browser site
Definition at line 774 of file pom_tokens.h.
#define POM_briefcase_browser_with_plugin ( 1 << 16 ) |
Token to represent unmanaged biefcase browser with plugin site
Definition at line 779 of file pom_tokens.h.
#define POM_bypass_access_check 3010 |
Definition at line 173 of file pom_tokens.h.
#define POM_bypass_attr_update 3011 |
Definition at line 174 of file pom_tokens.h.
#define POM_can_have_revisable_subclasses 0x00800000 |
Definition at line 372 of file pom_tokens.h.
#define POM_can_have_versionable_subclasses 0x00800000 |
Definition at line 367 of file pom_tokens.h.
#define POM_cannot_be_frozen ( 1 << 7 ) |
Definition at line 214 of file pom_tokens.h.
#define POM_case_insensitive ( 1 << 10 ) |
Definition at line 270 of file pom_tokens.h.
#define POM_char 2001 |
Definition at line 144 of file pom_tokens.h.
#define POM_check_private_uniqueness_switch 3022 |
Definition at line 188 of file pom_tokens.h.
#define POM_check_space_uniqueness_switch 3022 |
Definition at line 190 of file pom_tokens.h.
#define POM_class_is_exportable 0x80000000 |
Definition at line 365 of file pom_tokens.h.
#define POM_class_is_revisable 0x00200000 |
Definition at line 371 of file pom_tokens.h.
#define POM_class_is_versionable 0x00200000 |
Definition at line 366 of file pom_tokens.h.
#define POM_class_prop_has_flat_tables 0x00010000 |
Definition at line 368 of file pom_tokens.h.
#define POM_class_requires_sa 0x40000000 |
Definition at line 364 of file pom_tokens.h.
#define POM_contains ( 1 << 11 ) |
Definition at line 271 of file pom_tokens.h.
#define POM_contains_between ( 1 << 17 ) |
Definition at line 274 of file pom_tokens.h.
#define POM_contains_gt ( 1 << 16 ) |
Definition at line 273 of file pom_tokens.h.
#define POM_contains_like ( 1 << 18 ) |
Definition at line 275 of file pom_tokens.h.
#define POM_contains_lt ( 1 << 15 ) |
Definition at line 272 of file pom_tokens.h.
#define POM_contains_not_between ( POM_not | POM_contains_between ) |
Definition at line 296 of file pom_tokens.h.
#define POM_contains_not_gt ( POM_not | POM_contains_gt ) |
Definition at line 294 of file pom_tokens.h.
#define POM_contains_not_like ( POM_not | POM_contains_like ) |
Definition at line 293 of file pom_tokens.h.
#define POM_contains_not_lt ( POM_not | POM_contains_lt ) |
Definition at line 295 of file pom_tokens.h.
#define POM_contains_other_than ( POM_not | POM_contains ) |
Definition at line 292 of file pom_tokens.h.
#define POM_conv_attr_new 12001 |
Definition at line 506 of file pom_tokens.h.
#define POM_conv_attr_removed 12002 |
Definition at line 507 of file pom_tokens.h.
#define POM_conv_class_changed 11001 |
Definition at line 501 of file pom_tokens.h.
#define POM_conv_class_removed 11002 |
Definition at line 502 of file pom_tokens.h.
#define POM_date 2002 |
Definition at line 145 of file pom_tokens.h.
#define POM_DEC_5000 10008 |
Definition at line 485 of file pom_tokens.h.
#define POM_DEC_ALPHA_NT 10014 |
Definition at line 491 of file pom_tokens.h.
#define POM_DEC_ALPHA_OSF 10009 |
Definition at line 486 of file pom_tokens.h.
#define POM_DEC_ALPHA_VMS 10010 |
Definition at line 487 of file pom_tokens.h.
#define POM_delete_lock 3 |
Definition at line 422 of file pom_tokens.h.
#define POM_disable_api 3018 |
Definition at line 181 of file pom_tokens.h.
#define POM_double 2003 |
Definition at line 146 of file pom_tokens.h.
#define POM_ds_checking_switch 3001 |
Definition at line 165 of file pom_tokens.h.
#define POM_enable_set_attr_callbacks 3021 |
Definition at line 184 of file pom_tokens.h.
#define POM_enquiry_and 14001 |
Definition at line 549 of file pom_tokens.h.
#define POM_enquiry_and_filter 14002 |
Definition at line 550 of file pom_tokens.h.
#define POM_enquiry_asc_order 0 |
Definition at line 538 of file pom_tokens.h.
#define POM_enquiry_ascii 18504 |
Definition at line 641 of file pom_tokens.h.
#define POM_enquiry_avg 19004 |
Definition at line 654 of file pom_tokens.h.
#define POM_enquiry_between 15007 |
Definition at line 565 of file pom_tokens.h.
#define POM_enquiry_bind_value 1 |
Definition at line 541 of file pom_tokens.h.
#define POM_enquiry_concat 18503 |
Definition at line 640 of file pom_tokens.h.
#define POM_enquiry_configure_cnf 20102 |
Definition at line 703 of file pom_tokens.h.
#define POM_enquiry_configure_eblck 20101 |
Definition at line 702 of file pom_tokens.h.
#define POM_enquiry_const_value 0 |
Definition at line 540 of file pom_tokens.h.
#define POM_enquiry_contains 17501 |
Definition at line 611 of file pom_tokens.h.
#define POM_enquiry_contains_between 17504 |
Definition at line 614 of file pom_tokens.h.
#define POM_enquiry_contains_gt 17503 |
Definition at line 613 of file pom_tokens.h.
#define POM_enquiry_contains_like 17505 |
Definition at line 615 of file pom_tokens.h.
#define POM_enquiry_contains_lt 17502 |
Definition at line 612 of file pom_tokens.h.
#define POM_enquiry_contains_not_between 17510 |
Definition at line 620 of file pom_tokens.h.
#define POM_enquiry_contains_not_gt 17508 |
Definition at line 618 of file pom_tokens.h.
#define POM_enquiry_contains_not_like 17507 |
Definition at line 617 of file pom_tokens.h.
#define POM_enquiry_contains_not_lt 17509 |
Definition at line 619 of file pom_tokens.h.
#define POM_enquiry_contains_other_than 17506 |
Definition at line 616 of file pom_tokens.h.
#define POM_enquiry_count 19300 |
Definition at line 656 of file pom_tokens.h.
#define POM_enquiry_countall 19301 |
Definition at line 657 of file pom_tokens.h.
#define POM_enquiry_countdist 19302 |
Definition at line 658 of file pom_tokens.h.
#define POM_enquiry_cpid_of 19901 |
Definition at line 682 of file pom_tokens.h.
#define POM_enquiry_desc_order 1 |
Definition at line 539 of file pom_tokens.h.
#define POM_enquiry_difference 18003 |
Definition at line 629 of file pom_tokens.h.
#define POM_enquiry_divide 19803 |
Definition at line 677 of file pom_tokens.h.
#define POM_enquiry_equal 15000 |
Definition at line 558 of file pom_tokens.h.
#define POM_enquiry_exists 17001 |
Definition at line 603 of file pom_tokens.h.
#define POM_enquiry_full_outer_join 15011 |
Definition at line 570 of file pom_tokens.h.
#define POM_enquiry_greater_than 15001 |
Definition at line 559 of file pom_tokens.h.
#define POM_enquiry_greater_than_or_eq 15002 |
Definition at line 560 of file pom_tokens.h.
#define POM_enquiry_in 16501 |
Definition at line 595 of file pom_tokens.h.
#define POM_enquiry_intersection 18004 |
Definition at line 630 of file pom_tokens.h.
#define POM_enquiry_is_not_null 15502 |
Definition at line 580 of file pom_tokens.h.
#define POM_enquiry_is_null 15500 |
Definition at line 579 of file pom_tokens.h.
#define POM_enquiry_join 15008 |
Definition at line 567 of file pom_tokens.h.
#define POM_enquiry_left_outer_join 15009 |
Definition at line 568 of file pom_tokens.h.
#define POM_enquiry_length 18507 |
Definition at line 644 of file pom_tokens.h.
#define POM_enquiry_less_than 15003 |
Definition at line 561 of file pom_tokens.h.
#define POM_enquiry_less_than_or_eq 15004 |
Definition at line 562 of file pom_tokens.h.
#define POM_enquiry_like 16001 |
Definition at line 587 of file pom_tokens.h.
#define POM_enquiry_lower 18505 |
Definition at line 642 of file pom_tokens.h.
#define POM_enquiry_ltrim 18501 |
Definition at line 638 of file pom_tokens.h.
#define POM_enquiry_max 19000 |
Definition at line 651 of file pom_tokens.h.
#define POM_enquiry_min 19001 |
Definition at line 652 of file pom_tokens.h.
#define POM_enquiry_minus 19801 |
Definition at line 675 of file pom_tokens.h.
#define POM_enquiry_mod 19804 |
Definition at line 678 of file pom_tokens.h.
#define POM_enquiry_multiply 19802 |
Definition at line 676 of file pom_tokens.h.
#define POM_enquiry_not 14000 |
Definition at line 548 of file pom_tokens.h.
#define POM_enquiry_not_between 15006 |
Definition at line 564 of file pom_tokens.h.
#define POM_enquiry_not_equal 15005 |
Definition at line 563 of file pom_tokens.h.
#define POM_enquiry_not_exists 17002 |
Definition at line 604 of file pom_tokens.h.
#define POM_enquiry_not_in 16502 |
Definition at line 596 of file pom_tokens.h.
#define POM_enquiry_not_like 16002 |
Definition at line 588 of file pom_tokens.h.
#define POM_enquiry_nvl 15012 |
Definition at line 572 of file pom_tokens.h.
#define POM_enquiry_or 14003 |
Definition at line 551 of file pom_tokens.h.
#define POM_enquiry_plus 19800 |
Definition at line 674 of file pom_tokens.h.
#define POM_enquiry_right_outer_join 15010 |
Definition at line 569 of file pom_tokens.h.
#define POM_enquiry_rtrim 18502 |
Definition at line 639 of file pom_tokens.h.
#define POM_enquiry_substr 18500 |
Definition at line 637 of file pom_tokens.h.
#define POM_enquiry_sum 19002 |
Definition at line 653 of file pom_tokens.h.
#define POM_enquiry_tc_to_number 19501 |
Definition at line 666 of file pom_tokens.h.
#define POM_enquiry_todate 19502 |
Definition at line 667 of file pom_tokens.h.
#define POM_enquiry_tonumber 19500 |
Definition at line 665 of file pom_tokens.h.
#define POM_enquiry_uid_of 19900 |
Definition at line 681 of file pom_tokens.h.
#define POM_enquiry_union 18001 |
Definition at line 627 of file pom_tokens.h.
#define POM_enquiry_unionall 18002 |
Definition at line 628 of file pom_tokens.h.
#define POM_enquiry_upper 18506 |
Definition at line 643 of file pom_tokens.h.
#define POM_error_traceback_switch 3005 |
Definition at line 169 of file pom_tokens.h.
#define POM_escape_character 3019 |
Definition at line 182 of file pom_tokens.h.
#define POM_external_reference 2011 |
Definition at line 154 of file pom_tokens.h.
#define POM_float 2004 |
Definition at line 147 of file pom_tokens.h.
#define POM_gmt_to_local 6001 |
Definition at line 312 of file pom_tokens.h.
#define POM_has_initial_value ( 1 << 0 ) |
Definition at line 208 of file pom_tokens.h.
#define POM_has_lowerbound ( 1 << 1 ) |
Definition at line 209 of file pom_tokens.h.
#define POM_has_reference_to ( 1 << 8 ) |
Definition at line 268 of file pom_tokens.h.
#define POM_has_upperbound ( 1 << 2 ) |
Definition at line 210 of file pom_tokens.h.
#define POM_HP_68K 10004 |
Definition at line 481 of file pom_tokens.h.
#define POM_HP_RISC 10005 |
Definition at line 482 of file pom_tokens.h.
#define POM_IBM_MVS 10012 |
Definition at line 489 of file pom_tokens.h.
#define POM_IBM_RS6000 10013 |
Definition at line 490 of file pom_tokens.h.
#define POM_import_always_map 13002 |
Definition at line 517 of file pom_tokens.h.
#define POM_import_default_as_apt 13005 |
Definition at line 520 of file pom_tokens.h.
#define POM_import_default_to_current 13004 |
Definition at line 519 of file pom_tokens.h.
#define POM_import_default_to_map 13003 |
Definition at line 518 of file pom_tokens.h.
#define POM_import_mode 3015 |
Definition at line 178 of file pom_tokens.h.
#define POM_import_raise_error 13001 |
Definition at line 516 of file pom_tokens.h.
#define POM_import_to_group 3017 |
Definition at line 180 of file pom_tokens.h.
#define POM_import_to_user 3016 |
Definition at line 179 of file pom_tokens.h.
#define POM_in_db_only 9002 |
Definition at line 395 of file pom_tokens.h.
#define POM_in_ds_and_db 9003 |
Definition at line 396 of file pom_tokens.h.
#define POM_in_ds_only 9001 |
Definition at line 394 of file pom_tokens.h.
#define POM_index_func_coalesce "COALESCE" |
Definition at line 712 of file pom_tokens.h.
#define POM_index_func_substr "SUBSTR" |
Definition at line 711 of file pom_tokens.h.
#define POM_index_func_upper "UPPER" |
Definition at line 710 of file pom_tokens.h.
#define POM_inst_is_being_deleted 7008 |
Definition at line 329 of file pom_tokens.h.
#define POM_inst_is_loaded 7002 |
Definition at line 323 of file pom_tokens.h.
#define POM_inst_is_loaded_for_modify 7003 |
Definition at line 324 of file pom_tokens.h.
#define POM_inst_is_modified 7005 |
Definition at line 326 of file pom_tokens.h.
#define POM_inst_is_new 7004 |
Definition at line 325 of file pom_tokens.h.
#define POM_inst_is_not_loaded 7001 |
Definition at line 322 of file pom_tokens.h.
#define POM_inst_is_selected 7006 |
Definition at line 327 of file pom_tokens.h.
#define POM_inst_is_selected_modified 7007 |
Definition at line 328 of file pom_tokens.h.
#define POM_int 2005 |
Definition at line 148 of file pom_tokens.h.
#define POM_INTEL_NT 10015 |
Definition at line 492 of file pom_tokens.h.
#define POM_is_classvariable ( 1 << 3 ) |
Definition at line 211 of file pom_tokens.h.
#define POM_is_equal_to ( 1 << 3 ) |
Definition at line 263 of file pom_tokens.h.
#define POM_is_greater_than ( 1 << 4 ) |
Definition at line 264 of file pom_tokens.h.
#define POM_is_less_than ( 1 << 5 ) |
Definition at line 265 of file pom_tokens.h.
#define POM_is_like ( 1 << 7 ) |
Definition at line 267 of file pom_tokens.h.
#define POM_is_not_equal_to ( POM_not | POM_is_equal_to ) |
Definition at line 287 of file pom_tokens.h.
#define POM_is_not_greater_than ( POM_not | POM_is_greater_than ) |
Definition at line 288 of file pom_tokens.h.
#define POM_is_not_less_than ( POM_not | POM_is_less_than ) |
Definition at line 289 of file pom_tokens.h.
#define POM_is_not_like ( POM_not | POM_is_like ) |
Definition at line 291 of file pom_tokens.h.
#define POM_is_not_null ( POM_not | POM_is_null ) |
Definition at line 290 of file pom_tokens.h.
#define POM_is_null ( 1 << 6 ) |
Definition at line 266 of file pom_tokens.h.
#define POM_is_referenced_by ( 1 << 9 ) |
Definition at line 269 of file pom_tokens.h.
#define POM_is_unique ( 1 << 5 ) |
Definition at line 212 of file pom_tokens.h.
#define POM_journaling_switch 3004 |
Definition at line 168 of file pom_tokens.h.
#define POM_large_array 0x01000000 |
Definition at line 405 of file pom_tokens.h.
#define POM_local_to_gmt 6002 |
Definition at line 313 of file pom_tokens.h.
#define POM_log_sql_switch 3006 |
Definition at line 170 of file pom_tokens.h.
#define POM_logical 2006 |
Definition at line 149 of file pom_tokens.h.
#define POM_long_string 2013 |
Definition at line 156 of file pom_tokens.h.
#define POM_lost_lock_dont_know 3 |
Definition at line 459 of file pom_tokens.h.
#define POM_lost_lock_session_gone 0 |
Definition at line 456 of file pom_tokens.h.
#define POM_lost_lock_session_killed 1 |
Definition at line 457 of file pom_tokens.h.
#define POM_lost_lock_stolen 2 |
Definition at line 458 of file pom_tokens.h.
#define POM_MAX_action_token 0 |
Definition at line 387 of file pom_tokens.h.
#define POM_MAX_array_type_token 0x08000000 |
Definition at line 411 of file pom_tokens.h.
#define POM_MAX_conv_attr_token 12002 |
Definition at line 508 of file pom_tokens.h.
#define POM_MAX_conv_class_token 11002 |
Definition at line 503 of file pom_tokens.h.
#define POM_MAX_date_conversion_token 6002 |
Definition at line 314 of file pom_tokens.h.
#define POM_MAX_env_token 3022 |
Definition at line 191 of file pom_tokens.h.
#define POM_MAX_import_token 13005 |
Definition at line 521 of file pom_tokens.h.
#define POM_MAX_instance_state_token 7008 |
Definition at line 330 of file pom_tokens.h.
#define POM_MAX_lock_type_token 3 |
Definition at line 423 of file pom_tokens.h.
#define POM_MAX_lost_lock_token 3 |
Definition at line 460 of file pom_tokens.h.
#define POM_MAX_machine_token 10015 |
Definition at line 493 of file pom_tokens.h.
#define POM_MAX_order_token 8004 |
Definition at line 344 of file pom_tokens.h.
#define POM_MAX_procedure_arg_token 20003 |
Definition at line 695 of file pom_tokens.h.
#define POM_MAX_search_token 9003 |
Definition at line 397 of file pom_tokens.h.
#define POM_MAX_space_type_token 2 |
Definition at line 434 of file pom_tokens.h.
#define POM_MAX_timeout_strategy 4004 |
Definition at line 199 of file pom_tokens.h.
#define POM_MAX_type_token 2013 |
Definition at line 157 of file pom_tokens.h.
#define POM_MIN_action_token 1 |
Definition at line 386 of file pom_tokens.h.
#define POM_MIN_array_type_token 0x01000000 |
Definition at line 404 of file pom_tokens.h.
#define POM_MIN_conv_attr_token 12001 |
Definition at line 505 of file pom_tokens.h.
#define POM_MIN_conv_class_token 11001 |
Definition at line 500 of file pom_tokens.h.
#define POM_MIN_date_conversion_token 6001 |
Definition at line 311 of file pom_tokens.h.
#define POM_MIN_env_token 3001 |
Definition at line 164 of file pom_tokens.h.
#define POM_MIN_import_token 13001 |
Definition at line 515 of file pom_tokens.h.
#define POM_MIN_instance_state_token 7001 |
Definition at line 321 of file pom_tokens.h.
#define POM_MIN_lock_type_token 0 |
Definition at line 418 of file pom_tokens.h.
#define POM_MIN_lost_lock_token 0 |
Definition at line 455 of file pom_tokens.h.
#define POM_MIN_machine_token 10001 |
Definition at line 477 of file pom_tokens.h.
#define POM_MIN_order_token 8001 |
Definition at line 339 of file pom_tokens.h.
#define POM_MIN_procedure_arg_token 20001 |
Definition at line 691 of file pom_tokens.h.
#define POM_MIN_search_token 9001 |
Definition at line 393 of file pom_tokens.h.
#define POM_MIN_space_type_token 0 |
Definition at line 430 of file pom_tokens.h.
#define POM_MIN_timeout_strategy 4000 |
Definition at line 193 of file pom_tokens.h.
#define POM_MIN_type_token 2001 |
Definition at line 143 of file pom_tokens.h.
#define POM_modify_lock 1 |
Definition at line 420 of file pom_tokens.h.
Definition at line 285 of file pom_tokens.h.
#define POM_no_lock 0 |
Definition at line 419 of file pom_tokens.h.
#define POM_non_array 0x08000000 |
Definition at line 408 of file pom_tokens.h.
Definition at line 286 of file pom_tokens.h.
#define POM_not ( 1 << 0 ) |
Definition at line 260 of file pom_tokens.h.
#define POM_note 2012 |
Definition at line 155 of file pom_tokens.h.
#define POM_null_is_valid ( 1 << 6 ) |
Definition at line 213 of file pom_tokens.h.
#define POM_object_mask_frozen ( 1 << 0 ) |
Definition at line 239 of file pom_tokens.h.
#define POM_object_mask_has_ds ( 1 << 5 ) |
Definition at line 248 of file pom_tokens.h.
#define POM_object_mask_has_ixr ( 1 << 1 ) |
Definition at line 240 of file pom_tokens.h.
#define POM_object_mask_is_bulkcheckedout ( 1 << 4 ) |
Definition at line 247 of file pom_tokens.h.
#define POM_object_mask_is_locked ( 1 << 2 ) |
Definition at line 241 of file pom_tokens.h.
#define POM_object_mask_not_changed ( 1 << 3 ) |
Definition at line 245 of file pom_tokens.h.
#define POM_or ( 1 << 2 ) |
Definition at line 262 of file pom_tokens.h.
#define POM_order_ascending 8001 |
Definition at line 340 of file pom_tokens.h.
#define POM_order_ascending_asnumber 8003 |
Definition at line 342 of file pom_tokens.h.
#define POM_order_descending 8002 |
Definition at line 341 of file pom_tokens.h.
#define POM_order_descending_asnumber 8004 |
Definition at line 343 of file pom_tokens.h.
#define POM_proc_mode_in 20001 |
Definition at line 692 of file pom_tokens.h.
#define POM_proc_mode_inout 20003 |
Definition at line 694 of file pom_tokens.h.
#define POM_proc_mode_out 20002 |
Definition at line 693 of file pom_tokens.h.
#define POM_public ( POM_public_read | POM_public_write ) |
Definition at line 224 of file pom_tokens.h.
#define POM_public_read ( 1 << 8 ) |
Definition at line 215 of file pom_tokens.h.
#define POM_public_write ( 1 << 9 ) |
Definition at line 216 of file pom_tokens.h.
#define POM_read_lock 2 |
Definition at line 421 of file pom_tokens.h.
#define POM_rollback_switch 3002 |
Definition at line 166 of file pom_tokens.h.
#define POM_SGI 10011 |
Definition at line 488 of file pom_tokens.h.
#define POM_short 2007 |
Definition at line 150 of file pom_tokens.h.
#define POM_site_archive ( 1 << 14 ) |
Token to represent archive site
Definition at line 769 of file pom_tokens.h.
#define POM_site_config_definition_runtime 4 |
Definition at line 531 of file pom_tokens.h.
#define POM_site_config_file_definition 3 |
Definition at line 530 of file pom_tokens.h.
#define POM_site_config_file_overlay 2 |
Definition at line 529 of file pom_tokens.h.
#define POM_site_config_file_preferences 1 |
Definition at line 528 of file pom_tokens.h.
#define POM_site_external_application ( 15 << 8 ) |
Token to represent application type
Definition at line 756 of file pom_tokens.h.
#define POM_site_Http ( 1 << 3 ) |
Token to represent Http site
Definition at line 736 of file pom_tokens.h.
#define POM_site_Hub ( 1 << 2 ) |
Token to represent Hub site
Definition at line 732 of file pom_tokens.h.
#define POM_site_master_delete_allowed ( 1 << 6 ) |
Token to represent master delete allowed
Definition at line 748 of file pom_tokens.h.
#define POM_site_ODS ( 1 << 1 ) |
Token to represent ODS site
Definition at line 728 of file pom_tokens.h.
#define POM_site_Offline ( 1 << 5 ) |
Token to represent offline site
Definition at line 744 of file pom_tokens.h.
#define POM_site_TCXML ( 1 << 4 ) |
Token to represent tcxml site
Definition at line 740 of file pom_tokens.h.
#define POM_site_test_env ( 1 << 13 ) |
Token to represent test environment
Definition at line 764 of file pom_tokens.h.
#define POM_site_unknown ( 1 << 12 ) |
Token to represent unknown site
Definition at line 760 of file pom_tokens.h.
#define POM_site_unmanaged ( 1 << 7 ) |
Token to represent unmanaged site
Definition at line 752 of file pom_tokens.h.
#define POM_small_array 0x02000000 |
Definition at line 406 of file pom_tokens.h.
#define POM_space_change 1 |
Definition at line 432 of file pom_tokens.h.
#define POM_space_exclusive 1 |
Definition at line 443 of file pom_tokens.h.
#define POM_space_markup 0 |
Definition at line 431 of file pom_tokens.h.
#define POM_space_non_exclusive 0 |
Definition at line 439 of file pom_tokens.h.
#define POM_space_private 2 |
Definition at line 447 of file pom_tokens.h.
#define POM_space_staging 2 |
Definition at line 433 of file pom_tokens.h.
#define POM_sponsor_group "Sponsor" |
Sponsored user login defines.
Definition at line 718 of file pom_tokens.h.
#define POM_SPONSORABLE 1 |
Definition at line 719 of file pom_tokens.h.
#define POM_SPONSORABLE_OFF 0 |
Definition at line 720 of file pom_tokens.h.
#define POM_string 2008 |
Definition at line 151 of file pom_tokens.h.
#define POM_SUM_array_type_token (POM_any_array | POM_non_array) |
Definition at line 410 of file pom_tokens.h.
#define POM_SUM_attr_tokens |
Definition at line 225 of file pom_tokens.h.
#define POM_SUM_class_tokens 0xf0a10000 |
Definition at line 374 of file pom_tokens.h.
#define POM_SUM_object_tokens |
Definition at line 250 of file pom_tokens.h.
#define POM_SUM_operator_tokens |
Definition at line 299 of file pom_tokens.h.
#define POM_SUN_68K 10006 |
Definition at line 483 of file pom_tokens.h.
#define POM_SUN_SPARC 10007 |
Definition at line 484 of file pom_tokens.h.
#define POM_timeout_interval 3008 |
Definition at line 172 of file pom_tokens.h.
#define POM_timeout_strategy 3007 |
Definition at line 171 of file pom_tokens.h.
#define POM_timeout_strategy_count 4004 |
Definition at line 198 of file pom_tokens.h.
#define POM_timeout_strategy_exp 4003 |
Definition at line 197 of file pom_tokens.h.
#define POM_timeout_strategy_flat 4001 |
Definition at line 195 of file pom_tokens.h.
#define POM_timeout_strategy_linear 4002 |
Definition at line 196 of file pom_tokens.h.
#define POM_timeout_strategy_none 4000 |
Definition at line 194 of file pom_tokens.h.
#define POM_tonumber ( 1 << 20 ) |
Definition at line 277 of file pom_tokens.h.
#define POM_transient ( 1 << 10 ) |
Definition at line 217 of file pom_tokens.h.
#define POM_transmit_directory 3014 |
Definition at line 177 of file pom_tokens.h.
#define POM_typed_reference 2009 |
Definition at line 152 of file pom_tokens.h.
#define POM_uninheritable_class 0x20000000 |
Definition at line 363 of file pom_tokens.h.
#define POM_uninstantiable_class 0x10000000 |
Note:- Bits 0x01000000, 0x02000000 and 0x04000000 are used by other tokens.
Definition at line 362 of file pom_tokens.h.
#define POM_UNKNOWN 10001 |
Definition at line 478 of file pom_tokens.h.
#define POM_untyped_reference 2010 |
Definition at line 153 of file pom_tokens.h.
#define POM_update_timestamp 3020 |
Definition at line 183 of file pom_tokens.h.
#define POM_variable_length_array 0x04000000 |
Definition at line 407 of file pom_tokens.h.
#define POM_VAX 10003 |
Definition at line 480 of file pom_tokens.h.
#define POM_wildcard_character_any 3012 |
Definition at line 175 of file pom_tokens.h.
#define POM_wildcard_character_one 3013 |
Definition at line 176 of file pom_tokens.h.