UF_SUBDIV_ask_parms (view source)
Defined in: uf_subdiv.h
Overview
Returns the parameters used for a subdiv feature. Given a subdiv
feature tag, determines the subdiv_type and the parameters for the
type in the subdiv_structure_ptr structure.
Environment
Internal and External
See Also
History
Originally released in V15.0
Required License(s)
gateway
int UF_SUBDIV_ask_parms
(
tag_t subdiv_tag,
UF_SUBDIV_type_p_t subdiv_type,
UF_SUBDIV_data_structures_p_u subdiv_structure_pointer
)
tag_t | subdiv_tag | Input | Object identifier of the subdiv feature |
UF_SUBDIV_type_p_t | subdiv_type | Output | type of subdiv feature |
UF_SUBDIV_data_structures_p_u | subdiv_structure_pointer | Output to UF_*free* | pointer to one of the subdiv data structures. This must be freed by calling UF_SUBDIV_free. |
UF_SUBDIV_ask_type (view source)
Defined in: uf_subdiv.h
Overview
This function returns the type of subdiv feature.Given a subdiv feature tag,
determines the subdiv_type.
Environment
Internal and External
See Also
History
Originally released in V15.0
Required License(s)
gateway
int UF_SUBDIV_ask_type
(
tag_t subdiv_tag,
UF_SUBDIV_type_p_t subdiv_type
)
tag_t | subdiv_tag | Input | object identifier of the subdiv feature |
UF_SUBDIV_type_p_t | subdiv_type | Output | type of subdiv feature |
UF_SUBDIV_create (view source)
Defined in: uf_subdiv.h
Overview
Creates a subdiv feature. The subdiv_type contains the method to use
for splitting faces. It indicates the type of parameters used in the
subdiv_structure_ptr structure. The output of this function is the
object identifier associated to the subdiv feature.
Environment
Internal and External
See Also
History
Originally released in V15.0
Required License(s)
solid_modeling
int UF_SUBDIV_create
(
UF_SUBDIV_type_t subdiv_type,
UF_SUBDIV_data_structures_p_u subdiv_structure_pointer,
tag_p_t subdiv_tag
)
UF_SUBDIV_edit (view source)
Defined in: uf_subdiv.h
Overview
Edits a subdiv feature. The subdiv_type contains the type of subdiv
feature being edited. It indicates the type of parameters used in the
subdiv_structure_ptr structure.
Environment
Internal and External
See Also
History
Originally released in V15.0
Required License(s)
solid_modeling
int UF_SUBDIV_edit
(
UF_SUBDIV_type_t subdiv_type,
UF_SUBDIV_data_structures_p_u subdiv_structure_pointer,
tag_t subdiv_tag
)
UF_SUBDIV_free (view source)
Defined in: uf_subdiv.h
Overview
This function frees any data retrieved via the ask_parms function.
Call UF_SUBDIV_free after a call to UF_SUBDIV_ask_parms.
Environment
Internal and External
See Also
History
Originally released in V15.0
Required License(s)
solid_modeling
int UF_SUBDIV_free
(
UF_SUBDIV_type_t subdiv_type,
UF_SUBDIV_data_structures_p_u subdiv_structure_pointer
)