/*
uf_sket_types.h
File Description:
Open C API s for the sketch module.
*******************************************************************************/
#ifndef UF_SKET_TYPES_INCLUDED
#define UF_SKET_TYPES_INCLUDED
#include <uf_defs.h>
#include <uf_obj_types.h>
/* output_mode used by UF_SKET_add_extracted_objects */
#define UF_SKET_EXTR_ORIG_TYPE (0)
#define UF_SKET_EXTR_MULTI_SPLINES (1)
#define UF_SKET_EXTR_SINGLE_SPLINE (2)
/* ref_info used by UF_SKET_attach_to_face */
#define UF_SKET_HORIZONTAL (1)
#define UF_SKET_VERTICAL (2)
#define UF_SKET_WITH_NORMAL (1)
#define UF_SKET_OPPOSITE_NORMAL (2)
#define UF_SKET_ALONG_CURVE (1)
#define UF_SKET_OPPOSITE_CURVE (-1)
/* geometric constraint type used by UF_SKET_delete_legacy_constraint */
#define UF_SKET_DATUM (10)
#define UF_SKET_CONSTANT_OFFSETS (11)
#define UF_SKET_POINT_ON_CURVE (12)
#define UF_SKET_MIDPOINT_OF_CURVE (13)
#define UF_SKET_HORIZONTAL_LINES (14)
#define UF_SKET_VERTICAL_LINES (15)
#define UF_SKET_CONSTANT_ANGLES (16)
#define UF_SKET_CONSTANT_LENGTH_LINES (17)
#define UF_SKET_COLLINEAR (18)
#define UF_SKET_PARALLEL (19)
#define UF_SKET_PERPENDICULAR (20)
#define UF_SKET_EQUAL_LENGTH (21)
#define UF_SKET_EQUAL_RADIUS (22)
#define UF_SKET_TANGENT_CURVES (23)
/*
Sketch Status definitions
*/
/*
As of V17, the values of these UF_SKET_status_e will be recorded in
the part file. Hence, their values cannot be arbitrarily changed.
*/
enum UF_SKET_status_e
{
UF_SKET_unknown_status,
UF_SKET_not_evaluated,
UF_SKET_under_constrained,
UF_SKET_well_constrained,
UF_SKET_over_constrained,
UF_SKET_inconsistently_constrained
} ;
typedef enum UF_SKET_status_e UF_SKET_status_t, *UF_SKET_status_p_t;
enum UF_SKET_reference_status_e
{
UF_SKET_reference,
UF_SKET_active
};
typedef enum UF_SKET_reference_status_e UF_SKET_reference_status_t;
enum UF_SKET_con_type_e
{
UF_SKET_no_con = 0,
UF_SKET_fixed = 1,
UF_SKET_horizontal = 2,
UF_SKET_vertical = 3,
UF_SKET_parallel = 4,
UF_SKET_perpendicular = 5,
UF_SKET_collinear = 6,
UF_SKET_equal_length = 7,
UF_SKET_equal_radius = 8,
UF_SKET_constant_length = 9,
UF_SKET_constant_angle = 10,
UF_SKET_coincident = 11,
UF_SKET_concentric = 12,
UF_SKET_mirror = 13,
UF_SKET_point_on_curve = 14,
UF_SKET_midpoint = 15,
UF_SKET_tangent = 16,
UF_SKET_radius_dim = 17,
UF_SKET_diameter_dim = 18,
UF_SKET_horizontal_dim = 19,
UF_SKET_vertical_dim = 20,
UF_SKET_parallel_dim = 21,
UF_SKET_perpendicular_dim = 22,
UF_SKET_angular_dim = 23,
UF_SKET_reserved_con_1 = 24, /* Do not use */
UF_SKET_reserved_con_2 = 25, /* Do not use */
UF_SKET_reserved_con_3 = 26, /* Do not use */
UF_SKET_reserved_con_4 = 27, /* Do not use */
UF_SKET_reserved_con_5 = 28, /* Do not use */
UF_SKET_reserved_con_6 = 29, /* Do not use */
UF_SKET_point_on_string = 30,
UF_SKET_slope = 31,
UF_SKET_uniform_scaled = 32,
UF_SKET_non_uniform_scaled = 33,
UF_SKET_assoc_trim = 34, /* Limited support */
UF_SKET_assoc_offset = 35, /* Limited support */
UF_SKET_perimeter_dim = 36,
UF_SKET_pgm_offset = 37,
UF_SKET_normal = 38,
UF_SKET_point_on_loop = 39,
UF_SKET_recipe_trim = 40,
UF_SKET_pattern = 41,
UF_SKET_rigid_set = 42,
UF_SKET_g1 = 43,
UF_SKET_g2 = 44,
UF_SKET_align = 45,
UF_SKET_tangent_to_string = 46,
UF_SKET_perpendicular_to_string = 47,
UF_SKET_scalable_set = 48,
UF_SKET_reserved_con_9 = 49, /* Do not use */
UF_SKET_reserved_con_10 = 50, /* Do not use */
UF_SKET_last_con_type /* The last constraint type indicator; NOT to be used. */
};
typedef enum UF_SKET_con_type_e UF_SKET_con_type_t, *UF_SKET_con_type_p_t;
#define UF_SKET_MAX_CON_TYPES 51
#define UF_SKET_MAX_GEOMETRY_PER_CON 4
enum UF_SKET_con_class_e
{
UF_SKET_no_cons,
UF_SKET_all_cons,
UF_SKET_geo_cons,
UF_SKET_dim_cons
};
typedef enum UF_SKET_con_class_e UF_SKET_con_class_t, *UF_SKET_con_class_p_t;
struct UF_SKET_info_s
{
int subtype; /* UF_v9_sketch_subtype, UF_v13_sketch_subtype or
UF_extracted_sketch_subtype
*/
char name[ UF_OBJ_NAME_BUFSIZE ]; /* sketch's name */
tag_t csys_tag; /* sketch's CSYS tag */
double csys[12]; /* sketch's CSYS :
sketch_csys[0-8] : the orientation,
sketch_csys[9-11]: the origin
*/
char view_name[16]; /* sketch's view name (for pre-V13 sketches only) */
tag_t datum_tag; /* sketch's datum tag (for pre-V13 sketches only) */
double datum[3]; /* sketch's datum (for pre-V13 sketches only) */
} ;
typedef struct UF_SKET_info_s UF_SKET_info_t, *UF_SKET_info_p_t;
/******************************************************************************
enum and structures for creating dimensions
******************************************************************************/
/*
*/
/*
Associativity types for sketch dimension.
*/
enum UF_SKET_assoc_type_e{
UF_SKET_assoc_type_none,
UF_SKET_end_point,
UF_SKET_arc_center,
UF_SKET_tangency,
UF_SKET_curve_point,
UF_SKET_anchor_point
} ;
typedef enum UF_SKET_assoc_type_e UF_SKET_assoc_type_t;
enum UF_SKET_assoc_mod_e{
UF_SKET_first_end_point,
UF_SKET_last_end_point
} ;
typedef enum UF_SKET_assoc_mod_e UF_SKET_assoc_mod_t;
struct UF_SKET_dim_object_s
{
tag_t object_tag; /* Tag of the object - sketch curves, edge,
datum plane, datum axis, NX curves */
UF_SKET_assoc_type_t object_assoc_type; /* Object associativity type:
UF_SKET_end_point;
UF_SKET_arc_center -
object must be an arc;
UF_SKET_tangency -
object must be an arc;
UF_SKET_curve_point -
object must be a spline
UF_SKET_anchor_point -
object must be a sketch conic */
int object_assoc_mod_value; /* Object associativity modifier:
UF_SKET_first_end_point or UF_SKET_last_end_point
if object_assoc_type = UF_SKET_end_point;
Not Used
if object_assoc_type = UF_SKET_arc_center or
UF_SKET_anchor_point;
parameter percentage (0 - 100) (used to find approx tgt pt)
if object_assoc_type = UF_SKET_tangency;
the index number of the defining point of the spline(starting from 1)
if object_assoc_type = UF_SKET_curve_point;
*/
} ;
typedef struct UF_SKET_dim_object_s UF_SKET_dim_object_t, *UF_SKET_dim_object_p_t;
/******************************************************************************
enum and structures for createing geometric constraints
******************************************************************************/
enum UF_SKET_geom_vertex_e
{
UF_SKET_no_vertex,
UF_SKET_start_vertex,
UF_SKET_end_vertex,
UF_SKET_center_vertex, /* used only for Arcs/Ellipses */
UF_SKET_spline_defining_point, /* used only for splines */
UF_SKET_anchor_vertex, /* used only by general conics */
UF_SKET_spline_pole, /* used only for splineByPoles */
UF_SKET_mid_vertex /* used only for Arcs/Lines */
} ;
typedef enum UF_SKET_geom_vertex_e UF_SKET_geom_vertex_t;
enum UF_SKET_help_type_e
{
UF_SKET_no_help_data,
UF_SKET_use_help_pt,
UF_SKET_use_help_param
};
typedef enum UF_SKET_help_type_e UF_SKET_help_type_t;
struct UF_SKET_con_geom_s
{
tag_t geom_tag; /* The geomtry's tag */
UF_SKET_geom_vertex_t vertex_type; /* Vertex type if it is the vertex
of the geometry that will be
constrained.
Valid types are specified in
UF_SKET_geom_vertex_t.
*/
int vertex_index; /* Starting from 1. Used to
indicate which defining point
of the spline will be constrained.
Only used when vertex_type is
UF_SKET_spline_defining_point.
*/
UF_SKET_help_type_t use_help; /* Whether to use help data (either
help points or help parameter.)
Valid types as specified in
UF_SKET_help_type_t. Help
points/parameters are used to
indicate whereabouts on the geometry
a constraint should apply to. They
are only needed when the constraints
are of type UF_SKET_tangent,
UF_SKET_point_on_curve, or
UF_SKET_point_on_string.
*/
double help_point[3]; /* Help point */
double help_parameter; /* Help parameter */
};
typedef struct UF_SKET_con_geom_s UF_SKET_con_geom_t, *UF_SKET_con_geom_p_t;
#endif /* UF_SKET_TYPES_INCLUDED */