UF_SKET_assoc_mod_e (view source)
Defined in: uf_sket_types.h
Also known as:
Data Members
UF_SKET_first_end_point
UF_SKET_last_end_point
UF_SKET_assoc_type_e (view source)
Defined in: uf_sket_types.h
Also known as:
Overview
Associativity types for sketch dimension.
Data Members
UF_SKET_assoc_type_none
UF_SKET_end_point
UF_SKET_arc_center
UF_SKET_tangency
UF_SKET_curve_point
UF_SKET_anchor_point
UF_SKET_con_class_e (view source)
Defined in: uf_sket_types.h
Also known as:
- UF_SKET_con_class_t
- UF_SKET_con_class_p_t
Data Members
UF_SKET_no_cons
UF_SKET_all_cons
UF_SKET_geo_cons
UF_SKET_dim_cons
UF_SKET_con_type_e (view source)
Defined in: uf_sket_types.h
Also known as:
- UF_SKET_con_type_t
- UF_SKET_con_type_p_t
Data Members
UF_SKET_no_con = 0
UF_SKET_fixed = 1
UF_SKET_horizontal = 2
UF_SKET_vertical = 3
UF_SKET_parallel = 4
UF_SKET_perpendicular = 5
UF_SKET_collinear = 6
UF_SKET_equal_length = 7
UF_SKET_equal_radius = 8
UF_SKET_constant_length = 9
UF_SKET_constant_angle = 10
UF_SKET_coincident = 11
UF_SKET_concentric = 12
UF_SKET_mirror = 13
UF_SKET_point_on_curve = 14
UF_SKET_midpoint = 15
UF_SKET_tangent = 16
UF_SKET_radius_dim = 17
UF_SKET_diameter_dim = 18
UF_SKET_horizontal_dim = 19
UF_SKET_vertical_dim = 20
UF_SKET_parallel_dim = 21
UF_SKET_perpendicular_dim = 22
UF_SKET_angular_dim = 23
UF_SKET_reserved_con_1 = 24
UF_SKET_reserved_con_2 = 25
UF_SKET_reserved_con_3 = 26
UF_SKET_reserved_con_4 = 27
UF_SKET_reserved_con_5 = 28
UF_SKET_reserved_con_6 = 29
UF_SKET_point_on_string = 30
UF_SKET_slope = 31
UF_SKET_uniform_scaled = 32
UF_SKET_non_uniform_scaled = 33
UF_SKET_assoc_trim = 34
UF_SKET_assoc_offset = 35
UF_SKET_perimeter_dim = 36
UF_SKET_pgm_offset = 37
UF_SKET_normal = 38
UF_SKET_point_on_loop = 39
UF_SKET_recipe_trim = 40
UF_SKET_pattern = 41
UF_SKET_rigid_set = 42
UF_SKET_g1 = 43
UF_SKET_g2 = 44
UF_SKET_align = 45
UF_SKET_tangent_to_string = 46
UF_SKET_perpendicular_to_string = 47
UF_SKET_scalable_set = 48
UF_SKET_reserved_con_9 = 49
UF_SKET_reserved_con_10 = 50
UF_SKET_last_con_type
UF_SKET_geom_vertex_e (view source)
Defined in: uf_sket_types.h
Also known as:
Overview
enum and structures for createing geometric constraints
Data Members
UF_SKET_no_vertex
UF_SKET_start_vertex
UF_SKET_end_vertex
UF_SKET_center_vertex
UF_SKET_spline_defining_point
UF_SKET_anchor_vertex
UF_SKET_spline_pole
UF_SKET_mid_vertex
UF_SKET_help_type_e (view source)
Defined in: uf_sket_types.h
Also known as:
Data Members
UF_SKET_no_help_data
UF_SKET_use_help_pt
UF_SKET_use_help_param
UF_SKET_reference_status_e (view source)
Defined in: uf_sket_types.h
Also known as:
- UF_SKET_reference_status_t
Data Members
UF_SKET_reference
UF_SKET_active
UF_SKET_status_e (view source)
Defined in: uf_sket_types.h
Also known as:
- UF_SKET_status_t
- UF_SKET_status_p_t
Overview
As of V17, the values of these UF_SKET_status_e will be recorded in
the part file. Hence, their values cannot be arbitrarily changed.
Data Members
UF_SKET_unknown_status
UF_SKET_not_evaluated
UF_SKET_under_constrained
UF_SKET_well_constrained
UF_SKET_over_constrained
UF_SKET_inconsistently_constrained