UF_WELD_ask_body_id (view source)
Defined in: uf_weld.h
Overview
Gets all body tags of welds in a weld feature set.
Environment
Internal and External
See Also
History
Original release was in V16.0.1
int UF_WELD_ask_body_id
(
tag_t feature_set_tag,
tag_p_t * body_id,
int * num_objects
)
tag_t | feature_set_tag | Input | Feature set tag of the weld |
tag_p_t * | body_id | Output to UF_*free* | Array of body tags of welds. This must be freed by calling UF_free. |
int * | num_objects | Output | Number of welds in the weld feature set. |
UF_WELD_ask_connected_parts (view source)
Defined in: uf_weld.h
Overview
Gets the body tags of the connected parts for a weld feature set.
Environment
Internal and External
See Also
History
Original release was in V16.0.1
int UF_WELD_ask_connected_parts
(
tag_t feature_set_tag,
UF_WELD_conn_parts_info_p_t conn_info
)
UF_WELD_ask_groove_or_edge_guide (view source)
Defined in: uf_weld.h
Overview
Given a Groove or Edge weld tag, this function returns the guide curves for
the weld. For all other types of welds refer to UF_WELD_ask_guide_curves.
Environment
Internal and External.
See Also
History
Originally released in v16.0.1
int UF_WELD_ask_groove_or_edge_guide
(
tag_t weld_feat_tag,
uf_list_p_t * guide_crv_cnt,
uf_list_p_t * guide_curves
)
tag_t | weld_feat_tag | Input | tag of the weld feature, can be only Groove or Edge weld feature |
uf_list_p_t * | guide_crv_cnt | Output to UF_*free* | tags of the first set of guide strings use UF_MODL_delete_list to free |
uf_list_p_t * | guide_curves | Output to UF_*free* | tags of the second set of guide strings use UF_MODL_delete_list to free |
UF_WELD_ask_guide_curves (view source)
Defined in: uf_weld.h
Overview
Given the feature set tag, this function returns the guide curves for all
weld types except Groove and Edge welds. Note that guide curves are not
returned if the input tag is a Plug or Slot weld.
Environment
Internal and External.
See Also
History
Originally released in v16.0.1
int UF_WELD_ask_guide_curves
(
tag_t weld_feat_tag,
int * guide_crv_cnt,
tag_t * * guide_curves
)
tag_t | weld_feat_tag | Input | tag of the weld feature, can be either Fillet, Arc Spot, Resistance Spot, Resistance Seam, Bead, Tape, Dollop or Clinch |
int * | guide_crv_cnt | Output | Number of guide curves |
tag_t * * | guide_curves | Output to UF_*free* | tag of guide curves |
UF_WELD_ask_linked_face_parent (view source)
Defined in: uf_weld.h
Overview
Given a face from a Linked or Extract feature returns the source occurrence
or parent object
Environment
Internal and External
See Also
History
Original release was in V16.0.1
int UF_WELD_ask_linked_face_parent
(
tag_t face_tag,
tag_p_t source_obj
)
tag_t | face_tag | Input | face tag of the LINKED_FACE feature |
tag_p_t | source_obj | Output | Tag of the source object for the feature |
UF_WELD_ask_linked_feat_source (view source)
Defined in: uf_weld.h
Overview
Given a Linked or Extract feature returns the source occurrence or parent
object
Environment
Internal and External
See Also
History
Original release was in V16.0.1
int UF_WELD_ask_linked_feat_source
(
tag_t linked_feat_tag,
tag_p_t source_obj
)
tag_t | linked_feat_tag | Input | Tag of the linked or extract feature |
tag_p_t | source_obj | Output | Tag of the source object for the feature |
UF_WELD_ask_number_of_welds (view source)
Defined in: uf_weld.h
Overview
Returns the number of welds in a weld feature set.
Environment
Internal and External
See Also
History
Original release was in V16.0.1
int UF_WELD_ask_number_of_welds
(
tag_t feature_set_tag,
int * num_of_welds
)
tag_t | feature_set_tag | Input | Feature set tag of weld |
int * | num_of_welds | Output | Number of welds present in the weld feature set. |
UF_WELD_ask_seam_weld_info (view source)
Defined in: uf_weld.h
Overview
Given the feature set tag, this function returns the tags of the seams in the
feature set and the faces involved in the seam. Please note that this function
works for seam weld and bead.
Environment
Internal and External.
History
Originally released in v16.0.1
int UF_WELD_ask_seam_weld_info
(
tag_t seam_feature_set,
int * seam_count,
tag_p_t * seam_id,
int * num_sets,
int * * n_faces_in_each_set,
tag_p_t * * set_of_faces
)
tag_t | seam_feature_set | Input | tag of the seam feature set |
int * | seam_count | Output | count of the seams in the feature set |
tag_p_t * | seam_id | Output to UF_*free* | tags of the seams in the feature set. Use UF_free to free this variable. |
int * | num_sets | Output | number of sets of faces involved in the weld |
int * * | n_faces_in_each_set | Output to UF_*free* | number of faces in each set. Must free using UF_free_string_array |
tag_p_t * * | set_of_faces | Output to UF_*free* | tags of the faces involved in the weld. Use UF_free_string_array to free the array |
UF_WELD_ask_segment_len_of_welds (view source)
Defined in: uf_weld.h
Overview
Returns the segment length of weld in a weld feature set. If the weld is a
continuous weld then the total length of weld is returned.
Environment
Internal and External
See Also
History
Original release was in V16.0.1
int UF_WELD_ask_segment_len_of_welds
(
tag_t feature_set_tag,
double * seg_len
)
tag_t | feature_set_tag | Input | Feature set tag of weld |
double * | seg_len | Output | Segment length of weld |
UF_WELD_ask_spacing_of_welds (view source)
Defined in: uf_weld.h
Overview
Returns the spacing between welds in a weld feature set. If the weld is a
single or continuous weld then the spacing returned is zero.
Environment
Internal and External
See Also
History
Original release was in V16.0.1
int UF_WELD_ask_spacing_of_welds
(
tag_t feature_set_tag,
double * spacing
)
tag_t | feature_set_tag | Input | Feature set tag of weld |
double * | spacing | Output | Spacing between welds. |
UF_WELD_ask_spot_face_data (view source)
Defined in: uf_weld.h
Overview
Given the spot ( or clinch ) feature set tag, this function will return the
information regarding the weld. This function will work for resistance spot,
arc spot and clinch.
Environment
Internal and External
See Also
History
Originally released in v16.0.1
int UF_WELD_ask_spot_face_data
(
tag_t spot_feature_set,
int * num_sets,
int * spot_count,
UF_WELD_spot_info_p_t * spot_info
)
tag_t | spot_feature_set | Input | tag of the spot feature set |
int * | num_sets | Output | number of sets of faces in the spot weld |
int * | spot_count | Output | number of spots in the feature set |
UF_WELD_spot_info_p_t * | spot_info | Output to UF_*free* | pointer to the data structure which contains the spot weld information ( see uf_weld_types.h ) for the given feature set tag. Use UF_WELD_free_spot_data to free this pointer. |
UF_WELD_ask_spot_face_info (view source)
Defined in: uf_weld.h
Overview
Given the spot ( or clinch ) feature set tag, this function will return the
information regarding the weld. This function will work for resistance spot,
arc spot and clinch.
Environment
Internal and External
See Also
History
Originally released in v18.0.4. Will be made obsolete in V20
int UF_WELD_ask_spot_face_info
(
tag_t spot_feature_set,
int * num_sets,
int * spot_count,
UF_WELD_spot_data_p_t * spot_info
)
tag_t | spot_feature_set | Input | tag of the spot feature set |
int * | num_sets | Output | number of sets of faces in the spot weld |
int * | spot_count | Output | number of spots in the feature set |
UF_WELD_spot_data_p_t * | spot_info | Output to UF_*free* | pointer to the data structure which contains the spot weld information ( see uf_weld_types.h ) for the given feature set tag. Use UF_WELD_free_spot_info to free this pointer. |
UF_WELD_ask_spot_weld_info (view source)
Defined in: uf_weld.h
Overview
Given the spot feature set tag, this function returns the tags of the spot
points and the faces involved in the weld.
Environment
Internal and External
History
Originally Released in v16.0.1
int UF_WELD_ask_spot_weld_info
(
tag_t spot_feature_set,
tag_p_t top_body,
int * spot_count,
tag_p_t * spot_points,
int * num_sets,
int * * n_faces_in_each_set,
tag_p_t * * set_of_faces
)
tag_t | spot_feature_set | Input | tag of the spot feature set |
tag_p_t | top_body | Output | tag of the top body |
int * | spot_count | Output | number of spots in the feature set |
tag_p_t * | spot_points | Output to UF_*free* | feature tags of the spot points in the feature set. Use UF_free to free this variable |
int * | num_sets | Output | number of sets of faces |
int * * | n_faces_in_each_set | Output to UF_*free* | number of faces in each set. Must free using UF_free_string_array |
tag_p_t * * | set_of_faces | Output to UF_*free* | tags of the faces involved in the weld. Use UF_free_string_array to free the array |
UF_WELD_free_spot_data (view source)
Defined in: uf_weld.h
Overview
Frees the memory used for storing spot weld information
Environment
Internal and External.
See Also
History
Originally released in v16.0.1
int UF_WELD_free_spot_data
(
int spot_count,
UF_WELD_spot_info_p_t * spot_info
)
int | spot_count | Input | number of spots in the spot feature set |
UF_WELD_spot_info_p_t * | spot_info | Input | pointer to the data structure which contains the spot weld information |
UF_WELD_free_spot_info (view source)
Defined in: uf_weld.h
Overview
Frees the memory used for storing spot weld information
Environment
Internal and External.
See Also
History
Originally released in v18.0.4 . Will be made obsolete in V20
int UF_WELD_free_spot_info
(
int spot_count,
UF_WELD_spot_data_p_t * spot_info
)
int | spot_count | Input | number of spots in the spot feature set |
UF_WELD_spot_data_p_t * | spot_info | Input | pointer to the data structure which contains the spot weld information |
UF_WELD_is_object_weld (view source)
Defined in: uf_weld.h
Overview
Returns whether the input object is weld.
Environment
Internal and External
See Also
History
Original release was in V16.0.1
int UF_WELD_is_object_weld
(
tag_t object,
logical * is_weld,
tag_p_t feature_set_tag
)
tag_t | object | Input | Tag of weld body |
logical * | is_weld | Output | TRUE if the body is weld otherwise returns FALSE |
tag_p_t | feature_set_tag | Output | Feature set tag of the weld body |
UF_WELD_locate_welds2 (view source)
Defined in: uf_weld.h
Overview
To fetch an array of all weld objects in the specified assembly.
Optionally, filter the weld objects by weld type.
The weld_array must be freed using UF_free.
This replaces UF_WELD_locate_welds, which only returns legacy welds.
Environment
Internal and External
History
Originally released in NX 5.0
int UF_WELD_locate_welds2
(
tag_t work_part,
UF_WELD_feature_types_array types_array,
int * count,
tag_p_t * weld_array
)
tag_t | work_part | Input | The specified assembly to query |
UF_WELD_feature_types_array | types_array | Input | An array of logicals to indicate which weld types to return. Use UF_WELD_INIT_TYPES_ARRAY(types_array,false) to initialize all to off. Use UF_WELD_INIT_TYPES_ARRAY(types_array,true) to get all weld types. To get a specific weld feature, use UF_WELD_feature_types_e to turn on a specific weld feature. |
int * | count | Output | Pointer to the number of weld object which answer the query. This may be 0. This storage is not allocated by the function. Pass in a valid integer location If the count is not desired, pass in a NULL instead of a pointer |
tag_p_t * | weld_array | Output to UF_*free* | The pointer in which to return the array containing the tags of the found weld_objects. If NULL is passed in instead of a pointer, then the array is not returned. Such an option might be used to simply obtain a count of the objects. If the pointer is returned as non_NULL, then the array must be freed by UF_free |
UF_WELD_populate_attr_list (view source)
Defined in: uf_weld.h
Overview
Gets the attribute titles of weld belonging to a weld feature_set_tag.
Environment
Internal and External
See Also
History
Original release was in V16.0.1
int UF_WELD_populate_attr_list
(
tag_t feature_set_tag,
char * * * attribute_title,
int * count
)
tag_t | feature_set_tag | Input | Feature set tag of the weld |
char * * * | attribute_title | Output to UF_*free* | Attibute titles of the weld. This must be freed by calling UF_free_string_array. |
int * | count | Output | Number of attributes of the weld. |