UF_LIB_ask_lib_attribute_values (view source)
Defined in: uf_lib.h
Overview
This function provides a list of attribute values of an NX object that
was previously retrieved from a library. The library is referenced by the
specified UF_CAM_db_object_t. The values are the current values (in the
library) of the specified attributes of the NX object.
The caller should use UF_free_string_array to free these returned arrays.
Environment
Internal and External
History
Released in V16.0
Required License(s)
gateway
int UF_LIB_ask_lib_attribute_values
(
UF_CAM_db_object_t db,
tag_t ug_object,
int count,
const char * * db_alias,
char * * * values
)
UF_CAM_db_object_t | db | Input | - the db object to query in |
tag_t | ug_object | Input | - the NX object to query about |
int | count | Input | - the number of attribute to ask their values of |
const char * * | db_alias | Input | - the list of attribute db aliases to ask the values of |
char * * * | values | Output to UF_*free* | - the requested values. This is an array of strings that must be freed by calling UF_free_string_array. |
UF_LIB_ask_libref (view source)
Defined in: uf_lib.h
Overview
This function provides the library reference (or libref) of the specified
NX object. The libref is an attribute which is returned for every record
in every record set. It is also the attribute which is used to retrieve
an object from a library. An NX object will only have a libref if it was
created by being retrieved from a library.
Environment
Internal and External
History
Released in V16.0
Required License(s)
gateway
int UF_LIB_ask_libref
(
tag_t ug_object,
const char * * libref
)
tag_t | ug_object | Input | - the desired NX object |
const char * * | libref | Output to UF_*free* | - the libref of the specified object |
UF_LIB_ask_record_in_rset (view source)
Defined in: uf_lib.h
Overview
This function provides a record from a record set. The record is returned
as an array of strings. Each element of the array is the value of an
attribute of the specified record. The ith element of the array is the
value of the ith attribute returned from ask_rset_map. Note that all values
are returned as strings. If the value has type double or int the caller
will need to convert as required by the application.
The caller should use UF_free_string_array to free these returned arrays.
Environment
Internal and External
History
Released in V16.0
Required License(s)
gateway
int UF_LIB_ask_record_in_rset
(
UF_RSET_t rset,
int record_num,
int * count,
const char * * * values
)
UF_RSET_t | rset | Input | - the desired record set |
int | record_num | Input | - the desired record number (0 based) |
int * | count | Output | - the number of values of attributes |
const char * * * | values | Output to UF_*free* | - the values of the attributes. The caller should call UF_free_string_array to free this array. |
UF_LIB_ask_rset_count (view source)
Defined in: uf_lib.h
Overview
This function returns the number of records that the specified UF_RSET_t
contains.
Environment
Internal and External
History
Released in V17.0
Required License(s)
gateway
int UF_LIB_ask_rset_count
(
UF_RSET_t rset,
int * count
)
UF_RSET_t | rset | Input | - the UF_RSET_t whose record count is desired |
int * | count | Output | - the number of records in the UF_RSET_t |
UF_LIB_ask_rset_map (view source)
Defined in: uf_lib.h
Overview
This function provides a description (or map) of the contents of a record
set. It provides a list of the attributes that each record in the record
set has as well as the type of each of those attributes. One can think of
a record set as a table. The rows of the table are the individual records
in the record set. The columns headings are the attributes that are found
in the record set.
NOTE: Use UF_LIB_free_rset_map to free returned memory
See the
description
Environment
Internal and External
See Also
History
Released in V16.0
Required License(s)
gateway
int UF_LIB_ask_rset_map
(
UF_RSET_t rset,
int * count,
const char * * * attr_names,
const char * * attr_types
)
UF_RSET_t | rset | Input | - the record set of interest. This was returned by execute_query. |
int * | count | Output | - the number of attributes in the record set. |
const char * * * | attr_names | Output to UF_*free* | count - the name of the attributes in the record set. |
const char * * | attr_types | Output to UF_*free* | count - the types of the attributes. The ith attr_types is the type of the ith attr_names. |
UF_LIB_delete_rset (view source)
Defined in: uf_lib.h
Overview
This function deletes the specified UF_RSET_t.
Environment
Internal and External
History
Released in V17.0
Required License(s)
gateway
int UF_LIB_delete_rset
(
UF_RSET_t rset
)
UF_LIB_execute_query (view source)
Defined in: uf_lib.h
Overview
This function will execute a query in a library and return a record set
containing the objects in the library that satisfy the query.
See the above File Description for a discussion of the query syntax. The
Class Query in the Definition File is &&ed to the query specified here as
a parameter. The contents of the RSET returned is determined by the
RSET definition for the specified class name. This definition is found in the
Definition File.
Environment
Internal and External
History
Released in V16.0
Required License(s)
gateway
int UF_LIB_execute_query
(
UF_CAM_db_object_t db,
const char * cls_name,
const char * query,
int * count,
UF_RSET_t * rset
)
UF_CAM_db_object_t | db | Input | - the library object in which to execute the query. |
const char * | cls_name | Input | - the class name |
const char * | query | Input | - the query |
int * | count | Output | - the number of objects satisfying the query |
UF_RSET_t * | rset | Output | - the record of objects that satisfy the query |
UF_LIB_execute_query_for_count (view source)
Defined in: uf_lib.h
Overview
This function will execute a query in a library and return a count of the
number of objects in the library that satisfy the query. See the above
File Description for a discussion of the query syntax. The Class Query in
the Definition File is &&ed to the query specified here as a parameter.
Environment
Internal and External
History
Released in V16.0
Required License(s)
gateway
int UF_LIB_execute_query_for_count
(
UF_CAM_db_object_t db,
const char * cls_name,
const char * query,
int * count
)
UF_CAM_db_object_t | db | Input | - the library object in which to execute the query |
const char * | cls_name | Input | - the class name |
const char * | query | Input | - the query |
int * | count | Output | - the number of objects in the library that satisfy the query. |
UF_LIB_free_rset_map (view source)
Defined in: uf_lib.h
Overview
This function frees the memory returned from UF_LIB_ask_rset_map
Environment
Internal and External
See Also
History
Released in V16.0
Required License(s)
gateway
int UF_LIB_free_rset_map
(
int count,
const char * * attr_names,
const char * attr_types
)
int | count | Input | - the number of attributes in the record set. |
const char * * | attr_names | Input | - the name of the attributes in the record set. |
const char * | attr_types | Input | - the types of the attributes. The ith attr_types is the type of the ith attr_names. |
UF_LIB_merge_rsets (view source)
Defined in: uf_lib.h
Overview
This function merges the contents of two record sets. The merged record set
contains the records of 'rset1' followed by the records of 'rset2'. The
records appear in the same order they did in their original record sets.
'rset1' and 'rset2' are unchanged.
Environment
Internal and External
History
Released in V17.0
Required License(s)
gateway
int UF_LIB_merge_rsets
(
UF_RSET_t rset1,
UF_RSET_t rset2,
UF_RSET_t * merged_rset
)
UF_LIB_sort_rset (view source)
Defined in: uf_lib.h
Overview
This function sorts the contents of a record set. The sort key is of the
form:
db_alias1/{ a|d },db_alias2/{ a|d },...,db_aliasN/{ a|d }
where a = ascending, d = descending. For example, if Diameter and Cost are
both DB Aliases that are found in the record set one could sort the set
primarily by Diameter in ascending order and then, within Diameter, sort by
Cost in decreasing order with a sort key of:
Diameter/a,Cost/d
Here Diameter is the primary key. Records of the set that have the same
Diameter are then sorted by Cost. The original record set is not changed.
Environment
Internal and External
History
Released in V17.0
Required License(s)
gateway
int UF_LIB_sort_rset
(
UF_RSET_t rset,
const char * sort_key,
UF_RSET_t * sorted_rset
)
UF_RSET_t | rset | Input | - the record set to sort |
const char * | sort_key | Input | - the sort key to sort by |
UF_RSET_t * | sorted_rset | Output | - the sorted record set |