UF_BREP_ask_edge_class (view source)
Defined in: uf_brep.h
Overview
This function returns the class numbers for the edge.
A ring edge is an edge, like the end of a cylinder, that has a curve but
no vertices. A closed edge is like a ring edge but has one vertex. An
open edge has two vertices. In topology structures, it is permissible for
a closed edge to have two vertices as children but they must be the
same vertex.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_BREP_ask_edge_class
(
const UF_BREP_topology_t * item,
int * edge_class,
int * geom_class
)
const UF_BREP_topology_t * | item | Input | Item of topology for which the edge class numbers are to be returned. |
int * | edge_class | Output | Class number of edge: UF_BREP_EDGE_OPEN UF_BREP_EDGE_CLOSED UF_BREP_EDGE_RING |
int * | geom_class | Output | Class number of geometry on edge: UF_BREP_EDGE_NORMAL: has 3D curve. UF_BREP_EDGE_INTERSECTION: has 3D curve derived from surfaces. UF_BREP_EDGE_TOLERANT: has SP curve. UF_BREP_EDGE_SP: not a tolerant edge but represented with an SP curve. |
UF_BREP_ask_geometry (view source)
Defined in: uf_brep.h
Overview
The given geometry is queried from the model and returned in the
application-supplied structure. Any arrays needed (for example in
b-surfaces and extruded surfaces) are allocated by Open API and
must be freed with UF_free, or with UF_BREP_free_geometry_data.
For curves, geom_sense is forward if the curve tangent is pointing in
the same direction as traversing the edge from the start vertex to the
end vertex. For surfaces, geom_sense is forward if the surface normal
points in the face normal direction (which the loop direction
determines).
Special attention is given to geometries that cannot be returned
without approximation. Blend surfaces, intersection edges, and
tolerant edges have no direct representation in available geometry
types. Therefore, when requesting data for a face or edge, the
mappings and tolerances must always be supplied in the respective
structures. Applications sometimes provide different tolerances for
faces and edges, or for different types of surfaces or curves.
This function's results are undefined if any function that changes the
body's topology is used between the time UF_BREP_ask_topology is
called and the time this function is called. This includes any feature
changes or any other modelling operation.
Geometry may be asked on a topology being used to create a body.
It is important to realize that when asking for fin geometry for a
tolerant edge, the SP curves returned were produced at the time the
edge was made tolerant (when it was modelled). Its accuracy was
determined at that time. Such curves are returned by this function as
they were constructed when made. Setting a smaller tolerance for this
function does not improve their accuracy. A smaller tolerance in this
function only improves the accuracy of curves or surfaces that must be
approximated by this function.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_BREP_ask_geometry
(
const UF_BREP_topology_t * topology,
const UF_BREP_options_t * options,
const UF_BREP_mapping_t * mapping,
UF_BREP_geometry_t * geometry,
UF_BREP_orientation_t * geom_sense,
int * num_states,
UF_BREP_state_t * * states
)
const UF_BREP_topology_t * | topology | Input | Pointer to topology item structure defining geometry to be returned |
const UF_BREP_options_t * | options | Input | Applicable options: All tolerances for edge and fin curves, and for surfaces, should be specified. |
const UF_BREP_mapping_t * | mapping | Input | Surface and curve type mappings to cause output to be in b-spline geometry. |
UF_BREP_geometry_t * | geometry | Input | Pointer to geometry structure to receive the description. |
UF_BREP_orientation_t * | geom_sense | Input / Output | Input: Geometry orientation with respect to the topology entity. For faces, fins, and edges: UF_BREP_ORIENTATION_FORWARD or UF_BREP_ORIENTATION_REVERSE. Otherwise UF_BREP_ORIENTATION_NONE. Output: Pointer to geometry structure to receive the description. |
int * | num_states | Output | number of states in the states array |
UF_BREP_state_t * * | states | Output to UF_*free* | UF_BREP allocated array. If the caller passes in a NULL, UF_BREP does not allocate the array. This should be freed by calling UF_free. |
UF_BREP_ask_identifier (view source)
Defined in: uf_brep.h
Overview
Returns a unique identifier within a body for topology elements that
do not have NX tags, viz., vertices, fins, and shells. The identifier is
useful for Open API level algorithms that need to test for identical
topology elements, e.g., is a vertex on an edge the same as a vertex on
another edge?
Return
void
Environment
Internal and External
Required License(s)
gateway
void UF_BREP_ask_identifier
(
const UF_BREP_topology_t * body_topos,
int * identifier
)
const UF_BREP_topology_t * | body_topos | Input | Topology entity for which to return an identifier. |
int * | identifier | Output | Unique for all other topology identifiers within the same body. |
UF_BREP_ask_topology (view source)
Defined in: uf_brep.h
Overview
Returns a topological description of a body or face. The body_topos
list with the children pointer arrays defines the connections between
the entities of the body.
The topology for a face is returned as if it were a sheet body, unless
SP curve modifications are requested, in which case the vertices are
omitted.
The orientation of edges or fins in loops is indicated by the
orientation member of the oriented child structure.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_BREP_ask_topology
(
tag_t body,
const UF_BREP_options_t * options,
UF_BREP_topology_t * * body_topos,
int * num_states,
UF_BREP_state_t * * states
)
tag_t | body | Input | Tag of body for which to return topology |
const UF_BREP_options_t * | options | Input | Options are specified as needed. Fin modifications (flattening, singularities) are specified here when requesting surface data for trimming. |
UF_BREP_topology_t * * | body_topos | Output to UF_*free* | Topology structures and arrays that describe the body. |
int * | num_states | Output | Number of states in the state array |
UF_BREP_state_t * * | states | Output to UF_*free* | UF_BREP allocated array. If the caller passes in a NULL, UF_BREP does not allocate the array. This should be freed by calling UF_free. |
UF_BREP_ask_topology_source (view source)
Defined in: uf_brep.h
Overview
Returns the source of the specified topology.
Environment
Internal and External
See Also
Required License(s)
gateway
int UF_BREP_ask_topology_source
(
const UF_BREP_topology_t * body_topos,
UF_BREP_topo_source_t * topo_source
)
UF_BREP_attach_geometry (view source)
Defined in: uf_brep.h
Overview
The given geometry is created and attached to the topology item
indicated. UF_BREP_attach_geometry returns an error if the geometry
already has attached geometry.
No geometry is permitted to be attached to a topology item not of the
correct type. Only edges and fins may have curves, only faces may
have surfaces, and only vertices may have points. You may attach 3D
curves to edges and SP curves to the fins of that edge. The additional
information is sometimes useful in creating a valid edge.
For curves, geom_sense is forward if the curve tangent is pointing in
the same direction as traversing the edge from the start vertex to the
end vertex. For surfaces, geom_sense is forward if the surface normal
points in the face normal direction (which the loop direction
determines).
Simplifications performed on b-geometry are the following:
A bspline that is linear is converted to a line. This is done for
linear and quadratic spline data.
A bspline that represents a circle is converted to a circle.
A surface of revolution with a line as the generator is
converted to a cylinder or cone, if the generator is aligned
suitably.
A surface of revolution with an arc as the generator is
converted to a sphere or torus, if the generator is aligned
suitably. Even partial arcs are simplified to the complete
surface.
A bsurface that is planar is converted to a plane. This is done
for linear and quadratic bsurface data.
A bsurface that is linear in one direction and circular in the
other is converted to a cylinder or cone.
A bsurface that is circular in both directions is converted to a
sphere or torus.
Please note the following items:
Some configurations of spline data that represent analytic geometry
may not be simplified. This is because particular forms may not be
recognized by Open API.
If simplification is requested, and SP curves are to be used to
construct the face, it is necessary that the simplification introduce a
transformation of the surface parameterization that is linear in
nature. Any other transformation causes SP curves to assume an
incorrect shape. In particular, conversions of b-surfaces and
b-curves to their analytic equivalents may introduce
parameterization changes that are incompatible with using SP
curves for face construction. If the latter is the case, a state that so
indicates is returned.
Environment
Internal and External
See Also
Required License(s)
solid_modeling
int UF_BREP_attach_geometry
(
UF_BREP_topology_t * topology,
const UF_BREP_geometry_t * geometry,
const UF_BREP_orientation_t geom_sense,
const UF_BREP_options_t * options,
int * num_states,
UF_BREP_state_t * * states
)
UF_BREP_topology_t * | topology | Input | Pointer to topological structure containing item to which the geometry is to be attached |
const UF_BREP_geometry_t * | geometry | Input | Pointer to geometry structure defining geometry to be attached |
const UF_BREP_orientation_t | geom_sense | Input | Geometry orientation with respect to the topology entity. For faces, fins, and edges use: UF_BREP_ORIENTATION_FORWARD or UF_BREP_ORIENTATION_REVERSE. Otherwise use UF_BREP_ORIENTATION_NONE. |
const UF_BREP_options_t * | options | Input | Applicable options: Simplification, UF_BREP_simplify_option |
int * | num_states | Output | number of states in the states array |
UF_BREP_state_t * * | states | Output to UF_*free* | UF_BREP allocated array. If the caller passes in a NULL, UF_BREP does not allocate the array. This should be freed by calling UF_free. |
UF_BREP_delete_geometry (view source)
Defined in: uf_brep.h
Overview
Deletes the geometry attached to the specified topology. Note that the
delete is permissible only on topologies that have not yet become a
NX body. Typically a UF_BREP_attach_geometry call would follow
a UF_BREP_delete_geometry call, e.g., if the attach failed for a
known and correctable reason.
Environment
Internal and External
See Also
Required License(s)
solid_modeling
int UF_BREP_delete_geometry
(
const UF_BREP_topology_t * item
)
UF_BREP_free_geometry_data (view source)
Defined in: uf_brep.h
Overview
All data structures allocated by Open API when UF_BREP_ask_geometry was called
are freed.
Environment
Internal and External
See Also
Required License(s)
solid_modeling
int UF_BREP_free_geometry_data
(
UF_BREP_geometry_p_t geometry,
UF_BREP_free_fn_t fn
)
UF_BREP_geometry_p_t | geometry | Input / Output | Data structures allocated by UF_BREP_ask_geometry are freed. |
UF_BREP_free_fn_t | fn | Input | UF_BREP_free_geometry_data calls UF_BREP_free_fn_t to free geometry structure data, e.g., B-curve and B-surface pole arrays. If free_function is NULL, then this routine uses UF_free. |
UF_BREP_heal_body (view source)
Defined in: uf_brep.h
Overview
This routine fixes, or cleans up, a body created by other Open API
functions. It attempts to re-intersect edges, reposition vertices, and set
tolerances as designated by the level specified, to make the body pass
all checks. Any object (typically a face or edge) that cannot be fixed is
returned in the state list.
The tolerance value specified is an upper limit. Any entity that
requires a tolerance larger than this limit in order to pass checks is
returned in the states array.
Any given object may have more than one entry in the states array.
The healing levels cause the following fix ups to be attempted:
0 Report problems with the body in the state list.
1 For all problems fixable with tolerances, apply the smallest
tolerance that alleviates the problem.
2 For any edge that must be tolerant at level 1, use
surface-surface intersection to attempt to create an exact
curve for the edge. Any that cannot be made exact are made
tolerant.
3 For any edge that must be tolerant at level 1 and for all spline
edges, use surface-surface intersection to attempt to create an
exact curve for the edge. Any that cannot be made exact are
made tolerant.
4 For all edges, use surface-surface intersection to attempt to
create an exact curve for the edge. Any that cannot be made
exact are made tolerant.
Environment
Internal and External
Required License(s)
solid_modeling
int UF_BREP_heal_body
(
tag_t body,
int level,
double toler,
int * num_states,
UF_BREP_state_t * * states
)
tag_t | body | Input | body to fix |
int | level | Input | healing level: any of 0 through 4 |
double | toler | Input | maximum tolerance; fix up of entities requiring tolerances exceeding this are returned in the state list |
int * | num_states | Output | number of states in the states array |
UF_BREP_state_t * * | states | Output to UF_*free* | UF_BREP allocated array. If the caller passes in a NULL, UF_BREP does not allocate the array. This should be freed by calling UF_free. |
UF_BREP_make_body (view source)
Defined in: uf_brep.h
Overview
Creates an NX body from a UF_BREP topology hierarchy that defines the
body topology and geometry. In addition to returning the NX body tag,
UF_BREP_make_body assigns the NX edge and face tags to the
corresponding input UF_BREP topology structures. UF_BREP_make_body
also does the equivalent of UF_BREP_heal_body to help make the NX body
pass validity checks.
With solid topology input, the output is an NX solid body. With face
topology input, the output is an NX sheet body. For a multi-face sheet
topology, you must call UF_BREP_make_body for each face of the sheet,
and then use UF_MODL_create_sew to sew the sheets together. You can
call UF_BREP_make_body with a sheet topology, but the resulting NX
sheet body represents only the first face of the input sheet topology.
Environment
Internal and External
See Also
Required License(s)
solid_modeling
int UF_BREP_make_body
(
UF_BREP_topology_t * topology,
tag_t * body,
int * num_states,
UF_BREP_state_t * * states
)
UF_BREP_topology_t * | topology | Input | Topology that has all geometry attached. The toplogy is made into an NX body. You can pass a face topology element. |
tag_t * | body | Output | NX tag of body |
int * | num_states | Output | number of states in state array |
UF_BREP_state_t * * | states | Output to UF_*free* | UF_BREP allocated array. If the caller passes in a NULL, UF_BREP does not allocate the array. This should be freed by calling UF_free. |
UF_BREP_release_topology (view source)
Defined in: uf_brep.h
Overview
Frees the UF_BREP structures of a topology. The structures include
the oriented children structure arrays.
If a is topology built by the user and not finished, UF_BREP_release_topology
must be called.
Environment
Internal and External
See Also
Required License(s)
solid_modeling
int UF_BREP_release_topology
(
const UF_BREP_topology_t * body_topos,
UF_BREP_free_fn_t fn
)
const UF_BREP_topology_t * | body_topos | Input | Topology for body the application is done with |
UF_BREP_free_fn_t | fn | Input | UF_BREP_free_geometry_data calls UF_BREP_free_fn_t to free geometry structure data, e.g., B-curve and B-surface pole arrays. If the free_function is NULL, then this routine uses UF_free. |
UF_BREP_validate_topology (view source)
Defined in: uf_brep.h
Overview
Optional function to validate the body_topos tree. It validates the
children contents, i.e., shells must be the children of the body, faces
must be children of shells, loops the children of faces, fins (if present)
the children of loops, edges the children of fins (if present, children of
loops if not), and vertices the children of edges (if edges are present)
or fins (if edges are not present). Thus the type members must be set
to valid values and the children arrays must be set (but the children
arrays may be unspecified, when it is desirable to build the body in
stages.)
The extension fields are updated with a pointer for use by the
UF_BREP module. The application must not alter this value and
must use it only with the macros designated for that purpose.
Environment
Internal and External
See Also
Required License(s)
solid_modeling
int UF_BREP_validate_topology
(
const UF_BREP_topology_t * body_topos,
int * num_states,
UF_BREP_state_t * * states
)
const UF_BREP_topology_t * | body_topos | Input | Topology structure array to initialize |
int * | num_states | Output | Number of states in the state array |
UF_BREP_state_t * * | states | Output to UF_*free* | UF_BREP allocated array. If the caller passes in a NULL, UF_BREP does not allocate the array. This should be freed by calling UF_free. |