/*
uf.h
File Description :
Open C API general interface. These are general purpose functions that
will be common to most Open C API programs, as well as specialized functions
that do not belong to any of the other interfaces.
***************************************************************************/
#ifndef UF_INCLUDED
#define UF_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_cfi_types.h>
#include <uf_ugopenint.h>
#include <uf_cfi_types.h>
#include <uf_retiring.h>
#include <libufun_exports.h>
#define NONE 0
#define METRIC 1
#define ENGLISH 2
/*****************************************************************************
Unique identifiers for standard NX applications
*****************************************************************************/
#define UF_APP_NONE (0) /* No App Module (may be in External UF)*/
#define UF_APP_DRAFTING (1) /* Drafting */
#define UF_APP_MECHANISMS (14) /* CAE - Mechanisms */
#define UF_APP_CAM (16) /* Manufacturing */
/* obsoleted in NX 3 (38) ICAD - Generative Modeling */
#define UF_APP_MODELING (40) /* Modeling */
#define UF_APP_VALISYS (47) /* Valisys - Quality Control */
#define UF_APP_GATEWAY (48) /* Gateway */
/* UGMX retired in V18.0.0.12 */
#define UF_APP_UGMX (50) /* UGMX Interface */
#define UF_APP_HARNESS (51)
#define UF_APP_FLAT (60) /* Sheet Metal Design - Flat Patterns */
#define UF_APP_SHTNEST (61) /* Sheet Metal Design - Nesting */
#define UF_APP_PUNCH (62) /* Sheet Metal Design - Punch Press */
#define UF_APP_MPG (63) /* Sheet Metal Design - Multipart Gridding */
#define UF_APP_SSL (64) /* Sheet Metal Design - Surface Layout */
#define UF_APP_SHTFAB (65) /* Sheet Metal Design - Fabrication */
#define UF_APP_SMD (66) /* Sheet Metal Design Application */
#define UF_APP_BUILDER (67) /* UI Builder */
#define UF_APP_SFEM (68) /* CAE Advanced Simulation */
#define UF_APP_ROUTE (69) /* PSA - Routing Applications */
/* obsoleted (70) PSA - Virtual Mockup (Division) */
#define UF_APP_PIPE (71) /* PSA - Routing - Piping */
#define UF_APP_TUBE (72) /* PSA - Routing - Tubing */
#define UF_APP_STEEL (73) /* PSA - Routing - Steel */
#define UF_APP_CONDUIT (74) /* PSA - Routing - Conduit */
#define UF_APP_RACEWAY (75) /* PSA - Routing - Raceway */
#define UF_APP_SHOPS (76) /* Manufacturing - Shop floor app */
#define UF_APP_WIRE (77) /* PSA - Routing - Wiring */
#define UF_APP_MTB (78) /* Manufacturing - Machine Tool Builder */
#define UF_APP_SKETCHER (79) /* Sketcher Task Environment */
#define UF_APP_NOPART (80) /* No Part loaded menubar */
/* obsoleted (81) CAE - Advanced FEM */
#define UF_APP_ROUTE_MECH (82) /* PSA - Routing - Mechanical */
#define UF_APP_ROUTE_ELEC (83) /* PSA - Routing - Electrical */
#define UF_APP_ROUTE_LGCL (84) /* PSA - Routing - Logical */
#define UF_APP_SBSM (85) /* SBSM - Straight Break Sheet Metal */
#define UF_APP_SEQUENCING (86) /* Sequencing Task Environment */
#define UF_APP_UFUN (87) /* UFUN app */
#define UF_APP_STUDIO (88) /* Shape Studio */
#define UF_APP_DESFEM (89) /* CAE - Design Simulation */
#define UF_APP_SHIP (90) /* PSA - Ship Building */
#define UF_APP_AEROSM (91) /* PSA - Aerospace Sheet Metal Application */
#define UF_APP_FLEX_PCB (92) /* Flexible Printed Circuit Design */
#define UF_APP_INSPECTION (93) /* CMM Inspection Programming */
#define UF_APP_MECHATRONICS (94) /* Mechatronics Designer */
#define UF_APP_STYLER (95) /* Block Styler */
#define UF_APP_SUBSET_DEFINITION (96) /* Subset Definition task environment */
#define UF_APP_TRUE_STUDIO (97) /* True Studio Task Environment */
#define UF_APP_SHIP_BASICDESIGN (98) /* Ship Building */
#define UF_APP_SHIP_DETAILSDESIGN (99)/* Ship Building */
#define UF_APP_SHIP_MANUFACTURE (100) /* Ship Building */
#define UF_APP_SINUCAST (101) /* SinuCAST */
#define UF_APP_SUBDIVISION_MODELING (102) /* Subdivision Modeling Task Environment */
/* Codesets supported by NX. This is returned by the
function UF_ask_codeset. */
enum UF_codeset_e
{
UF_CODESET_NOT_INITIALIZED=-2, /* This is an error condition. */
UF_CODESET_NOT_SUPPORT=-1, /* This is an error condition. */
UF_CODESET_ASCII, /* Only ASCII characters are supported.
If NX does not recognize a
codeset, then it will revert to
UF_CODESET_ASCII. */
UF_CODESET_ISO8859_1, /* Western European standard */
UF_CODESET_EUC, /* Japanese EUC codeset */
UF_CODESET_SJIS, /* Japanese SJIS codeset */
UF_CODESET_ISO8859_4, /* Finnish, Latvian, Norwegian, Swedish
and other European languages. */
UF_CODESET_ISO8859_5, /* Russian, Ukrainian, Bulgarian and other
Eastern European languages. */
UF_CODESET_ISO8859_8, /* Hebrew codeset */
UF_CODESET_BIG5, /* Traditional Chinese for Taiwan */
UF_CODESET_NT_866, /* No longer used, placeholder only */
UF_CODESET_ISO8859_2, /* Czech, Polish, Slovak and other
Eastern European languages. */
UF_CODESET_NT_852, /* No longer used, placeholder only */
UF_CODESET_NT_862, /* No longer used, placeholder only */
UF_CODESET_KSC5601, /* Korean codeset */
UF_CODESET_GB2312, /* Simplified Chinese for Mainland China */
UF_CODESET_NT_1251, /* Windows NT Russian codeset */
UF_CODESET_NT_1255, /* Windows NT Hebrew codeset */
UF_CODESET_NT_1250, /* Windows NT Eastern European codeset */
UF_CODESET_NT_1252, /* Windows NT Western European and US
codeset */
UF_CODESET_ISO8859_15, /* Western European codeset including
EURO */
UF_CODESET_NT_1253, /* Windows NT Greek codeset */
UF_CODESET_ISO8859_7, /* Greek Codeset */
UF_CODESET_UTF8, /* UTF-8 Codeset */
UF_CODESET_NT_1254, /* Windows NT Turkish codeset */
UF_CODESET_NT_1257, /* Windows NT Baltic codeset */
UF_CODESET_NT_1256, /* Windows NT Arabic codeset */
UF_CODESET_ISO8859_6, /* Arabic Codeset */
UF_CODESET_ISO8859_11, /* Thai Unix and Windows (CP 874) */
UF_CODESET_NT_1258 /* Vietnamese codeset */
};
typedef enum UF_codeset_e UF_codeset_t;
/*
This type is used to hold information about a timer in NX. You
can have more than one timer active at a time, each active timer requires
a UF_timer_t variable.
*/
typedef unsigned short UF_timer_t, *UF_timer_p_t;
/*
The structure UF_timer_values_t below is used to get the values from the
timer. The routine UF_end_timer fills the fields of this structure, when the
timer is closed. The timer is initiated by the routine UF_begin_timer.
*/
struct UF_timer_values_s
{
double cpu_time; /* Total CPU time (User + System) for this process */
double real_time; /* Total elapsed time */
};
typedef struct UF_timer_values_s
UF_timer_values_t, *UF_timer_values_p_t;
/*
The structure UF_system_info_t below is used to get the information about
the current process. The routine UF_ask_system_info retrieves the
information about the process and fills the structure. Once the data is used,
the memory allocated to these fields should be freed by calling the routine,
UF_free_system_info.
*/
struct UF_system_info_s
{
char *date_buf; /* Current date and time info */
char *user_name; /* User, who is running this process */
char *program_name; /* The current program name */
char *node_name; /* Machine, on which this process is running */
char *machine_type; /* Hardware type on which the machine is running */
char *os_name; /* Operating system, on which this process is running
*/
char *os_version; /* Version and release level of this Operating System
*/
long physical_memory; /* Returns the number of bytes of physical memory
on this machine. */
char **bundles_used; /* Array of the names of the bundles currently in use. */
int number_of_bundles; /* The number of bundles currently in use */
};
typedef struct UF_system_info_s
UF_system_info_t, *UF_system_info_p_t;
/****************************************************************************
* Get the information about an Open C Program
*
* This routine can be used to gather the system information of an Open C
* program, like the machine name, Operating System information etc., and is
* useful in benchmarking, where you want to record the information about
* the machine the benchmark was run on.
*
* This routine outputs the data through the structure UF_system_info_t.
*
* Once the data is no longer needed, the memory allocated to the fields
* of this structure should be freed by a corresponding call to the routine
* UF_free_system_info.
*
* Environment: Internal and External
*
* See Also:
* UF_free_system_info
* UF_system_info_t
*
* History: Released in V18.0, modified in NX 6.0 to return used bundles
****************************************************************************/
extern UFUNEXPORT int UF_ask_system_info(
UF_system_info_p_t info /* <OF>
structure to hold the process information.
The allocated fields should be freed by
calling UF_free_system_info
*/
);
/****************************************************************************
* Free the fields of the structure UF_system_info_t, containing the process
* information
*
* This structure is filled earlier by a call to the routine UF_ask_system_info
*
* Environment: Internal and External
*
* See Also:
* UF_ask_system_info
* UF_system_info_t
*
* History: Released in V18.0
****************************************************************************/
extern UFUNEXPORT int UF_free_system_info(
UF_system_info_p_t info /* <I>
structure whose fields are to be freed
*/
); /* */
/****************************************************************************
* Start a timer.
*
* This routine can be used to gather timing information about an Open C
* program, and is useful in benchmarking. This routine will start a timer.
* The timer will be stopped with a corresponding call to UF_end_timer.
*
* More than one timer can be active at any time, this is useful when you
* have one overall timer, and then several sub-timers timing individual
* sub-operations.
*
* Environment: Internal and External
*
* See Also:
* UF_end_timer
* UF_timer_values_t
*
* History: Released in V18.0
****************************************************************************/
extern UFUNEXPORT int UF_begin_timer (
UF_timer_p_t timer /* <O>
* Timer id that is created
*/
);
/****************************************************************************
* Stop the timer and get the timer values
*
* This routine is used to gather timing information about an Open C program,
* and is useful in benchmarking. This routine will stop the timer created by
* a corresponding UF_begin_timer call, and output the timing information in
* the structure UF_timer_values_t.
*
* Environment: Internal and External
*
* See Also:
* UF_begin_timer
* UF_timer_values_t
*
* History: Released in V18.0
****************************************************************************/
extern UFUNEXPORT int UF_end_timer (
UF_timer_t timer, /* <I>
* Timer to be stopped
*/
UF_timer_values_p_t values /* <O>
* Timer values when it is
* stopped
*/
);
/*****************************************************************************
* Frees the memory allocated and returned by an Open C API routine.
*
* Return : void
*
* Environment: Internal and External
*
* See Also:
*
* History:
*****************************************************************************/
extern UFUNEXPORT void UF_free (
void *data /* <I> Pointer to data item to free */
);
/*****************************************************************************
* Allocates a block of storage and returns a pointer to it. Use UF_free
* to free the allocated memory when no longer required.
*
* Return:
* void * - a pointer to the block of storage, aligned so
* that any data type can be stored in it.
* when error occur or nbytes = 0, a NULL pointer
* is returned
*
* Environment: Internal and External
*
* See Also:
*
* History: This function was originally released in V15.0
*****************************************************************************/
extern UFUNEXPORT void *UF_allocate_memory(
unsigned int nbytes, /* <I>
The number of bytes to be allocated.
If 0, NULL is returned
*/
int *error_code /*<O>
NX standard error code
0 success
!=0 failure
*/
);
/*****************************************************************************
* Reallocates a block of storage and returns a pointer to it. Use UF_free
* to free the allocated memory when no longer required.
*
* Return:
* void * - a pointer to the block of storage, aligned so
* that any data type can be stored in it.
* when error occur or nbytes = 0, a NULL pointer
* is returned
*
* Environment: Internal and External
*
* See Also:
*
* History: This function was originally released in V16.0
*****************************************************************************/
extern UFUNEXPORT void *UF_reallocate_memory(
void *data, /* <I>
Pointer to previously allocated memory
*/
unsigned int nbytes, /* <I>
The number of bytes to be allocated.
If 0, NULL is returned
*/
int *error_code /* <O>
NX standard error code
*/
);
/*****************************************************************************
* Frees the memory allocated for an array of pointers and frees the
* strings within the array. You must pass in the number of pointer in
* the array. Various Open C API routines malloc space for an array
* of pointers, and then allocate space for each of the pointers.
*
* Return : void
*
* Environment: Internal and External
*
* See Also:
*
* History:
*****************************************************************************/
extern UFUNEXPORT void UF_free_string_array (
int n_strings , /* <I>
number of pointers
*/
char **string_array /*<I> n_strings
pointer to the array of pointers to free
*/
);/**/
/*****************************************************************************
* Returns the message string associated with an error code.
*
* Environment: Internal and External
*
* See Also:
*
* History:
*****************************************************************************/
extern UFUNEXPORT int UF_get_fail_message (
int fail_code , /* <I>
the failure code to translate
*/
char message[ 133 ] /* <O>
the message corresponding to the fail code
*/
);
/*****************************************************************************
* Returns the message string associated with an error code in current user interface language.
*
* Environment: Internal and External
*
* See Also:
*
* History: Originally released in NX 10.0
*****************************************************************************/
extern UFUNEXPORT int UF_get_translated_fail_message(
int fail_code , /* <I>
the failure code to translate
*/
char ** message /* <O>
the message corresponding to the fail code
*/
);
/***************************************************************************
* Explanation: In UG V9, when an entity had a known Entity IDentifier *
* (EID), that EID was saved with the part and would be the same the next *
* time the part was loaded. In V10, because multiple parts can be loaded *
* at once, the Tag (ie, EID) of an object can not be guaranteed between *
* sessions. For this reason, "Handles" were created to identify objects *
* between sessions. To aid applications where the EID was saved in some *
* data file between sessions, UF_ask_new_tag_of_entity() was created to *
* return the V10 tag corresponding to the EID of an entity in a V9 part *
***************************************************************************/
/***************************************************************************
* This function replaces UF_TAG_ask_handle_of_tag.
*
* Return the persistent HANDLE for an object tag.
*
* Multiple parts can be loaded into NX during a single session, and
* the Tag (i.e. Object Identifier) cannot be guaranteed between sessions.
* Consequently, "handles" were created to identify objects between sessions.
* This handle is persistent between sessions once the object is saved to a part file.
* A handle of a new object in this session which is never saved is not guaranteed
* to stay the same until the object is saved. Recreating the same object in a new
* session may not be the same even if seemingly identical steps were taken to create
* the object. This is particularly true across versions of software.
*
* Handles should not be compared directly for checking identity as they contain
* version information. Handles should be broken apart using UF_TAG_decompose_handle
* and the file_data strings compared and the sub_file_id integers compared but the
* version should be ignored.
*
* Operations which change the name of the part will change the handle as well - so
* "Save As" will cause handles to change.
*
* This function will return an error when the part data of the handle
* contains a character that cannot be represented. For this reason
* it is suggested that UF_TEXT_set_text_mode(UF_TEXT_ALL_UTF8) be
* set when you are working with handles that may come from parts that have
* characters that are outside of your locale (e.g. parts with Japanese
* characters on an english system).
*
* Output:
* The name of handle for object tag. This string must be freed by calling UF_free.
*
* Environment: Internal and External
* See Also: UF_TAG_ask_tag_of_handle
* History: Originally released in NX 10.0
***************************************************************************/
extern UFUNEXPORT int UF_TAG_ask_handle_from_tag (
tag_t object_tag, /* <I>
tag of object to query for persistent handle
*/
char **handle /* <OF>
Output handle for the tag.
*/
);
/****************************************************************************
* Return the object tag of a persistent HANDLE.
*
* Return:
* Returns object tag of object handle
*
* Environment: Internal and External
*
* See Also: UF_TAG_ask_handle_from_tag
*
* History:
****************************************************************************/
extern UFUNEXPORT tag_t UF_TAG_ask_tag_of_handle (
char *object_handle /* <I>
Name of persistent handle
*/
);/* */
#define UF_ask_new_tag_of_entity UF_TAG_ask_new_tag_of_entity
/****************************************************************************
* Returns the new tag of the object corresponding to the known object
* ID in the V9 part. This only works for the Object IDs of the last V9
* part loaded into this session.
* NOTE: This was renamed from UF_ask_new_tag_of_entity()
*
* Return:
* New tag
*
* Environment: Internal and External
* See Also: UF_TAG_ask_handle_from_tag
* History:
****************************************************************************/
extern UFUNEXPORT tag_t UF_TAG_ask_new_tag_of_entity (
tag_t v9_eid /* <I>
Known Object ID (EID) of V9 part
*/
);/* */
/*****************************************************************************
* Given the constituent parts of data manager, filename, subfile id and
* version, this function returns the resulting handle.
*
* Environment: Internal and External
*
* See Also:
*
* History:
******************************************************************************/
extern UFUNEXPORT int UF_TAG_compose_handle (
const char *file_data , /* <I>
Data about the file. This string would come
from a call to UF_TAG_decompose_handle.
*/
unsigned int sub_file_id , /* <I>
sub_file identifier. The sub_file is
an internal file in the part file database.
*/
unsigned int version , /* <I>
Version of part
*/
char **handle /* <OF>
String containing the composed handle
*/
);
/*****************************************************************************
* Given the handle, the constituent parts of data manager, filename, subfile
* id and version are returned.
*
* Note this function will return an error if you have UF_TEXT_set_text_mode()
* set to locale and the file that the data is coming from has characters
* outside of your locale. It is suggested that you set your text mode to
* UF_TEXT_ALL_UTF8 when you are working with handles.
*
* Environment: Internal and External
*
* See Also: UF_TAG_ask_new_tag_of_entity
* UF_TAG_ask_handle_from_tag
*
* History:
******************************************************************************/
extern UFUNEXPORT int UF_TAG_decompose_handle(
char *handle , /* <I>
Handle to decompose
*/
char **file_data , /* <OF>
Data about the file. This can be used by
UF_TAG_compose_handle. This argument
must be freed by calling UF_free.
*/
unsigned int *sub_file_id , /* <O>
Sub-file identifier for handle. The
sub_file is an internal file in the part
file database.
*/
unsigned int *version /* <O>
Version of part in which handle is located.
*/
);
#define UF_set_program_name UF_MISC_set_program_name
/****************************************************************************
* Each part file has an internal history storage area where the program
* name can be stored when the system saves the part file. This function
* enables you to specify either the entire program name (External
* mode) or append a name to the program name (Internal mode). You
* should call this routine before you call UF_PART_open since it does
* not set the program name on parts that are already opened. A utility
* called ug_inspect enables you to read the program name stored in the
* history area.
*
* Interactively (Internal mode), when you are in NX, the program
* name will take the version of NX currently being run (e.g. NX9.0.0.19)
* and append the string being passed into UF_MISC_set_program_name. For
* example, if you specify "XYZ version 9.0" as the name string to this
* routine, then the program name in the history would look like:
* NX 9.0.0.19XYZ version 9.0
* To separate the version and string, put a leading space in the name being
* passed into this routine. " XYZ version 9.0" passed in will create:
* NX 9.0.0.19 XYZ version 9.0
*
* Once UF_terminate is called, the appended string is removed and it will
* default back to the NX version number the next time the part is saved.
*
* In External mode, the program name is what you specify in the name
* string. From our previous example this would be XYZ version 9.0.
* The limitation for the length of the name string depends on which
* mode you are in, Internal or External. The maximum length of the
* entire program name is 128 characters. In Internal mode, because the
* name string is concatenated to the program name you are limited to
* 64 characters. In External mode, since the name string you specify
* becomes the program name you are limited to 128 characters. In
* either mode, if you specify a name that is to long, the name is
* truncated to either 64 or 128 characters (Internal and External mode
* respectively).
*
* The internal history area is like a log file. If you resave the part file
* with a different program a new history entry is added to the part file.
* That is, the history grows larger. Thus you are likely to see two lines of
* history if you have saved the part file twice and specified a name with
* each save.
*
* Return: void
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT void UF_MISC_set_program_name (
const char *name /* <I>
Name of program to store in the internal history
*/
);
/****************************************************************************
* UF_MISC_set_program_name_persistent will work exactly like UF_MISC_set_program_name
* with the exception that a call to UF_terminate will not remove the appended
* name from the part history. It will stay around for the entire NX session.
*
* Return: void
*
* Environment: Internal and External
*
* See Also:
*
* History: Originally released in NX12.0.1
****************************************************************************/
extern UFUNEXPORT void UF_MISC_set_program_name_persistent (
const char *name /* <I>
Name of program to store in the internal history
*/
);
/****************************************************************************
* Translates environment variables to their equivalence strings. You
* must supply the complete name of the variable argument. The pointer passed
* back points to an operating system string. This string must not be changed.
*
* Environment: Internal and External
*
* See Also: See the example
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_translate_variable (
const char *variable , /* <I>
Environment Variable to Translate
*/
char **translation /* <O>
Translated variable name or NULL if nonexistent.
*/
);
/****************************************************************************
* Sets an environment variable to the string specified in value. You must
* supply the complete name of variable.
*
* Environment: Internal and External
*
* See Also: See the example
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_set_variable (
const char *variable , /* <I>
Environment Variable to set in Operating System
*/
const char *value /* <I>
Value or equivalence string for the variable.
*/
);
/****************************************************************************
* Initializes the Open C API environment and allocates an Open C
* API execute license. If you do not call UF_initialize, then subsequent
* calls to Open C API fail with an error code of
* UF_err_program_not_initialized. This function must be the first
* function you call after you have declared your variables.
*
* In external mode, you may only call UF_initialize once. Once
* UF_terminate is called, there is no way to reconnect to the Open C environment.
*
* Programs need to call UF_terminate before exiting to ensure licenses are
* released and avoid errors in downstream NXOpen programs.
*
* Environment: Internal and External
*
* See Also:
* Refer to the UGII_UGOPEN_SESSION variable
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_initialize (
void
);/**/
/****************************************************************************
* Same as UF_initialize with the addition that Direct Model is also initialized.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_initialize_dm (
void
);
/****************************************************************************
* Checks if the Open C API environment has been successfully
* initialized.
*
* Return:
* return code:
* 0 = Open C API is not initialized.
* 1 = Open C API has been properly
* initialized.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_is_initialized (
void
);/* */
/****************************************************************************
* Terminates the Open C API environment and deallocates a
* Open C API execute license. If UF_terminate is not called, the
* Open C API execute license may not be freed. Once UF_terminate
* is called in an external Open C API program, the program will
* exit. You will not be able to call UF_initialize again and continue
* operation.
*
* Calling this method will release all licenses in the default context.
*
* Once UF_terminate has completed in an external program, you can no
* longer write to the console window. It must be reinitialized with system
* calls.
*
* Environment: Internal and External
*
* See Also:
* Refer to the UGII_UGOPEN_SESSION variable
* History:
****************************************************************************/
extern UFUNEXPORT int UF_terminate (
void
);
/****************************************************************************
* Reserve a license against the specified license context.
* If the specified user-defined context does not already exist it will be created.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_reserve
(
const char* license , /* <I>
License feature name to be reserved
*/
const char* context_name /* <I>
Name of context to reserve license against. Will use the default context if NULL is specified.
*/
);
/****************************************************************************
* Release a license against the specified license context.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_release
(
const char* license , /* <I>
License feature name to be released
*/
const char* context_name /* <I>
Name of context to release license against. Will use the default context if NULL is specified.
*/
);
/****************************************************************************
* Release all licenses against the specified license context. If
* the context specified is a user-defined context it will be deleted.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_release_all
(
const char* context_name /* <I>
Name of context release to release. Will use the default context if NULL is specified.
*/
);
/****************************************************************************
* Returns the licenses that are currently reserved against a context.
* This method will also output the licenses reserved against the default context in the syslog.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_get_reserved_licenses
(
const char* context_name, /* <I>
Name of context to release against. Will use the default context if NULL is specified.
*/
int *n_licenses, /* <O>
The number of licenses.
*/
char*** licenses /* <OF>
The list of license reserved against the specified context. This must be
freed by calling UF_free_string_array.
*/
);
/***************************************************************************
* Encodes an input authorization file using an integer value for
* perturbation.
*
* Environment: Internal
*
* See Also:
*
* History:
*************************************************************************/
extern UFUNEXPORT int UF_encode_auth_file (
int key , /* <I>
Value used to perturb the input file
*/
char *input_file , /* <I>
Input authorization file name
*/
char *output_file /* <I>
Output encoded authorization file name
*/
);
/***************************************************************************
* Decodes an input authorization file using an integer key value that
* matches the original key for perturbation.
*
* NOTE: See %UGII_BASE_DIR%\UGALLIANCE\alliance_readme.txt for more information
*
* Environment: Internal
*
* See Also:
*
* History:
**************************************************************************/
extern UFUNEXPORT int UF_decode_auth_file (
int key , /* <I>
Integer valued key for decoding the input file
*/
char *input_file, /* <I>
Input authorization file to decode
Use the leaf name of a file located under the folder %UGALLIANCE%\auth_files.
Entering the full path will return an error of -5 "Invalid file name".
*/
void **out_mem /* <OF>
Pointer to decoded contents of the authorization
file. Use UF_free to deallocate the memory.
*/
);
/*****************************************************************************
* Returns the current application module. The value that is returned
* maps to a string defined constant. You can find the string in the
* header file uf.h. The strings are of the form UF_APP_<module>.
* For example, UF_APP_DRAFTING represents the drafting module.
*
* Note - if this function is called from an external program it will
* always return a FALSE and an app id of APP_NONE.
*
* Environment: Internal and External
* See Also:
* History:
*****************************************************************************/
extern UFUNEXPORT int UF_ask_application_module(
int *module_id /* <O>
The module identification value of the
current application.
*/
);
/*****************************************************************************
* Calls and executes a GRIP program. Your GRIP program must be written,
* compiled, linked, and ready to run.
*
* While a GRIP program executes, it can have access to an Open C API function
* arguments and their contents. Argument passing to the GRIP program occurs
* through UFARGS. After GRIP program termination, the Open C API program has
* access to any assignments made by the GRIP program. The GRIP program
* completes its execution and then UF_call_grip outputs a return value.
*
* Note: If the path is omitted in the grip_executable string passed to
* UF_call_grip, NX will look in the current directory for the grip program.
* It will not look in the directory of the ufunc program or use any
* environment variables, including UGII_INITIAL_GRIP_DIR, to search for the
* GRIP program.
*
* UF_translate_variable can be used to extract an environment variable and
* concatenate it with the program name.
*
* The following GRIP commands are not
* supported in External mode when calling GRIP:
* ALL OF GRIP NC
* PLNOTE EDTXHT CHAIN
* BLANK UNBLNK RVBLNK
* If any of these commands are encountered, an error is written to the
* batch log file.
*
* Environment: Internal and External
*
* See Also: See the example
* which calls the grip program.
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_call_grip (
char *grip_executable, /* <I>
Name of GRIP program to execute (file name
or full path name).
*/
int count, /* <I>
Count of arguments to pass to GRIP executable
*/
UF_args_p_t UFARGS /* <I>
An array of structures where each element in
the array is a structure that contains an
arguments type, size, and address. Note that
if an argument is type UF_TYPE_CHAR, the array
must be initialized prior to the UF_call_grip
call.
*/
);
/*****************************************************************************
* This routine retrieves a customer default value from the database.
* There are several different conditions that can arise from querying
* the database:
* 1) The record was found and its units match. The function
* returns SUCCESS(0)
* 2) The record was not found. If units given was ENGLISH or METRIC
* nothing is returned and the function returns a FAILED(1). If
* the units given was NONE a second and/or third attempt is made
* with units ENGLISH THEN METRIC used instead. The results of
* these attempts can be any of the conditions outlined above.
*
* If you specify either METRIC or ENGLISH for units, this function
* automatically appends _MU or _EU to the input name. For example, if you
* specify METRIC and input the name "UG_gridSpacingY", the function searches
* for "UG_gridSpacingY_MU".
*
* If you specify NONE for units, the function searches for the name
* as specified. If the name is not found it searches again with _EU
* appended to the name. If the name is still not found, then it
* appends _MU to the name for its final search.
*
* Return:
* return code:
* 0 = Success
* 1 = Record not found
* <0 or >1 = Use UF_get_fail_message to get error.
*
* Environment: Internal and External
*
* See Also: See the example
*
* History:
*****************************************************************************/
extern UFUNEXPORT int UF_get_customer_default(
char * name , /* <I>
Name of Module ID and default
*/
int units , /* <I>
Units are enumerated as follows:
0 = NONE
1 = METRIC
2 = ENGLISH
*/
char ** default_value /* <OF>
String containing default value. If
*default_value is NULL then the value was
not found or an error occurred. Use UF_free
to deallocate memory when no longer required.
*/
);
/**************************************************************************
* Returns the current major release version number. For example, if
* you call this function from V10.4.1, it returns V10.4. You must use
* UF_free to deallocate space used by release.
*
* Environment: Internal and External
*
* See Also:
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_get_release(
char ** release /* <OF>
Major release version number
*/
);
typedef void (*UF_load_f_p_t)( void );
/**********************************************************************
* Loads the shared library specified by library_name and finds the entry
* point specified by symbol_name in that library. The reference to the
* specified entry point is output as a function pointer declared to accept
* and return void (i.e. type UF_load_f_p_t).
*
* For the entry point to be found on Windows NT, you must declare it with
* the DllExport macro, e.g.
*
* extern DllExport int my_function(...
*
* without the DllExport, the name will not be exported. Since the DllExport
* also works on Unix systems, the best practice is just to always use the
* DllExport macro for routines you want exported.
*
* If library_name is found but symbol_name is not, an appropriate error
* code returns, but the loaded library may not be unloaded. The user
* should call UF_unload_library to explicitly unload library_name on
* failure, if appropriate.
*
* To load a shared library into an external application - the library must
* not be linked against any interactive libraries. This can be accomplished
* by using the "-noui" option on Unix.
*
* NOTE: UF_load_library is intended for function (i.e. "text" entry
* point) lookup only. It should NOT be used for data symbol lookup.
*
* Environment: Internal and External
*
* See Also: UF_unload_library
* The UF_load_library example is split into an, internal program
* which is loaded by the external program.
*
* History:
**********************************************************************/
extern UFUNEXPORT int UF_load_library(
const char * library_name ,/* <I>
Name of shared library to load.
*/
const char * symbol_name ,/* <I>
Name of symbol (function) to find.
*/
UF_load_f_p_t *function_ptr /* <O>
Pointer to symbol (function) in library.
*/
);/**/
/**********************************************************************
* Unloads the shared library specified by library_name. UF_unload_library
* unloads the library unconditionally, effectively invalidating all function
* pointers previously set by calls to UF_load_library for the specified
* library.
*
* Environment: Internal and External
*
* See Also: UF_load_library
* The two UF_load_library example one and
* example two use UF_unload_library.
*
* History:
*
*********************************************************************/
extern UFUNEXPORT int UF_unload_library(
char * library_name /* <I>
Name of shared library to unload.
*/
);
/****************************************************************************
* Force NX to shut down immediately. This is a substitute for the standard
* c function: exit(0)
*
* Warning: depending on the current state of NX, forcing a shutdown
* may produce warnings/errors as NX attempts to close itself.
*
* Environment: Internal and External
*
* History: NX 6.0.1
****************************************************************************/
extern UFUNEXPORT void UF_sys_exit( void );/**/
/*****************************************************************************
* Checks to see if an NX Manager process is
* active. It returns true if NX Manager is active.
*
* Environment: Internal and External
*
* See Also:
*
* History:
*****************************************************************************/
extern UFUNEXPORT int UF_is_ugmanager_active(
logical *is_active /* <O>
Returns true if NX Manager is active
*/
);
/****************************************************************************
* Returns the code set identifier supported by a machine. The code set
* identifier can be any one of the enumerated constants in UF_codeset_e.
*
* Environment: Internal and External
*
* See Also: UF_codeset_t
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_ask_codeset(
UF_codeset_t *codeset /*<O>
Pointer to the codeset identifier.
*/
);
/*
* These are the reasons against which call backs can be registered.
*
* The registered callbacks will be called whenever the specific reason occurs
* in interactive NX.
*
* For all the reasons, except for UF_close_part_reason, the callbacks will be
* called towards the end of that particular operation. For example, the
* callbacks registered against UF_create_part_reason will be called when a
* new part is created, after almost all the process of creating this new part
* is completed.
*
* The UF_change_work_part_reason call back will be called after a work part change
* has occurred. It should be noted that this callback may be called at times where the
* old work part (which is passed as the part tag data to the call back routine) may
* not necessarily be different from the new work part. For example, this call back is
* also called if the display part has changed but the new work part is still the same tag
* and now represents a component in a different display part. This call back may be
* called more than once as part of a single operation.
*
* An attempt to query the work or display part in a UF_save_part_reason_callback
* may return unexpected results.
*
* The callbacks registered against UF_close_part_reason will be called at the
* beginning of part close.
*
* The callbacks registered against UF_modified_part_reason will be called
* when the part is modified for the first time after opening it or after a
* save operation.
*
* These callbacks give a handle to the user to do some extra processing, in
* addition to the processing that NX does, during that particular operation.
*
* In NX Manager mode, when a new part is being created it first loads the
* template part (seed part), changes the template part to be the work part
* and then renames the work part to the new part name given. So, the following callbacks are being called:
* UF_modified_part_reason, UF_open_part_reason, UF_change_work_part_reason,
* UF_rename_part_reason and UF_create_part_reason.
*/
enum UF_callback_reason_e
{
UF_create_part_reason, /* Callback when a new part is created. */
UF_open_part_reason, /* Callback when an existing part is opened. */
UF_save_part_reason, /* Callback when a part is saved. */
UF_save_as_part_reason, /* Callback when a part is saved-as. */
UF_close_part_reason, /* Callback when a part is closed. */
UF_modified_part_reason, /* Callback when a part is modified. */
UF_rename_part_reason, /* Callback when a part is renamed. */
UF_change_work_part_reason, /* Callback when there is a new work part.
The part returned is of the old work part.
Use UF_ASSEM_ask_work_part to get new work part. */
UF_post_save_as_part_reason, /* Callback reason for adding parts for
Save As at the end of in progress Save As operation
of selected part/parts, it's like nested Save As.
Only issued in managed mode. */
UF_max_reason /* Do not use - not a valid reason */
};
typedef enum UF_callback_reason_e UF_callback_reason_e_t;
/* Definition of a callback function prototype. */
typedef void (*UF_callback_fn_t)(
UF_callback_reason_e_t, /* <I> reason the callback has been called */
const void*, /* <I> This is the pointer to the part tag that
caused the callback. For UF_change_work_part_reason
the part returned is of the old work part.
Use UF_ASSEM_ask_work_part to get new work part.
*/
void* /* <I> This is a user supplied pointer. Typically
this will be a structure pointer of data
that your callback function will need.
*/
);
typedef struct UF_registered_fn_s *UF_registered_fn_p_t;
/****************************************************************************
* Registers the callback to be called whenever the reason specified
* occurs within NX.
*
* Please note the following:
*
* Once a routine is registered as a callback, the shared library it
* resides in should not be unloaded until it is deregistered.
*
* The callback function must call UF_initialize and UF_terminate, if
* it makes any Open C function calls
*
* The callback function receives three arguments:
* argument 1 - The reason the callback has been called
* argument 2 - A pointer to the part tag that caused the callback.
* argument 3 - A user supplied pointer. Typically this will be a
* structure pointer of data that the callback function
* will need.
*
* The callback will be called towards the end of the processing for that
* particular reason. For example, the callback registered against
* UF_create_part_reason will be called when a new part is created, after
* almost all the process of creating this new part is completed.
*
* The only exception to the above is UF_close_part_reason, for which
* the callback will be called at the beginning of closing the part.
*
* NOTE: For the new and open part reasons the callback is run at a time
* when the newly created or opened part has not been set as the work part.
* Also operations such as create part, open part, save part or change display part
* should not be called from callbacks fired by any of these same operations.
*
* Environment: Internal and External
*
* See Also: UF_remove_callback_function
* UF_callback_reason_e
* Refer to the example of setting up a callback.
*
* History: V16 was changed to require the callback to call UF_initialize
****************************************************************************/
extern UFUNEXPORT int UF_add_callback_function (
UF_callback_reason_e_t reason, /* <I>
Reason to call callback
*/
UF_callback_fn_t fn, /* <I>
Function to call. Note this function
must call UF_initialize if it
makes any Open C function calls. It
should also call UF_terminate.
*/
void *user_data, /* <I>
User data. This pointer will be passed
to your callback function as the third
argument. It will typically be a
structure pointer with information that
your callback function will require.
*/
UF_registered_fn_p_t *function_id /* <O>
Identifier to use to remove callback
*/
);
/****************************************************************************
* Deregisters the callback specified by the identifier.
*
* Environment: Internal and External
*
* See Also: UF_add_callback_function
*
* History:
****************************************************************************/
extern UFUNEXPORT int UF_remove_callback_function (
UF_registered_fn_p_t function_id /* <I>
Identifier from UF_add_callback_function
*/
);
/****************************************************************************
* The following set of routines allow the registration of routines to be
* called when tags are created and deleted. This allows synchronisation of
* data structures outside of NX with NX. Note that the routines registered
* can not call any other UF routines themselves. Also the implementation
* of any routine so registered must be very efficient as it will be called
* very many times.
*
* Also it should be remembered that tags get reused. This means that the
* order of events is important so the event is interpreted with respect
* to the right incarnation of the tag.
****************************************************************************/
/****************************************************************************
* This enum identifies the type of an event that occurred on a tag.
****************************************************************************/
enum UF_TAG_event_e
{ UF_TAG_EVENT_NORMAL_CREATE, /* The tag was created. */
UF_TAG_EVENT_UNDO_OVER_CREATE, /* An undo occurred over the tag's
creation and so is now invalid. */
UF_TAG_EVENT_NORMAL_DELETE, /* The tag was deleted. */
UF_TAG_EVENT_UNDO_OVER_DELETE, /* An undo occurred over the tag's
deletion and so has come back to
life. */
UF_TAG_EVENT_UNDO_DELETE_EXPIRED, /* NX will now never undo over
the deletion so it will never come back
to life. */
UF_TAG_EVENT_UNDO_CREATE_EXPIRED /* NX will now never undo over
the tags creation. */
};
typedef enum UF_TAG_event_e UF_TAG_event_t;
/****************************************************************************
* Type of the event notification callback.
*****************************************************************************/
typedef void (*UF_TAG_event_fn_t)(UF_TAG_event_t reason, /* <I> */
tag_t tag, /* <I> */
void *closure /* <I> */);
/*****************************************************************************
* Register a new tag event callback. All callbacks are called on all tags
* for all events. This returns an identifier for the callback which is
* used to allow it removal.
*
* Please note the following items:
* . The routines registered can not call any other Open C routines
* In particular, the tag cannot be queried or edited in any way.
* . The implementation of any routine so registered must be very
* efficient as it is called many times.
* . Recall that tags get reused. This means that the order of events is
* important so the event is interpreted with respect to the right
* "incarnation" of the tag.
*
* Environment: Internal and External
*
* See Also: UF_TAG_unregister_event_cb
*
* History: This function was originally released in V15.0.
****************************************************************************/
extern UFUNEXPORT int UF_TAG_register_event_cb(
UF_TAG_event_fn_t callback, /* <I>
Callback function
*/
void *closure, /* <I>
Pointer passed to callback on
each call
*/
int *callback_id /* <O>
Identifier for callback
*/
);
/****************************************************************************
* Unregister a previously registered callback.
*
* Environment: Internal and External
*
* See Also: UF_TAG_register_event_cb
*
* History: This function was originally released in V15.0.
****************************************************************************/
extern UFUNEXPORT int UF_TAG_unregister_event_cb(
int callback_id /* <I> - identifier of callback */
);
/****************************************************************************
* Set a flag that determines if an Open C executable will issue
* warnings when a function that is scheduled to be retired is called.
* This can be used to alert the NX Open programmer that modification to
* their program is required.
*
* When routines are planned to be removed from the NX Open interface, the
* prototype will be moved to uf_retiring.h, along with a description of
* what the NX Open programmer should do. A warning can be issued when
* any of these routines are called by an NX Open application. This routine
* allows the NX Open programmer to set the value of this flag.
*
* This routine overrides the environment variable
* UGII_USING_RETIRING_FUNCTIONS which can be set by the user to get
* the same warnings. This routine is meant to be used when the programmer
* wants to force a particular value for a program.
*
* Environment: Internal and External
*
* See Also:
*
* History: Released in V16.0
****************************************************************************/
extern UFUNEXPORT int UF_set_retiring_flag(
int value /* <I>
0 = Don't warn user at all, this is the default
1 = Output a single message if any function is called
that is planned to be obsoleted
2 = Output a message for each function called that
is planned to be obsoleted. The message will include
the routine name, and the number of times called.
*/
);
/****************************************************************************
* Output a message to the syslog.
*
* This message can be used to print run time information about the NX Open
* program to the syslog and is useful for state checking, validation and
* debugging.
*
* Printing the trace is especially useful while debugging and reporting a
* problem.
*
* Environment: Internal and External
*
* See Also:
*
* History: Released in V18.0
****************************************************************************/
extern UFUNEXPORT int UF_print_syslog(
char *message, /* <I>
Message to be output to the syslog
*/
logical trace /* <I>
TRUE = Print the stack trace along with the message
FALSE = Print only the message
*/
);
/****************************************************************************
* Get name of the current syslog
*
* Environment: Internal and External
*
* See Also:
*
* History: Released in NX2.0.5
****************************************************************************/
extern UFUNEXPORT int UF_ask_syslog_filename(
char **filename /* <OF>
pointer to dynamically allocated path
filename must be freed with UF_free()
*/
);
/****************************************************************************
* Find a given subdirectory and file. This routine will traverse all the
* directories specified in the file custom_dirs.dat and ug_custom_dirs.dat
* looking for the file specified by the given subdirectory and filename.
* This routine will return the first file found.
*
* Environment: Internal and External
*
* See Also: UF_find_all_subdirectories
*
* History: Released in NX 1.0
****************************************************************************/
extern UFUNEXPORT int UF_find_file(
const char *subdirectory, /* <I>
The subdirectory in which to look for the
given file.
*/
const char *filename, /* <I>
The filename to look for, including any extension.
*/
char **path /* <OF>
The filename found. If no file is found, **path will
be NULL. The path must be freed by calling UF_free.
*/
);
/****************************************************************************
* Find all subdirectories of a given name in the directories specified in
* the file custom_dirs.dat and ug_custom_dirs.dat. Since the same
* subdirectory may be in multiple directories, an array of path names
* will be returned. As an example searching for the subdirectory "startup"
* will return almost all of the directories, since this is a standard
* subdirectory.
*
* Environment: Internal and External
*
* See Also: UF_find_file
*
* History: Released in NX 1.0
****************************************************************************/
extern UFUNEXPORT int UF_find_all_subdirectories(
const char *subdirectory, /* <I>
The subdirectory to look for.
*/
int *num_found, /* <O>
The number of subdirectories found.
*/
char ***path /* <OF>
The list of subdirectories found. This must be
freed by calling UF_free_string_array.
*/
);
/****************************************************************************
* Select the listing device. The listing device can be set to a file,
* the listing window, or both file and listing window. The listing
* device can also be set to no output.
*
* Return:
* 0 = Success
* 2 = Listing device is unavailable
* otherwise an error code
*
* Environment: Internal and External
*
* See Also: UF_UI_open_listing_window
* UF_UI_close_listing_window
* UF_UI_write_listing_window
*
* History:
****************************************************************************/
extern UFUNEXPORT int uc4400(
int listing_device, /*<I>
The listing device to use:
= 0 standard listing window
= 4 output to a file
= 8 output to both file and listing window
= 9 No output is written
*/
char *file_spec, /*<I>
This is only used for output to a file. This is
the file specification for the output file, and
must be less than MAX_FSPEC_NCHARS characters.
*/
int ip3 /*<I>
This is no longer used.
*/
);
/****************************************************************************
* Query the current disposition of the listing device.
*
* Environment: Internal and External
*
* Returns:
* 0 = Listing device is set to the listing window
* 4 = Listing device is set to a file
* 8 = Listing device is set to both file and the listing window
* 9 = Listing device is set to NULL
* otherwise the return is an error code.
*
* See Also: UF_UI_open_listing_window
* UF_UI_close_listing_window
* UF_UI_write_listing_window
* uc4400
*
* History:
****************************************************************************/
extern UFUNEXPORT int uc4409(
char file_name[ MAX_FSPEC_BUFSIZE ], /* <O>
For return code 4 or 8, this is the file specification
of the listing device file.
*/
int *ir3 /* <O>
Unused.
*/
);
/****************************************************************************
* Query the current NX Open program environment for the current image.
*
* Note: This value is updated during initialization so it is set for
* each image and won't remember the information from previous images.
*
* Environment: Internal and External
*
* Returns:
* Void
*
* History:
****************************************************************************/
extern UFUNEXPORT void uf3192(
int *ir1 /* <O>
The environment that the NX Open program is running in.
0 is External Open, 1 is Internal Open.
*/
);
/******************************************************************************
******************************************************************************
***** WARNING: The routines that follow will be obsoleted soon. *****
***** Do not use them! Use their indicated replacements. *****
******************************************************************************
******************************************************************************
*/
/* uf4401 opens the listing device set by uc4400 for output
if you only need to open the listing window for output
(and not a particular listing device set by uc4400)
this function may be replaced with UF_UI_open_listing_window */
extern UFUNEXPORT void uf4401(int *ir1);
/* uf4402 closes listing device set by uc4400
if you only need to close the listing window
(and not a particular device set by uc4400)
this function may be replaced by UF_UI_close_listing_window */
extern UFUNEXPORT void uf4402(void);
/* uc4403 write character string to listing device set by call to uc4400
if you only need to write to the listing window
(as opposed to a listing device set by uc4400)
this function may be replaced with UF_UI_write_listing_window */
extern UFUNEXPORT int uc4403(const char *cp1/* <I> */);
/* uc4404 write character string and integer to listing device set by uc4400
if you only need to write the data to the listing window
(and not a particular device set by uc4400)
this function may be replaced by UF_UI_write_listing_window */
extern UFUNEXPORT int uc4404(const char *cp1/* <I> */, int ip2);
/* uc4406 write character string and real to listing device set by uc4400
if you only need to write the data to the listing window
(and not a particular listing device set by uc4400)
this function may be replaced by UF_UI_write_listing_window */
extern UFUNEXPORT int uc4406(const char *cp1/* <I> */, double rp2);
/***************************************************************************
***************************************************************************/
#undef EXPORTLIBRARY
#endif /* UF_INCLUDED */