UF_callback_reason_e (view source)
 
Defined in: uf.h
 
Also known as:
 
Overview
These are the reasons against which call backs can be registered.

The registered callbacks will be called whenever the specific reason occurs
in interactive NX.

For all the reasons, except for UF_close_part_reason, the callbacks will be
called towards the end of that particular operation. For example, the
callbacks registered against UF_create_part_reason will be called when a
new part is created, after almost all the process of creating this new part
is completed.

The UF_change_work_part_reason call back will be called after a work part change
has occurred. It should be noted that this callback may be called at times where the
old work part (which is passed as the part tag data to the call back routine) may
not necessarily be different from the new work part. For example, this call back is
also called if the display part has changed but the new work part is still the same tag
and now represents a component in a different display part. This call back may be
called more than once as part of a single operation.

An attempt to query the work or display part in a UF_save_part_reason_callback
may return unexpected results.

The callbacks registered against UF_close_part_reason will be called at the
beginning of part close.

The callbacks registered against UF_modified_part_reason will be called
when the part is modified for the first time after opening it or after a
save operation.

These callbacks give a handle to the user to do some extra processing, in
addition to the processing that NX does, during that particular operation.

In NX Manager mode, when a new part is being created it first loads the
template part (seed part), changes the template part to be the work part
and then renames the work part to the new part name given. So, the following callbacks are being called:
UF_modified_part_reason, UF_open_part_reason, UF_change_work_part_reason,
UF_rename_part_reason and UF_create_part_reason.


Data Members

UF_create_part_reason
Callback when a new part is created.

UF_open_part_reason
Callback when an existing part is opened.

UF_save_part_reason
Callback when a part is saved.

UF_save_as_part_reason
Callback when a part is saved-as.

UF_close_part_reason
Callback when a part is closed.

UF_modified_part_reason
Callback when a part is modified.

UF_rename_part_reason
Callback when a part is renamed.

UF_change_work_part_reason
Callback when there is a new work part.
The part returned is of the old work part.
Use UF_ASSEM_ask_work_part to get new work part.

UF_post_save_as_part_reason
Callback reason for adding parts for
Save As at the end of in progress Save As operation
of selected part/parts, it's like nested Save As.
Only issued in managed mode.

UF_max_reason
Do not use - not a valid reason

 


 
UF_codeset_e (view source)
 
Defined in: uf.h
 
Also known as:
 
Overview
Codesets supported by NX. This is returned by the
function UF_ask_codeset.


Data Members

UF_CODESET_NOT_INITIALIZED=-2
This is an error condition.

UF_CODESET_NOT_SUPPORT=-1
This is an error condition.

UF_CODESET_ASCII
Only ASCII characters are supported.
If NX does not recognize a
codeset, then it will revert to
UF_CODESET_ASCII.

UF_CODESET_ISO8859_1
Western European standard

UF_CODESET_EUC
Japanese EUC codeset

UF_CODESET_SJIS
Japanese SJIS codeset

UF_CODESET_ISO8859_4
Finnish, Latvian, Norwegian, Swedish
and other European languages.

UF_CODESET_ISO8859_5
Russian, Ukrainian, Bulgarian and other
Eastern European languages.

UF_CODESET_ISO8859_8
Hebrew codeset

UF_CODESET_BIG5
Traditional Chinese for Taiwan

UF_CODESET_NT_866
No longer used, placeholder only

UF_CODESET_ISO8859_2
Czech, Polish, Slovak and other
Eastern European languages.

UF_CODESET_NT_852
No longer used, placeholder only

UF_CODESET_NT_862
No longer used, placeholder only

UF_CODESET_KSC5601
Korean codeset

UF_CODESET_GB2312
Simplified Chinese for Mainland China

UF_CODESET_NT_1251
Windows NT Russian codeset

UF_CODESET_NT_1255
Windows NT Hebrew codeset

UF_CODESET_NT_1250
Windows NT Eastern European codeset

UF_CODESET_NT_1252
Windows NT Western European and US
codeset

UF_CODESET_ISO8859_15
Western European codeset including
EURO

UF_CODESET_NT_1253
Windows NT Greek codeset

UF_CODESET_ISO8859_7
Greek Codeset

UF_CODESET_UTF8
UTF-8 Codeset

UF_CODESET_NT_1254
Windows NT Turkish codeset

UF_CODESET_NT_1257
Windows NT Baltic codeset

UF_CODESET_NT_1256
Windows NT Arabic codeset

UF_CODESET_ISO8859_6
Arabic Codeset

UF_CODESET_ISO8859_11
Thai Unix and Windows (CP 874)

UF_CODESET_NT_1258
Vietnamese codeset

 


 
UF_TAG_event_e (view source)
 
Defined in: uf.h
 
Also known as:
 
Overview
This enum identifies the type of an event that occurred on a tag.


Data Members

UF_TAG_EVENT_NORMAL_CREATE
The tag was created.

UF_TAG_EVENT_UNDO_OVER_CREATE
An undo occurred over the tag's
creation and so is now invalid.

UF_TAG_EVENT_NORMAL_DELETE
The tag was deleted.

UF_TAG_EVENT_UNDO_OVER_DELETE
An undo occurred over the tag's
deletion and so has come back to
life.

UF_TAG_EVENT_UNDO_DELETE_EXPIRED
NX will now never undo over
the deletion so it will never come back
to life.

UF_TAG_EVENT_UNDO_CREATE_EXPIRED
NX will now never undo over
the tags creation.