WeldPointExitBuilderFeatureInfo_Struct Struct¶
NXOpen.Weld.WeldPointExitBuilder.FeatureInfo is an alias for NXOpen.Weld.WeldPointExitBuilderFeatureInfo_Struct
-
class
NXOpen.Weld.
WeldPointExitBuilderFeatureInfo_Struct
¶ Bases:
object
Structure used to identify newly created features.
. Constructor: NXOpen.Weld.WeldPointExitBuilder.FeatureInfo()
Fields¶
Field | Description |
---|---|
Feature | the newly created or edited feature |
MethodUsed | the method used to create the feature |
Parent | the parent if method used was mirror or translate |
IsNewlyCreated | true if a new feature, false if an existing feature was edited. |
Feature¶
-
WeldPointExitBuilderFeatureInfo_Struct.
Feature
¶ the newly created or edited feature
-------------------------------------
Field Value Type:
NXOpen.Features.Feature
MethodUsed¶
-
WeldPointExitBuilderFeatureInfo_Struct.
MethodUsed
¶ the method used to create the feature
-------------------------------------
Field Value Type:
NXOpen.Weld.WeldPointExitBuilderMethodUsed
Parent¶
-
WeldPointExitBuilderFeatureInfo_Struct.
Parent
¶ the parent if method used was mirror or translate
-------------------------------------
Field Value Type:
NXOpen.Features.Feature